Deep dive into power conversion systems for battery energy storage systems
We’re bringing you the latest from the world of semiconductors – straight to your ears! From quick takes on trending applications to deep dives on product innovations, our experts give you their take on the tech behind the tech.
Dec 18, 2025
In this episode, host Kelsey Markl welcomes Global System Architect Dr. Manuel Strugholtz to explore the differences between grid-forming and grid-following technologies in stabilizing renewable energy grids. They discuss the challenges of transitioning to distributed energy systems, the technical demands of grid-forming inverters, and how semiconductor innovations like silicon carbide play a crucial role. Will grid-forming become the new standard for future energy grids? Tune in to find out!
In this episode of Podcast4Engineers, host Kelsey Markl speaks with Dr. Manuel Strugholtz, Global System Architect at Infineon.
Host:
Kelsey Markl is Head of Strategic Marketing Communications and Content at Infineon with more than a decade of experience in communications, content strategy, and storytelling. Not being an engineer is part of what makes the journey interesting. Kelsey approaches technical topics from the perspective of a curious outsider, asking the questions that help make complex ideas more accessible and relevant to engineers and broader audiences alike. Passionate about innovation and the people behind it, Kelsey enjoys exploring the trends, challenges, and breakthroughs shaping the future of engineering.
Guest:
Dr. Manuel Strugholtz holds a PHD in electrical engineering with focus on energy efficient intra- and inter system communication topologies. After finishing his doctoral thesis in 2012, he worked for Beckhoff Automation as a hardware and firmware developer for industry 4.0 automation products. From 2017-2023, Manuel headed the product management Team for system solutions at HOPPECKE batteries, where he gained extensive experience in stationary battery storage systems (BESS), uninterruptable power supplies (UPS) and cross application management. Since 2023 he works as a system architect for ESS and UPS at Infineon Technologies GIP in Warstein.
More episodes
Full transcript
Guest: We will take input from the market and from our customer sites worldwide from different regions and create our own critical mission profiles for those grid-forming applications. The junction temperature, for example, of the semiconductor will quickly jump, and therefore we have to improve our semiconductor on our power modules and we do it in the way that we specify them to be able to operate with an extended and increased junction temperature.
Host: This is the Podcast4Engineers, the podcast you just have to listen to if you're interested in what's going on in the semiconductor market. My name is Kelsey Markl, your host, and I'm joined today by Manuel Strugholtz, who is the Global System Architect for Commercial and Utility Scale ESS Systems. Manuel, thanks for being here.
Guest: Thank you for having me here.
Host: Okay, so we're following up this episode. This is the deep dive following Marco's episode on ESS, and we're going to really get into the details of grid forming versus grid following. But for our audience, can you just tell us what that is?
Guest: So, Think about it. The classical energy grid had large so-called baseline power plants. For example, large coal power plants, which were basically responsible for stabilizing the grid. They included large rotating masses in form of their generators who would then some kind of imprint their voltage and the frequency to the grid. And normal installations like photovoltaic power plants or grid-following, so-called grid-following inverters, which were the standard until now, were reading this information and synchronizing to this. Now we have a change and a trend towards more renewable energy sources. And those are all until now so-called grid-following instances and power plants who are reading this information from the grid. With the change that large coal plants, for example, are shut down, this information that is imprinted on the grid that these inverter sources read is getting more and more weak and less easy to read, and which potentially leads to an unstable grid.
Host: Okay. So, you kind of started defining already grid forming then. So, why is grid forming so important now?
Guest: Yeah, somehow, we are going from a centralized grid to a more distributed grid with lots of distributed energy sources. And this means those energy sources will have to supply the information, the synchronization information to the grid to make it more stable so that other sources can use this distributed information, frequency, voltage, current ratings, and so on, read those from the grid and synchronize to them. But this information has to be put into the grid in a distributed manner and not in a centralized manner. And this means that grid forming is really controlling and imprinting this information to the grid and not only following this information that is already on the grid.
Host: Okay, so it seems like grid-forming systems have a lot of responsibility on them. What specific attributes do they have to have in order to meet those demands?
Guest: Yeah, right. They have to do synchronization and are responsible for synchronization and angle stability, which means that if the frequency shifts a little bit in the frequency component, in the angle, they have to counteract that. Also, they have to make sure that a frequency or a drop in a frequency in the line frequency does not get critical. They have to counteract that. They do not have to follow that shift in frequency. They have to counteract and put their frequency in a kind of imprint to the grid. And, they have to regulate the voltage. If they recognize that the voltage is dropping on the grid, they also supply more energy to the grid to raise this voltage again.
Host: Okay. So they're really, really just, I mean, in the true sense of the word, stabilizing everything.
Guest: Correct. That's correct.
Host: Okay.
Guest: And they are doing this by, for example, different techniques, how they react and how they read this information from the grid in comparison to a grid-following inverter. For example, a grid-following inverter uses a PLL. which is an abbreviation for phase-locked loop. It's some kind of technical component who reads the data, the frequency data from the grid, so the inverter can synchronize to that. A grid-forming inverter does this in an active way. They use other technical ways to achieve that. Also, a grid-forming inverter often has the ability to black start a grid. This means if there is no external stimulus to the inverter system itself, they can create the stimulus by themselves and be able to, like the way the name suggested, black start a grid. It's also often called islanding operation, which means some instances of these grid-forming inverter resources can start the grid back up. And then these smaller islanding grids are stable. Other grid-following resources can synchronize up to them, provide their energy, and then hierarchy per hierarchy level, the whole grid will get back up again and synchronized until you have the whole grid running.
Host: So if we, for some reason, lose energy source, lose an energy source from the grid, then these grid-forming capabilities allow it to restart it, give it a jolt of energy to restart it.
Guest: That's correct.
Host: Okay. It sounds like grid-forming also in our conversations with Marco has really become mainstream. What types of installations can we expect to see with grid-forming?
Guest: In general, this is all in the range of the utility-scale installations, not really in the commercial installations. So, in the local backup solutions for self-consumption optimization, but really the larger installations who are directly connected to the grid at a substation level, for example.
Host: Okay, the whole city.
Guest: The whole city or at least parts of the city.
Host: Okay.
Guest: And regarding the architecture, it's both string-level power conversion and central power conversion. And therefore, you have to look at different requirements. For example, a central power conversion inverter or system right now is predominantly air-cooled. So, we have to cope with that and find solutions to enable this grid forming capabilities through this rather inefficient cooling way. String power conversion systems are normally and predominantly liquid cooled, which means you have to also have a look into that if you want to develop solutions for that.
Host: You mentioned these use cases have different requirements, but is there a standardization body setting standards in this area?
Guest: There are working groups worldwide working on this topic and trying to— or not trying, they are defining standards right now, but there are no standards right now. And until they're— until the availability is there for these standards, we will take input from the market and from other customer sites worldwide, from the different regions, and create our own critical mission profiles for those grid-forming applications.
Host: Okay. Critical mission profiles. It sounds pretty intense. Can you explain exactly what that means?
Guest: Yeah. A critical mission profile is basically the time throughout the day at which times an inverter has to provide 100% load or maybe 120% load for 10 minutes, 150% load to the grid or from the grid for 10 seconds. Those are examples. And these different operational states are then combined to a so-called mission profile, which then represents a typical day in such a grid which relies on grid-forming capabilities.
Host: Okay. So, yeah, those critical mission profiles seem pretty critical. Is this what Marco and you mean by overload conditions?
Guest: Exactly. That's the point. There are certain points in the day where maybe grid tends to become unstable. And therefore, the grid-forming inverter has to cope with that. And through an overload condition, he has to put more current back into the system to get the grid stable again. And this is more than normally the inverter is designed for. And therefore, the term overloads, because it's more than their design load, like 150% instead of 100%.
Host: Okay. Is this something that we can address at the semiconductor component level?
Guest: Of course we can. We have different solutions for that, but basically, we have to understand that an overload condition always means we had a lot of power cycling. We call it power cycling, where from one moment to the other you have huge swings in output power of the semiconductor, and this results in thermal cycling. So, the junction temperature, for example, of the semiconductor will quickly jump. And therefore, we have to improve our semiconductors on our power modules. And we do it in the way that we specify them to be able to operate with an extended and increased junction temperature. For example, instead of 150 degrees, our semiconductors can now operate at 175 degrees continuously. Though this will get a lot of stress out of the customer designing the system and optimizing the cooling solution. Speaking of the cooling solution, we are also improving the inside of the module, how the whole stack— this is consisting from the chip, the bond wires, all the substrates down to the heatsink level— that we form a very rigid solution there, that thermal stresses do not result in weakening of the whole product and the power semiconductor module itself.
Host: Okay, improving the interconnections then within the module?
Guest: Yeah, exactly like with the. xt solution.
Host: Okay, is there anything else that we're improving on the chip level or the semiconductor level?
Guest: Basically, we are trying to lower the whole Rth, so the thermal resistance, down to the heatsink level. This means that swings and huge power swings will not lead to huge junction temperature swings and thermal stress inside the module. Therefore, we improve our baseplate modules both for forced air cooling, baseplate indirect liquid cooling, and even with technologies like our WAVE solution for direct liquid cooling, which then helps to— reduce the temperature swings and therefore improve the lifetime of the whole system.
Host: And I think Marco mentioned something about switching the materials, silicon to silicon carbide, for example. Is that something we're also looking at that can address some of the grid forming requirements?
Guest: Of course. Using switching, for example, from IGBTs to silicon carbide allows you to use a lot higher or much higher switching frequencies. And silicon carbide has lower switching losses. in comparison to IGBT, which then lowers your overall losses and therefore the raise in temperature does not even happen. You're trying to shut down the source of these problems before they even occur.
Host: Okay. It sounds like a lot of it comes really down to the component level for grid forming, some of the requirements. Do we expect grid forming to replace grid following eventually?
Guest: Absolutely. Right now, grid forming capabilities come at a premium regarding the CapEx. There is still lots of engineering work and good thoughts to go into this. But we see throughout the world and the different regions that grid-forming requirements are always there. We hear it from the market and therefore both for central power conversion systems and future string power conversion systems, grid-forming capabilities and therefore overload requirements are becoming standard.
Host: Yeah, I think this is a real societal problem that we're all addressing together, how we stabilize the grid as we need more and more energy and switch to renewables. Thank you, Manuel, so much for being with us and explaining that to us.
Guest: Thank you for having me.
Host: And to our listeners out there, please stay tuned.