PSOC™ 4 Die Temperature

Die Temperature Component: Accurate Temperature Measurement

About

The Die Temperature component provides access to the analog signal whose voltage represents the temperature of the die. It also provides the API needed to convert the digital voltage representation of that analog signal to a temperature. This component does not provide the mechanism to convert the analog voltage to a digital value. That must be done in the design by connecting the signal to the ADC in the device and sampling the voltage.

  • Typical measured accuracy of +/- 1 ºC
  •  Valid operating range from –40 °C to +85 °C

The Die Temperature component provides access to the analog signal whose voltage represents the temperature of the die. It also provides the API needed to convert the digital voltage representation of that analog signal to a temperature. This component does not provide the mechanism to convert the analog voltage to a digital value. That must be done in the design by connecting the signal to the ADC in the device and sampling the voltage.

  • Typical measured accuracy of +/- 1 ºC
  •  Valid operating range from –40 °C to +85 °C
Documents

Designressourcen

Image gallary

Psoc4-dietemp
Psoc4-dietemp Psoc4-dietemp Psoc4-dietemp