Analog Resource Constraint (Cy_Analog_Constraint)
Precision Analog Signal Routing
-
Auf dieser Seite
About
The Analog Resource Constraint component allows you to define the route of the analog signal to which it is connected. This is an advanced feature that is not needed for most designs, and should be used with caution.
This feature enforces restricted analog signal routing to a designated resource, necessitating direct connection of all signal terminals to that routing resource.
Routing is strict. All of the devices connected to the net with the resource constraint must have a direct hardware connection to the resource. If the resources do not have a hardware connection to the specified constraint, an error will occur.
The Analog Resource Constraint component allows you to define the route of the analog signal to which it is connected. This is an advanced feature that is not needed for most designs, and should be used with caution.
This feature enforces restricted analog signal routing to a designated resource, necessitating direct connection of all signal terminals to that routing resource.
Routing is strict. All of the devices connected to the net with the resource constraint must have a direct hardware connection to the resource. If the resources do not have a hardware connection to the specified constraint, an error will occur.
Share in WeChat
Scan the QR code with your WeChat App to share this page.