Voltage Regulator Finder
Finder contains Simple and versatile low dropout linear voltage regulators from Infineon
-
Auf dieser Seite
About
Linear voltage regulators are the original type of regulator and can convert a wide range of direct input currents into a single regulated output current of a lower voltage. The input voltage must be higher than the voltage required by the load (output voltage) and there should be a difference of at least 2 V between the two voltage levels. For example, a 5 V low dropout voltage regulator could be used to convert 12 V into 5 V. However, it could not be used to convert 3.3 V into 5 V, as the output voltage would be higher in this case and the difference in voltage levels (dropout voltage) is less than 2 V.
To support you during the evaluation of your product/board, Infineon Developer Center provides you two main sections:
Software: here you will find all the software from Infineon
Tools: here you will find all tools which are getting offered by Infineon for the evaluation
Linear voltage regulators are the original type of regulator and can convert a wide range of direct input currents into a single regulated output current of a lower voltage. The input voltage must be higher than the voltage required by the load (output voltage) and there should be a difference of at least 2 V between the two voltage levels. For example, a 5 V low dropout voltage regulator could be used to convert 12 V into 5 V. However, it could not be used to convert 3.3 V into 5 V, as the output voltage would be higher in this case and the difference in voltage levels (dropout voltage) is less than 2 V.
To support you during the evaluation of your product/board, Infineon Developer Center provides you two main sections:
Software: here you will find all the software from Infineon
Tools: here you will find all tools which are getting offered by Infineon for the evaluation