- eFuses
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
- Gate Driver ICs for SiC MOSFETs
- Isolated Gate Driver ICs
- Gate driver ICs for GaN HEMTs
- Half-Bridge Gate Driver ICs
- High-Side Gate Driver Ics
- Level-Shift Gate Driver ICs
- Low-Side Gate Driver Ics
- Three-Phase Gate Driver Ics
- Transformer Driver ICs
- Overview
- AC-DC LED driver ICs
- Ballast IC
- DC-DC LED driver IC
- LED dimming interface IC
- Linear LED driver IC
- LITIX™ - Automotive LED Driver IC
- NFC wireless configuration IC with PWM output
- VCSEL driver
- Overview
- BLDC motor drivers
- BDC motor drivers
- Stepper & servo motor drivers
- Motor drivers with MCU
- Bridge drivers with MOSFETs
- Gate driver ICs
- Overview
- Automotive MOSFET
- Dual MOSFETs
- MOSFET (Si & SiC) Modules
- N-channel depletion mode MOSFET
- N-channel MOSFETs
- P-channel MOSFETs
-
Silicon carbide CoolSiC™ MOSFETs
- Overview
- Silicon Carbide MOSFET modules
- Silicon carbide MOSFET discretes
- Silicon carbide MOSFETs bare dies
- 400 V / 440 V Silicon Carbide MOSFETs
- 650 V Silicon Carbide MOSFETs
- 750 V Silicon Carbide MOSFETs
- 1200 V Silicon Carbide MOSFETs
- 2000 V Silicon Carbide MOSFETs
- 2300 V Silicon Carbide MOSFETs
- 3300 V Silicon Carbide MOSFETs
- 1700 V Silicon Carbide MOSFETs
- Small signal/small power MOSFET
- Overview
- IGBT modules
- MOSFET (Si & SiC) Modules
- Intelligent power modules (IPM)
- Diodes and thyristors (Si/SiC)
- Automotive IGBT and CoolSiC™ MOSFET modules
- High density power modules
- Overview
- Automotive transceivers
- Linear voltage regulators for automotive applications
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
May 29, 2026
Business & Financial Press
May 20, 2026
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
May 29, 2026
Business & Financial Press
May 20, 2026
Business & Financial Press
May 11, 2026
Business & Financial Press
May 07, 2026
Infineon announces PSOC™ 4 Multi-Sense; expands capacitive sensing technology with inductive and liquid sensing solutions
Infineon announces PSOC™ 4 Multi-Sense; expands capacitive sensing technology with inductive and liquid sensing solutions
Market News
Munich, Germany – 4 March 2025 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced that its PSOC™ 4 microcontroller (MCU) family now features Multi-Sense capabilities. Infineon expands its leading capacitive sensing technology CAPSENSE™ with a new, proprietary inductive sensing technology, as well as a non-invasive and non-contact liquid sensing solution. With PSOC 4, developers now have endless possibilities to develop new HMI and sensing solutions. From sleek metallic product designs with touch on metal buttons, to waterproof touch buttons, and innovative ways of sensing liquids, PSOC 4 Multi-Sense unlocks new possibilities of sensing.
Infineon’s PSOC 4000T is the first device to feature the company’s fifth-generation CAPSENSE and Multi-Sense. The supported sensing technologies can be combined in a single PSOC 4 MCU to optimize performance (e.g., combination of capacitive and inductive sensing), enable new use cases (e.g., underwater inductive sensing buttons) or realize cost savings (e.g., system control plus liquid sensing). In addition, Infineon’s fifth generation CAPSENSE with “Always On” technology enables sensing at 10x lower power consumption and offers a 10x higher signal-to-noise ratio than previous devices.
“Multi-Sense capability is more than a technology advancement – it’s a paradigm shift and proof that Infineon is committed to supporting customer demands for next-generation devices that support new HMI and sensing use cases,” said Vibheesh Bharathan, Director and Project Lead for PSOC 4 Multi-Sense, Infineon. “As a leader in sense and control for consumer and industrial markets, we continue to bring new features to enable customer designs of tomorrow’s digitalization solutions for home, office and industrial applications.”
Infineon’s new Multi-Sense capabilities in the PSOC™ 4 family include:
- Inductive sensing – Based on a new and proprietary methodology which is less sensitive to noise and more robust than current state of the art approaches that suffer from external noise as well as manufacturability concerns. Infineon’s inductive sensing technology enables new HMI use cases, such as touch-over-metal, force touch surfaces and proximity sensing. It is highly complementary to capacitive sensing and enables modern, metal-based and waterproof designs with sleek form factors such as metal touch buttons on refrigerators or robust HMI for underwater devices such as cameras and wearables.
- Liquid sensing – Non-invasive and non-contact liquid sensing capability with AI/ML based processing algorithm in PSOC 4 enables more cost-effective and accurate sensing than mechanical sensors and typical capacitive solutions. It is resistant to environmental factors such as temperature and humidity and can detect liquid levels with up to 10-bit resolution in various shapes of containers. The solution offers even more features that other liquid sensors cannot solve such as foam rejection, residue rejection and reliably work with varying air gaps between sensor and container. Liquid sensing on PSOC 4 brings more intelligence to applications managing liquids such as robot vacuum cleaner, soap dispensing in washing machine, coffee machines, humidifiers, etc.
- CAPSENSE hover touch – Hover touch sensing supports new use cases where a direct touch of a button is not required. Hover touch can eliminate multiple components in certain applications such as springs and gaskets in cooktop touch panels. By bridging the airgap with hover touch, customers achieve significant bill-of-material (BOM) savings, while realizing increased system performance, reduced design complexity, and faster time-to-market.
At embedded world 2025 in Nuremberg this March Infineon will show the capabilities of PSOC 4 Multi-Sense in a demo. Visitors can experience first-hand how inductive and liquid-level sensing uplevels design and functionality of a coffee machine and contributes to the perfect cup of coffee.
Availability
Infineon’s PSOC 4000T with fifth-generation CAPSENSE and new Multi-Sense capability is available now. A second device, the new PSOC 4100T Plus with higher memory and more I/Os, will be Multi-Sense-enabled in the second quarter of 2025, and all subsequent PSOC devices with CAPSENSE will incorporate this technology. The new PSOC 4000T series provides an upgrade path for PSOC 4000, PSOC 4000S and PSOC T 4700S based designs to fifth-generation HMI technology with software and package compatibility. For more information, visit www.infineon.com/multi-sense.
Infineon at embedded world
Embedded world will take place in Nuremberg, Germany from 11 to 13 March, 2025. Infineon will present its products and solutions for decarbonization and digitalization in hall 4A, booth #138 and virtually . For press inquiries please contact media.relations@infineon.com. Industry analysts interested in a briefing can email MarketResearch.Relations@infineon.com.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
PSOC 4000T Multi-Sense
Infineon’s PSOC™ 4 microcontroller family now features Multi-Sense capabilities. Infineon expands its leading capacitive sensing technology CAPSENSETM with a new, proprietary inductive sensing technology, as well as non-invasive and non-contact liquid sensing solution.
JPEG
2126x2004 px
Information Number : INFCSS202503-070
Ulrike Mittereder
Spokesperson Consumer, Compute and Communication, CSS Division
+49 89 234 43951