Pin and Code Wizard

Efficient Pin and Code Configuration Tool for ARM Cortex Microcontrollers

About fmx-pin-and-code-wizard

This Pin and Code Wizard is the tool helps to set the IO ports for 32-bit ARM® Cortex® microcontroller, and it has the following features.

  • After activating the peripherals and GPIOs, which are used, the tool assigns the peripherals to the corresponding pins automatically.
  • Customize easily the result of Pin assignment by graphical user interface.
  • Setting easily the port relocation.
  • The tool outputs the source code according to the Setting of IO port for peripheral library function calls.
  • Generating projects several IDEs.
  • The Pin and Code Wizard has the following advantages:
  • Decrease of the development costs.
  • Usage of the peripherals at their maximum.
  • Software: JRE (Java Runtime Environment) 32bit Version 7 or later
  • OS: Windows7(32bit/64bit) English/Japanese; Windows8(32bit/64bit) English/Japanese
  • Memory: About 1GB or more (Recommended 2GB or more)
  • Hard disk: About 1GB free capacity is required for installation

Note: Above conditions do not guarantee all operation.

This Pin and Code Wizard is the tool helps to set the IO ports for 32-bit ARM® Cortex® microcontroller, and it has the following features.

  • After activating the peripherals and GPIOs, which are used, the tool assigns the peripherals to the corresponding pins automatically.
  • Customize easily the result of Pin assignment by graphical user interface.
  • Setting easily the port relocation.
  • The tool outputs the source code according to the Setting of IO port for peripheral library function calls.
  • Generating projects several IDEs.
  • The Pin and Code Wizard has the following advantages:
  • Decrease of the development costs.
  • Usage of the peripherals at their maximum.
  • Software: JRE (Java Runtime Environment) 32bit Version 7 or later
  • OS: Windows7(32bit/64bit) English/Japanese; Windows8(32bit/64bit) English/Japanese
  • Memory: About 1GB or more (Recommended 2GB or more)
  • Hard disk: About 1GB free capacity is required for installation

Note: Above conditions do not guarantee all operation.

Documents

Design resources

Image gallery

Pin Count Wizard
Pin Count Wizard Pin Count Wizard Pin Count Wizard