- eFuses
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
- Gate Driver ICs for SiC MOSFETs
- Isolated Gate Driver ICs
- Gate driver ICs for GaN HEMTs
- Half-Bridge Gate Driver ICs
- High-Side Gate Driver Ics
- Level-Shift Gate Driver ICs
- Low-Side Gate Driver Ics
- Three-Phase Gate Driver Ics
- Transformer Driver ICs
- Overview
- AC-DC LED driver ICs
- Ballast IC
- DC-DC LED driver IC
- LED dimming interface IC
- Linear LED driver IC
- LITIX™ - Automotive LED Driver IC
- NFC wireless configuration IC with PWM output
- VCSEL driver
- Overview
- BLDC motor drivers
- BDC motor drivers
- Stepper & servo motor drivers
- Motor drivers with MCU
- Bridge drivers with MOSFETs
- Gate driver ICs
- Overview
- Automotive MOSFET
- Dual MOSFETs
- MOSFET (Si & SiC) Modules
- N-channel depletion mode MOSFET
- N-channel MOSFETs
- P-channel MOSFETs
-
Silicon carbide CoolSiC™ MOSFETs
- Overview
- Silicon Carbide MOSFET modules
- Silicon carbide MOSFET discretes
- Silicon carbide MOSFETs bare dies
- 400 V / 440 V Silicon Carbide MOSFETs
- 650 V Silicon Carbide MOSFETs
- 750 V Silicon Carbide MOSFETs
- 1200 V Silicon Carbide MOSFETs
- 2000 V Silicon Carbide MOSFETs
- 2300 V Silicon Carbide MOSFETs
- 3300 V Silicon Carbide MOSFETs
- 1700 V Silicon Carbide MOSFETs
- Small signal/small power MOSFET
- Overview
- IGBT modules
- MOSFET (Si & SiC) Modules
- Intelligent power modules (IPM)
- Diodes and thyristors (Si/SiC)
- Automotive IGBT and CoolSiC™ MOSFET modules
- High density power modules
- Overview
- Automotive transceivers
- Linear voltage regulators for automotive applications
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
May 29, 2026
Business & Financial Press
May 20, 2026
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
May 29, 2026
Business & Financial Press
May 20, 2026
Business & Financial Press
May 11, 2026
Business & Financial Press
May 07, 2026
Infineon and Marelli collaborate to drive innovation in Zone Control Units with AURIX™ TC4x MCU family
Infineon and Marelli collaborate to drive innovation in Zone Control Units with AURIX™ TC4x MCU family
Market News
Munich, Germany – 8 November 2024 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and Marelli, a leading mobility technology supplier to the automotive sector, are working together on the development of advanced E/E architecture solutions. This collaboration combines the two companies' automotive expertise, using Infineon's latest AURIX™ TC4x microcontrollers to develop innovative Zone Control Units (ZCUs). Designed for new E/E architectures, Infineon's AURIX TC4x family extends the functionality of automotive microcontroller units (MCUs) for safe and secured processing. The MCU family supports high-speed communication interfaces such as Multi-Gbit Ethernet and PCI Express, as well as new interfaces such as CAN-XL and 10BASE-T1S. This provides carmakers with outstanding performance, data throughput and flexibility when implementing next-generation E/E architectures.
“Marelli and Infineon have a long history of working together and the joint development of our ZCUs is another significant step forward,” said Ravi Tallapragada, President of Marelli's Electronic Systems business. “With Infineon's contribution, Marelli is well positioned to strengthen its role as a partner to carmakers venturing into zonal architectures. This collaboration allows us to offer market-leading products that enable the implementation of software-defined vehicles and build on our industry-leading position in ZCUs.”
“We are proud of our proven and strong collaboration with Marelli, it underlines our shared commitment to excellence and innovation,” said Lars Wemme, Senior Vice President Product Line ADAS, Chassis, E/E Architecture at Infineon. “With our new microcontrollers, we are helping Marelli drive its innovative solutions and become a pioneer in the growing OEM zone control market.”
By using Infineon's AURIX TC4x, Marelli has built a ZCU platform with important functions that are beneficial for the development of advanced software-defined vehicles:
- Data Routing Engine: Ensures communication with ultra-low latency and improves the efficiency and speed of data transmission in the vehicle.
- Hypervisor Integration: Allows for independent software updates, which are critical to maintaining the latest features without system downtime.
- Lighting Control Software Integration: Enables an innovative lighting control system to be integrated into the ZCU, paving the way for future MCU-less lamps.
The AURIX TC4x is a key enabler for software-defined vehicles, providing strong security performance through an enhanced security cluster and compliance with ISO/SAE 21434. The integrated Data Routing Engine reduces CPU load during data transfers, while the hypervisor acts as a virtualization layer that enables the combination of applications developed on multiple operating system platforms on a single AURIX TC4x platform. This, together with the virtualization-enabled hardware protection mechanism, facilitates the integration of different applications and ensures that each has its own allocated resources and requirements.
Availability
Samples of the AURIX TC4x are now available. Further information is available at www.infineon.com/products/microcontroller/32-bit-tricore/aurix-tc4x/tc4dx.. The latest Marelli ZCU demonstrator built with an AURIX TC4x microcontroller will be showcased at electronica 2024 in Munich from November 12 to 15 (hall C3, booth 502).
Infineon at electronica 2024
At this year's electronica in Munich, Infineon presents innovative solutions for applications that address the challenges of our time. Semiconductors contribute in many ways to the green and digital transformation, helping to shape an all-electric society. At electronica 2024, Infineon offers the opportunity to explore sustainable technologies that are revolutionizing the mobility and automotive landscape, enabling sustainable buildings and smarter living, and promoting the growth of artificial intelligence with minimal ecological impact. The company will present intelligent and energy-efficient solutions for tomorrow's connected world from November 12 to 15 in Hall C3, Booth 502 under the motto “Driving Decarbonization and Digitalization. Together.” More information is available at www.infineon.com/electronica
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Collaboration between Infineon and Marelli
The collaboration between Infineon and Marelli combines the two companies' automotive expertise, using Infineon's latest AURIX™ TC4x microcontrollers to develop innovative Zone Control Units (ZCUs)
JPEG
2126x2004 px
Information Number : INFATV202411-021