- eFuses
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
- Gate Driver ICs for SiC MOSFETs
- Isolated Gate Driver ICs
- Gate driver ICs for GaN HEMTs
- Half-Bridge Gate Driver ICs
- High-Side Gate Driver Ics
- Level-Shift Gate Driver ICs
- Low-Side Gate Driver Ics
- Three-Phase Gate Driver Ics
- Transformer Driver ICs
- Overview
- AC-DC LED driver ICs
- Ballast IC
- DC-DC LED driver IC
- LED dimming interface IC
- Linear LED driver IC
- LITIX™ - Automotive LED Driver IC
- NFC wireless configuration IC with PWM output
- VCSEL driver
- Overview
- BLDC motor drivers
- BDC motor drivers
- Stepper & servo motor drivers
- Motor drivers with MCU
- Bridge drivers with MOSFETs
- Gate driver ICs
- Overview
- Automotive MOSFET
- Dual MOSFETs
- MOSFET (Si & SiC) Modules
- N-channel depletion mode MOSFET
- N-channel MOSFETs
- P-channel MOSFETs
-
Silicon carbide CoolSiC™ MOSFETs
- Overview
- Silicon Carbide MOSFET modules
- Silicon carbide MOSFET discretes
- Silicon carbide MOSFETs bare dies
- 400 V / 440 V Silicon Carbide MOSFETs
- 650 V Silicon Carbide MOSFETs
- 750 V Silicon Carbide MOSFETs
- 1200 V Silicon Carbide MOSFETs
- 2000 V Silicon Carbide MOSFETs
- 2300 V Silicon Carbide MOSFETs
- 3300 V Silicon Carbide MOSFETs
- 1700 V Silicon Carbide MOSFETs
- Small signal/small power MOSFET
- Overview
- IGBT modules
- MOSFET (Si & SiC) Modules
- Intelligent power modules (IPM)
- Diodes and thyristors (Si/SiC)
- Automotive IGBT and CoolSiC™ MOSFET modules
- High density power modules
- Overview
- Automotive transceivers
- Linear voltage regulators for automotive applications
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
- Auxiliary motor control - 12 V DC motor controller
- Auxiliary motor control 48 V
- Automotive e-mirror module
- Door control module
- Roof control module
- Seat comfort module
- Seat control module
- Smart car access
- Smart power closure system
- Smart window control module
- Windshield wiper system
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
- Auxiliary inverter
- Auxiliary inverter - high-voltage (commercial vehicles)
- EV traction inverter
- Traction inverter (electric commercial vehicles)
- Traction inverter (electric two- & three-wheelers)
- DC-DC converter high-voltage
- DC-DC converter high-voltage (commercial vehicles)
- On-board charging (electric commercial vehicles)
- On-board charging (OBC)
- On-board charging (OBC) solutions for electric two- and three-wheelers
- Fuel-cell DC-DC boost converter
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
May 29, 2026
Business & Financial Press
May 20, 2026
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
May 29, 2026
Business & Financial Press
May 20, 2026
Business & Financial Press
May 11, 2026
Business & Financial Press
May 07, 2026
Infineon and Apex.AI are integrating AURIX™ TC3x microcontroller and Apex.Grace to expedite software-defined vehicle development
Infineon and Apex.AI are integrating AURIX™ TC3x microcontroller and Apex.Grace to expedite software-defined vehicle development
Market News
Munich, Germany and Palo Alto, California – 16 March, 2023 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and Apex.AI, a company developing safety-certified software for mobility and autonomous applications, today announced to co-develop a platform that significantly expedites software development for automotive customers. The companies have integrated Apex.AI’s software development kit and Infineon’s AURIX™ TC3X microcontroller to enable faster integration of safety-critical automotive functions into future vehicles.
“The AURIX TC3x is widespread across automotive applications and well known for its reliability, scalable performance and broad customer base,” said Thomas Schneid, Senior Director Software, Partnership & Ecosystem Management from Infineon. “Together with Apex.AI we are now speeding up software development and implementation of microcontrollers to make software-defined vehicles possible. New applications in the car demand new SW Ecosystem components which complement and enhance our existing SW environments”
“The mobility industry is challenged by moving from hardware-centric products to software-defined vehicles. The integration of the Infineon AURIX TC3x microcontroller family, the leading embedded automotive safety controller, with Apex.Grace™ will significantly accelerate development times and lower deployment costs,” said Dr. Jan Becker, Co-founder and CEO of Apex.AI.
Infineon’s AURIX TC3x is one of the major embedded safety controllers worldwide to obtain ASIL D certification according to the 2018 ISO 26262 standard. ASIL D is the highest level of automotive functional safety. Leading computing platforms for automated driving rely on the microcontroller as their safety host controller as it provides the safety and performance necessary to make automated driving happen. Apex.Grace, formerly known as Apex.OS, is the first complete SDK for software-defined vehicles (SDV) certified to ISO 262626 ASIL D.
Apex.Grace is the go-to choice for efficiently developing application software for software-defined vehicles. Apex.Ida, previously known as Apex.Middleware, provides a complete and integrated solution for intra- and inter-electronic control unit (ECU) communication and communication to the cloud. The two companies demonstrate that the development and integration of embedded safety-critical automotive applications can be significantly accelerated.
Apex.Grace is based on the open-source robot operating system (ROS). While ROS is the industry’s de facto development standard for prototyping for robotics and mobility applications, it does not meet safety and reliability requirements for automotive systems and other safety-critical applications, creating a hurdle for manufacturers. Apex.Grace enables the rapid and efficient transition from ROS-based prototypes to production-ready vehicles and is certified by TÜV Nord to ASIL D, the highest level of automotive functional safety.
More information
Infineon and Apex.AI will demonstrate the capabilities of the platform at Apex.AI’s booth (Hall 4, Booth 4-203) at Embedded World 2023 in Nuremberg, Germany, March 14-16, 2023. The companies will showcase the ease of deploying seat belt status notifications across multiple seats in a vehicle. The demo will show how the signals are processed through a vehicle's system, ultimately showcasing how a seatbelt warning is calculated and delivered to the driver. It will illustrate how the development and integration of embedded automotive applications can be significantly accelerated.
About Apex.AI
Apex.AI is a global company that develops secure, certified, developer-friendly, and scalable software for software-defined vehicles and mobility systems. The company's flagship product is Apex.Grace, an automotive-grade, real-time, reliable software development kit. Apex.AI provides automakers, truck manufacturers and suppliers with a software development kit, which helps automotive customers to transition from hardware-centric products to modern software-centric vehicles and develop software faster at a lower cost and with smaller effort. More information about Apex.AI is available at www.apex.ai. To get in touch, please email media@apex.ai.
Infineon at Embedded World
Embedded World will take place from 14 to 16 March, 2023 in Nuremberg, Germany. Infineon will present its products and solutions for decarbonization and digitalization in hall 4A, booth #138 and virtually. Company representatives will also hold several TechTalks as well as presentations at the accompanying Embedded World Conference, followed by discussions with the speakers. If you are interested in interviewing an expert at the show, please email media.relations@infineon.com, industry analyst, email: MarketResearch.Relations@infineon.com.
Press Photos
AURIX TC3x
Infineon and Apex.AI have integrated Apex.AI’s software development kit and Infineon’s AURIX™ TC3X microcontroller to enable faster integration of safety-critical automotive functions into future vehicles.
JPEG
886x838 px
Information Number : INFATV202303-081