- eFuses
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
- AURIX™ family – TC39xXX
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
- Gate Driver ICs for SiC MOSFETs
- Isolated Gate Driver ICs
- Gate driver ICs for GaN HEMTs
- Half-Bridge Gate Driver ICs
- High-Side Gate Driver Ics
- Level-Shift Gate Driver ICs
- Low-Side Gate Driver Ics
- Three-Phase Gate Driver Ics
- Transformer Driver ICs
- Overview
- AC-DC LED driver ICs
- Ballast IC
- DC-DC LED driver IC
- LED dimming interface IC
- Linear LED driver IC
- LITIX™ - Automotive LED Driver IC
- NFC wireless configuration IC with PWM output
- VCSEL driver
- Overview
- BLDC motor drivers
- BDC motor drivers
- Stepper & servo motor drivers
- Motor drivers with MCU
- Bridge drivers with MOSFETs
- Gate driver ICs
- Overview
- Automotive MOSFET
- Dual MOSFETs
- MOSFET (Si & SiC) Modules
- N-channel depletion mode MOSFET
- N-channel MOSFETs
- P-channel MOSFETs
-
Silicon carbide CoolSiC™ MOSFETs
- Overview
- Silicon Carbide MOSFET modules
- Silicon carbide MOSFET discretes
- Silicon carbide MOSFETs bare dies
- 400 V / 440 V Silicon Carbide MOSFETs
- 650 V Silicon Carbide MOSFETs
- 750 V Silicon Carbide MOSFETs
- 1200 V Silicon Carbide MOSFETs
- 2000 V Silicon Carbide MOSFETs
- 2300 V Silicon Carbide MOSFETs
- 3300 V Silicon Carbide MOSFETs
- 1700 V Silicon Carbide MOSFETs
- Small signal/small power MOSFET
- Overview
- IGBT modules
- MOSFET (Si & SiC) Modules
- Intelligent power modules (IPM)
- Diodes and thyristors (Si/SiC)
- Automotive IGBT and CoolSiC™ MOSFET modules
- High density power modules
- Overview
- Automotive transceivers
- Linear voltage regulators for automotive applications
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
- Automotive body electronics & power distribution
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
- Multicopters and drones
- AR and smart glasses
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
- Photovoltaic
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
- Automotive auxiliary systems
- Automotive gateway
- Automotive power distribution
- Body control modules (BCM)
- Comfort & convenience electronics
- Auxiliary motor control - 12 V DC motor controller
- Auxiliary motor control 48 V
- Automotive e-mirror module
- Door control module
- Roof control module
- Seat comfort module
- Seat control module
- Smart car access
- Smart power closure system
- Smart window control module
- Windshield wiper system
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
- EV inverters
- EV power conversion & OBC
- FCEV powertrain system
- Auxiliary inverter
- Auxiliary inverter - high-voltage (commercial vehicles)
- EV traction inverter
- Traction inverter (electric commercial vehicles)
- Traction inverter (electric two- & three-wheelers)
- DC-DC converter high-voltage
- DC-DC converter high-voltage (commercial vehicles)
- On-board charging (electric commercial vehicles)
- On-board charging (OBC)
- On-board charging (OBC) solutions for electric two- and three-wheelers
- Fuel-cell DC-DC boost converter
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
- Durable healthcare equipment
- Disposable healthcare equipment
- Healthcare wearables
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
- DRIVECORE for automotive software development
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
May 29, 2026
Business & Financial Press
May 20, 2026
Business & Financial Press
May 11, 2026
Business & Financial Press
May 07, 2026
- Company
- Our stories
- Events
- Press
- Investor
- Careers
- Quality
- Latest news
Business & Financial Press
May 29, 2026
Business & Financial Press
May 20, 2026
Business & Financial Press
May 11, 2026
Business & Financial Press
May 07, 2026
What is a MOSFET?
Learn more about power MOSFET basics, structure, operation modes and key work principles
A MOSFET (Metal Oxide Semiconductor Field Effect Transistor) is a semiconductor device that is typically used as a voltage-controlled switch.
It comprises three terminals: the gate, the drain, and the source. The main purpose of the MOSFET is to efficiently deliver power to a load.
A MOSFET is a voltage controlled device composed of a gate, a source and a drain. The gate voltage is typically provided by a microcontroller or a driver IC.
By applying the gate voltage to the gate terminal, the current will start to flow from the source to the drain terminals.
To understand the efficiency of the current flow, we can take a look at the RDS(on) rating of the device. The RDS(on) is the resistance from the source terminal to the drain terminal when the device is on. This rating is measured in ohms or milliohms.
There are two different MOSFET modes, the enhancement and the depletion. Both of these modes have two channel types, the N-channel, and the P-channel. The enhancement mode means that the device is always off, and needs a gate voltage to turn on.
On the other hand, the depletion mode means that the device is always on, and needs a gate voltage to turn off. Nowadays, the most commonly used MOSFETs are N-channel enhancement-type devices.
MOSFETs can also be lateral or vertical when it comes to their structure, which means that the conducting channel of the MOSFET is either lateral or vertical.
In the lateral structure, all three terminals are on top, on the same side of the silicon die.
It is very common for planar-type MOSFETs and it may also still be used nowadays for low-power MOSFETs, such as small signal types.
In vertical-type MOSFETs, the gate and source terminals are usually on top, on the same side of the die, while the drain terminal is on the vertically opposite side, as you can see here.
This type of structure is known as a trench MOSFET, and it is the most used design by MOSFET suppliers today. For example, CoolMOS™, OptiMOS™, and StrongIRFET™ are all vertical-type trench MOSFETs.
Let‘s use the N-type enhancement mode planar MOSFET to deep dive into the MOSFET structure. The most important element is the metal oxide semiconductor interface because it is responsible for its operation. Here, you can see the detailed structure of an N-type enhancement mode planar MOSFET.
The basis of the MOSFET construction is a silicon material that is lightly doped with Boron atoms to make it slightly P-type in concentration. This is called the p-substrate. To build the source and the drain regions, high-energy and high-concentration implants of N-type atoms are used.
The gate oxide, which is built with thin oxide, is on the silicon region between the source and the drain, partially overlapping these regions. When the gate voltage is applied, the negative atoms are attracted under the gate and the N-channel is formed. At this moment, the current will begin to flow.
Please note that other manufacturing steps may vary depending on the MOSFET type. Nevertheless, these are the basic operational building blocks of a MOSFET.
MOSFETs operate in three different modes: Depletion, Accumulation and Inversion.
These modes refer to the status of the MOSFET channel and are described below:
Depletion mode
The depletion mode refers to the MOSFET in the off state. That is when the voltage of the gate is lower than the gate threshold voltage.
The gate threshold voltage is the minimum voltage required to form the channel between the drain and the source terminals.
So, when the gate voltage is lower than the gate threshold voltage, a depletion is formed between the drain and the source and the MOSFET is in the off state. This way, no current will flow.
Accumulation mode
The accumulation mode happens when the gate voltage increases above zero but is still lower than the threshold voltage. This occurs at the beginning of the channel formation due to the positive gate voltage.
Note that there may be a very small sub-threshold or leakage current occurring in the channel! Here, an inversion layer begins to form, where the polarity of the P-substrate under the gate starts changing.
Inversion mode
The inversion mode has two types of operation:
› Triode or linear mode
› Saturation mode
Let’s start by focusing on the first one. In this operation mode, the current increases in a linear way with the applied drain voltage.
In this case, the gate voltage is higher than the gate threshold voltage. The inversion layer increases and the N-channel is formed between the drain and the source terminals, which means that the current will flow. This current is proportional to the gate and drain voltage, which is higher than zero.
On the other hand, the saturation mode occurs when the current through the device starts to level off or flatten.
This happens because the current cannot increase in a linear way for a long period of time with the applied drain voltage.
When the drain voltage reaches a value equal to the difference between the gate voltage and the threshold voltage, the conducting channel becomes “pinched off”, and the current will remain constant.
This “pinch off” occurs due to the reverse biasing effect on the drain terminal caused by the increase in the drain voltage.
On the right are typical datasheet curves related to the linear and saturation modes, where we can see the relationship between voltage and the output current.
By analyzing this graph, we can see the relation between the drain-source current and the drain-source voltage, applied for different values of the gate to source voltage.
Here, the dotted line indicates the edge of the saturation boundary, until the current increases linearly with the applied drain voltage. When this limit is exceeded, the drain current remains more or less constant with the increasing drain voltage.
By analyzing this graph, we can see the relation between the drain-source current and the drain-source voltage, applied for different values of the gate to source voltage.
Here, the dotted line indicates the edge of the saturation boundary, until the current increases linearly with the applied drain voltage. When this limit is exceeded, the drain current remains more or less constant with the increasing drain voltage.
Additionally, this graph shows the relation between the drain current and the applied gate voltage for a fixed value of the drain voltage.
As you can see, the current quickly increases once the gate voltage is higher than the threshold voltage.
Please note that there is some amount of current flow before the threshold voltage is reached. This is called subthreshold current or leakage current.