- eFuses
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
- TC39xXX/XP
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
- Gate Driver ICs for SiC MOSFETs
- Isolated Gate Driver ICs
- Gate driver ICs for GaN HEMTs
- Half-Bridge Gate Driver ICs
- High-Side Gate Driver ICs
- Level-Shift Gate Driver ICs
- Low-Side Gate Driver ICs
- Three-Phase Gate Driver ICs
- Transformer Driver ICs
- Overview
- AC-DC LED driver ICs
- Ballast IC
- DC-DC LED driver IC
- LED dimming interface IC
- Linear LED driver IC
- LITIX™ - Automotive LED Driver IC
- NFC wireless configuration IC with PWM output
- VCSEL driver
- Overview
- BLDC motor drivers
- BDC motor drivers
- Stepper & servo motor drivers
- Motor drivers with MCU
- Bridge drivers with MOSFETs
- Gate driver ICs
- Overview
- Automotive MOSFET
- Dual MOSFETs
- MOSFET (Si & SiC) Modules
- N-channel depletion mode MOSFET
- N-channel MOSFETs
- P-channel MOSFETs
-
Silicon carbide CoolSiC™ MOSFETs
- Overview
- Silicon Carbide MOSFET modules
- Silicon carbide MOSFET discretes
- Silicon carbide MOSFETs bare dies
- 400 V / 440 V Silicon Carbide MOSFETs
- 650 V Silicon Carbide MOSFETs
- 750 V Silicon Carbide MOSFETs
- 1200 V Silicon Carbide MOSFETs
- 2000 V Silicon Carbide MOSFETs
- 2300 V Silicon Carbide MOSFETs
- 3300 V Silicon Carbide MOSFETs
- 1700 V Silicon Carbide MOSFETs
- Small signal/small power MOSFET
- Overview
- IGBT modules
- MOSFET (Si & SiC) Modules
- Intelligent power modules (IPM)
- Diodes and thyristors (Si/SiC)
- Automotive IGBT and CoolSiC™ MOSFET modules
- High density power modules
- Overview
- Automotive transceivers
- Linear voltage regulators for automotive applications
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
- Automotive body electronics
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
- Automotive zonal architecture
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
- Auxiliary inverter
- Auxiliary inverter - high-voltage (commercial vehicles)
- EV traction inverter
- Traction inverter (electric commercial vehicles)
- Traction inverter (electric two- & three-wheelers)
- DC-DC converter high-voltage
- DC-DC converter high-voltage (commercial vehicles)
- On-board charging (electric commercial vehicles)
- On-board charging (OBC)
- On-board charging (OBC) solutions for electric two- and three-wheelers
- Fuel-cell DC-DC boost converter
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
- DRIVECORE™ for automotive software development
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
Jun 03, 2026
Business & Financial Press
Jun 03, 2026
Business & Financial Press
May 29, 2026
Business & Financial Press
May 20, 2026
- Company
- Our stories
- Events
- Press
- Investor
- Careers
- Quality
- Latest news
Business & Financial Press
Jun 03, 2026
Business & Financial Press
Jun 03, 2026
Business & Financial Press
May 29, 2026
Business & Financial Press
May 20, 2026
Infineon joins EEBus Initiative e.V., supporting the standardization for energy management systems
Infineon joins EEBus Initiative e.V., supporting the standardization for energy management systems
Market News
Munich, Germany – 4 October, 2022 – One key way to address the global trends of an increasing share of volatile renewable energy sources and a growing electrification in mobility is to improve system integration of electricity consumers from all sectors. Implementation requires holistic thinking: from green power generation to a stable and efficient grid infrastructure to storage and consumption. Bidirectional charging contributes significantly to this by, for example, allowing the electricity stored in the battery of an electric vehicle to be used to supply the power grid or electrical appliances in the home when needed. However, energy generators and consumer devices need a standardized language to be able to communicate.
As solution provider, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is interested in a standardized communication flow for the complete chain of energy control. Therefore, the company has joined EEBus, an initiative that promotes the standardization of interfaces to enable uniform communication between power generator and end user devices. The initiative brings together international companies and associations from different sectors such as energy relevant devices and systems, energy supply and grid operation, and information and communication technology. Infineon is the first semiconductor company to join the initiative.
“This principle of an unified energy eco-system has been the basic philosophy of the EEBus Initiative from the very beginning. We offer an open solution for all market participants instead of another proprietary isolated solution,” said Dr. Robert Böhm, Managing Director from EEBus Initiative e.V. “With EEBus we develop and standardize a dynamically flexible interface on behalf of the industry and provide a global standard for communication.”
“The continuous and collaborative coordination of members in working groups at eye level is creating a unified and vendor-independent communication solution which is essential for bidirectional charging and a decentralized power grid,” said Andreas Urschitz, Chief Marketing Officer of Infineon. “With EEBus' special focus on energy management, bidirectional end user devices can be integrated into the Smart Grid, easy and efficiently.”
EEBus as a uniform standard
EEBus is a manufacturer-independent and standardized language for the exchange of energy and application-relevant information that can be used free of charge. The standards-based language enables the proper functioning of all devices even during energy shortages and the provision of plug-and-play solutions for residential and commercial applications.
The EEBus Initiative distinguishes generally between content, namely the data model that is transmitted, and the type of transmission respectively the communication path. The EEBus data model “SPINE” (Smart Premises Interoperable Neutral-Message Exchange) can be transported via many communication paths and protocols. One possible transport protocol is the IP-based “SHIP” (Smart home IP) which is based on widely-used RFCs and can be used in existing IP infrastructure. To guarantee maximum flexibility, the EEBus architecture is based on the Smart Grid Architecture Model (SGAM) and offers solutions for several layers.
Regardless of previously used communication technologies or industry affiliation, companies can use SPINE to offer their services or platforms and potentially control millions of energy relevant devices or, as device manufacturers, smartly and interoperably connect their own products to a larger eco-system. More information about the EEBus Initiative e.V. is available at www.eebus.org.
More information about Infineon’s contribution to energy efficiency: www.infineon.com/green-energy
Press Photos
Standards Smart Home
As solution provider, Infineon is interested in a standardized communication flow for the complete chain of energy control. Therefore, the company has joined EEBus, an initiative that promotes the standardization of interfaces to enable uniform communication between power generator and end user devices.
JPEG
1240x689 px
Photo of Andreas Urschitz
Andreas Urschitz, Chief Marketing Officer of Infineon
JPEG
500x600 px
Information Number : INFXX202210-001