- XELOC™ - Consumer/Industrial Ultra-Wide Band Solutions
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
TRUSTECH 2021: SECORA™ ID with FIDO® enables flexible and fast security solutions for online authentication
TRUSTECH 2021: SECORA™ ID with FIDO® enables flexible and fast security solutions for online authentication
Market News
Munich, Germany, and Paris, France – 29 November, 2021 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is presenting the SECORA™ ID with FIDO® for secured authentication to online portals with user-friendly tokens. The leading security solution actively protects from tampering and fraud. Additionally, the company will showcase other products of the SECORA family of one-stop solutions at this year's TRUSTECH from November 30 to December 2 at Paris Expo Porte de Versailles in Pavilion 5.2.
SECORA ID with FIDO for online authentication
Based on FIDO, Infineon's latest addition to the SECORA ID portfolio makes it easy to enhance security of digital identities. The solution utilizes the open industry standard and provides a simple, reliable and secured method for online authentication. In combination with an electronic identity document (eID), FIDO can also be used by citizens to authenticate themselves to government portals and access their services. The solution is implemented on an EAL6+ certified security controller and a Java Card™ operating system. Being certified by the FIDO Alliance as a roaming authenticator, it supports FIDO's CTAP2 protocol, which enables 2-factor and multifactor authentication via the NFC interface. As a versatile offering, available both as a standalone product as well as in combination with the eMRTD applet, it will cover all markets – consumer, enterprise and eGov applications.
Secured access to blockchains with SECORA Blockchain
In numerous use cases in industries such as logistics, automotive, and energy, the blockchain technology helps to track supply chains, protect brands, prove asset ownership, and manage contracts. However, to add transactions to a blockchain, the users usually need a private key that must be kept in a secured area. Such a secured "vault" for storing private keys is enabled by SECORA Blockchain security controllers, protecting access to blockchains. The SECORA Blockchain demo at the TRUSTECH 21 shows how to protect brands integrating a SECORA Blockchain chip into the products, and then link it to the blockchain to prove that the products are genuine.
Connected Payments for wearables and IoT devices with SECORA Connect
Payment wearables and smart IoT devices in different form factors are becoming increasingly popular as additional functions such as ticketing and access are added. With SECORA Connect, Infineon's solution family for connected IoT devices, it is easy to secure payments and enable convenient biometric authentication. Based on an enhanced NFC Secure Element design, SECORA Connect enables smart wearables with payment, ticketing and other applications at the lowest power consumption, maximizing battery life for consumers. SECORA Connect is a complete turnkey solution that enables users to securely store, select and use multiple credentials such as payment cards and tickets. It turns wearables or IoT devices instantly into powerful and versatile digital wallets.
SECORA Pay enables fast and efficient payment
The SECORA Pay family offers customized, cost-effective Java Card™-based solutions for fast and agile implementation in payment card and innovative form factors. The product family is based on a SOLID FLASH chip platform from Infineon and supports the latest EMV applets. To expand the offering, a new SECORA Pay portfolio based on the latest 40nm technology platform has been added to the family. The solutions are available in three different flavors to support efficient card production for different use cases:
- SECORA Pay S: ready-to-go, off-the-shelf, optimized EMV solutions with reference approvals from major global payment schemes (VISA, Mastercard, Discover and American Express) as well as personalization scripting support
- SECORA Pay X: an enablement platform giving customers flexibility to support EMV-based payment schemes and local content in combination with Infineon’s ready-to-use reference solutions
- SECORA Pay W: turnkey EMV solutions based on innovative packaging technologies to support non-connected, passive wearables or payment accessories.
Availability
Engineering samples for the SECORA ID with FIDO are now available. Mass production is planned to start in April 2022. More information is available at www.infineon.com/secora-id.
Infineon at TRUSTECH 2021
Come and visit Infineon at this year’s TRUSTECH from 30 November to 2 December at the Paris Expo Porte de Versailles in Pavilion 5.2. Dive into the heart of security with Infineon’s SECORA™ family of one-stop solutions. With multiple flavors targeted at the full range of today’s and tomorrow’s use cases, SECORA™ covers everything from smart device and wearable payments through identification and access to blockchain-enabled asset and brand protection. At TRUSTECH 21, discover how all this – and more – is packed into one innovative product family.
Press Photos
SECORA™ use cases
SECORA™ ID, SECORA Blockchain, SECORA Connect, and SECORA Pay: Infineon will showcase its family of one-stop security solutions at TRUSTECH 2021 from 30 November to 2 December at Paris Expo Porte de Versailles in Pavilion 5.2.
JPEG
2126x1256 px
Information Number : INFCSS202111-023