LDO, a low dropout voltage regulator, is a linear voltage regulator designed to operate with a very small difference between the input and output voltage. An LDO voltage regulator is a semiconductor voltage regulator that are easy to design and use. Typically, the dropout voltage is in the range of 100-200 millivolts which is lower than the traditional linear voltage regulators.
A linear regulator plays a crucial role in electronic devices by providing a stable and regulated output voltage to systems, mainly from the power supplied by the battery. This is achieved through a process called voltage regulation, where the linear voltage regulator adjusts its output voltage to maintain a constant level, despite changes in the input voltage or load current. The output voltage is ideally stable with line and load variations, immune to changes in ambient temperature, and stable over time.
- Stability with line variations - The term line variation or line regulation states that the output voltage will remain stable even when the input voltage or line voltage changes.
- Stability with load variations - The term load regulation or load variation states that output voltage will remain stable even when the load current changes.
- Stability over time - The output voltage will remain stable over a long period, without any significant drift or degradation.
- Immunity to temperature changes - The output voltage will remain stable over a wide range of ambient temperatures.
LDO voltage regulators are key components in any power management system and require a ripple-free and stable power supply. The primary function of an LDO voltage regulator (low drop out regulator) is to provide a stable, regulated output voltage from a varying input voltage source.
- Voltage reference - The voltage reference is usually a bandgap reference or a Zener diode-based reference. It is a critical component that provides a stable reference voltage, which is used as a benchmark to regulate the output voltage.
- Error amplifier - The error amplifier amplifies the difference between the two voltages, generating an error signal that drives the series pass element. The amplifier compares the output voltage (fed back through the feedback voltage divider) with the reference voltage
- Feedback voltage divider - It provides a feedback path from the output voltage to the error amplifier. The divider network scales down the output voltage to a level that can be compared with the reference voltage.
- Series pass element (PMOS Transistor) - It is usually a bipolar or CMOS (Complementary Metal-Oxide-Semiconductor) transistor that controls the output current. PMOS is a high-current device that typically handles the load current. The error amplifier controls the gate voltage of the PMOS transistor, which in turn regulates the output current. The output current is controlled by a PMOS (p-channel metal–oxide–semiconductor) transistor, which in turn is controlled by an error amplifier.
There are three different types of LDO voltage regulators (Low Drop Out regulator) or each with its own unique characteristics and applications.
Infineon’s OPTIREG™ linear portfolio includes a range of products with the optimized input voltage range for post regulation. Since these products are used after a pre switch mode converter it is referred to as a post regulator.
Linear post regulators are known for their high-power supply rejection ratio (PSRR) and low output noise. They are designed to provide a low-noise, low-ripple output voltage. They are used as a "post-regulator" to further regulate the output voltage of a switching regulator or another voltage source. Linear post regulators are typically used in applications that require a high degree of voltage regulation.
All voltage tracker products implement various protection features, such as: Under/Over-Voltage, Over-Temperature, Reverse-Polarity, and Reverse-Current. Together with robust design implementation and AECQ100 grade package voltage tracker is the perfect solution to protect the sensor and ECU in a harsh environment.
They are known for their high accuracy and ability to track the reference voltage over a wide range of input voltages. Voltage trackers are often used in battery-powered devices, where the output voltage needs to track the battery voltage to ensure efficient power management. These LDOs regulators are designed to track a reference voltage, typically used in applications that require a voltage that is proportional to a reference voltage.
Infineon’s OPTIREG™ linear High Performance LDOs are state-of-the-art, ultra-low quiescent current LDO regulators that have a wide input voltage range to ensure usage in automotive applications that are permanently connected to the battery and under cranking conditions.
High power LDO regulators are used in high-reliability applications that require a high degree of voltage regulation, low noise, and high-power supply rejection ratio (PSRR). They are known for their high accuracy high PSRR, and low output noise. These regulators provide high-performance, low dropout voltage regulation solutions, idle for applications such as aerospace, automotive, and medical devices.
LDO voltage regulators offer several benefits that make them a popular choice in many power management applications.
- Simplest design with minimal external components.
- Fast load transient response.
- No ripple, low noise, better noise rejection
- Efficiency is high if the difference between input and output voltages is small.
- Low cost compared to DCDC converters.
- High Power Supply Rejection Ratio (PSRR).
- High accuracy, reliability, and flexibility
LDO regulators (Low Dropout Regulator) have a wide range of applications in various industries due to their ability to provide a stable and regulated output voltage, even with a low input voltage These liner voltage regulators are also used to reduce power consumption, noise, and heat generation, making them ideal for battery-powered devices and other low-power applications.
- Portable Electronics- LDO voltage regulators are idle for application such as Smartphones and tablets, Laptops and notebooks, Cameras and camcorders, MP3 players and portable audio devices.
- Industrial and Automation- LDO voltage regulators are used in automation applications such as Process control systems, Industrial automation systems, Motor control systems, and Power supplies for industrial equipment.
- Medical Devices- Linear voltage regulators or LDO regulators are used in medical applications such as medical imaging equipment, Patient monitoring systems, Portable defibrillators, Medical diagnostic equipment.
- Aerospace and Defense- LDO voltage regulators are idle for applications such as Avionics systems, Radar and communication systems, Navigation systems, Power supplies for military equipment.
- Automotive Systems- LDO regulators are used in Infotainment systems, Navigation systems, Automotive sensors and control systems, and Power supplies for automotive electronics.
- Internet of Things (IoT) Devices- Smart home devices, Wearable devices, IoT sensors and gateways, and Power supplies for IoT devices are some of the IOT applications of linear voltage regulators
- Telecommunications- LDO voltage regulators are idle for telecommunication application such as Network infrastructure equipment, Telecommunication switches and routers, Power supplies for telecommunication equipment, Base stations and cell towers.
- Computing and Storage- Servers and data centers, Storage systems and arrays, Power supplies for computing equipment, Cloud computing infrastructure are some of the computing and storage applications of LDO voltage regulators or LDO regulators.