- Linear voltage regulators for automotive applications
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
May 20, 2026
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
May 20, 2026
Business & Financial Press
May 11, 2026
Business & Financial Press
May 07, 2026
Quarterly Report
May 06, 2026
CIS launches USB 3.2 cameras powered by Infineon’s EZ-USB™ controllers for enhanced data transfer and performance
CIS launches USB 3.2 cameras powered by Infineon’s EZ-USB™ controllers for enhanced data transfer and performance
Market News
Munich, Germany – 17 June 2025 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) provides its EZ-USB™ FX10 and FX5 controllers to CIS Corporation for its new USB 5 Gbit/s and 10 Gbit/s camera. These next-generation devices build on the EZ-USB FX3, a widely adopted USB peripheral controller, by adding support for high-speed USB 10 Gbit/s and LVDS interfaces. This advancement increases total data bandwidth by up to 275 percent compared to the previous generation, enabling significantly faster data transfer and improved system performance.
“We are proud to support CIS in bringing next-generation products to the market with our EZ-USB controllers,” says Ganesh Subramaniam, Senior Vice President of Wired Connectivity Solutions at Infineon. “By combining high data throughput, low power consumption, and flexible connectivity, our solutions enable customers to develop advanced USB 3.2 products with shorter time-to-market and compact form factors. The collaboration with CIS is an excellent example of how our technology is driving innovation in emerging data-intensive applications across various industries.”
The EZ-USB FX10 features dual Arm® Cortex®-M4 and M0+ cores, 512 KB of flash memory, 128 KB of SRAM, 128 KB of ROM, and seven serial communication blocks (SCBs). It includes a cryptography accelerator and a high-bandwidth data subsystem that enables direct memory access (DMA) transfers between LVDS/LVCMOS interfaces and USB ports at speeds of up to 10 Gbit/s. An additional 1 MB of SRAM supports USB data buffering. The controller also offers USB-C connection detection and flip-mux functionality, removing the need for external logic components. This combination of processing power, interface flexibility, and integrated features supports a wide range of high-speed USB applications.
With the introduction of its new USB 3.2 cameras, CIS aims to expand beyond the industrial image processing market into sectors such as logistics, robotics, medical technology, and life sciences – areas where connectivity, speed, image quality, and compact design are critical. Product samples are already finalized, and mass production is scheduled to begin in July. In addition, CIS is expanding its portfolio with new camera models across multiple resolutions.
“We are developing models with 3M, 5M, 4K/8M, and 20M pixel sensors based on EZ-USB FX5 and FX10,” says Yusuke Muraoka, President of CIS Corporation. “Thanks to Infineon’s support, we expect to complete development in a relatively short time – despite having no prior experience with USB 3.2 technology, which makes this achievement particularly noteworthy.”
The upcoming 4K version of the camera integrates CIS’s proprietary Clairivu™ image signal processor (ISP). Despite this added complexity, the low power dissipation of EZ-USB FX5 and FX10 allows the device to fit into a compact 29 mm cubic housing – reducing the volume by approximately 50 percent compared to CIS’s previous 4K model. Combined with plug-and-play USB connectivity, this compact design greatly enhances the camera’s versatility and ease of integration.
Availability
The EZ-USB FX10 is available now. Further information is available at www.infineon.com/ez-usb-fx10.
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
CIS camera
Infineon EZ-USB™FX10 and FX5 controllers power new CIS USB 5 Gbit/s and 10 Gbit/s cameras, enhancing data transfer and performance
JPEG
2126x2126 px
Information Number : INFPSS202506-118
Michael Burner
Spokesperson Consumer, Compute and Communication, PSS Division
+49 89 234 39300