A CAN transceiver, or Controller Area Network transceiver, is an electronic device used in automotive and industrial applications to permit communication between various electronic control units (ECUs) within a network. It is the interface between the controller and the CAN bus, translating the logic level messages from the controller into the CAN differential scheme on the CANH and CANL pins.
The CAN transceiver is an integrated circuit that interfaces the CAN protocol controller (microcontroller or other device) and the physical two-wire CAN bus. It ensures that signals are transmitted and received accurately, providing the necessary voltage levels and protection against electromagnetic interference.
In this Glossary, Infineon discusses an overview of CAN transceiver:
- How does a CAN transceiver work?
- Types of CAN transceivers?
- What are the key features of a CAN transceiver?
- What are the benefits of using a CAN transceiver?
- CAN transceiver Applications
The transceiver also manages features such as bus biasing, wake-up patterns, and fault confinement, contributing to the reliability and robustness of the overall CAN network.
The CAN transceiver manages the communication interface between the microcontroller and the CAN bus. It serves as a vital component in a CAN (Controller Area Network) network, facilitating the exchange of data between the microcontroller and the physical bus. The transceiver operates by translating digital signals from the microcontroller into a form suitable for transmission over the CAN bus.
CAN transceivers follow CAN protocol. The CAN communications protocol, ISO-11898: 2003, describes how information is passed between devices on a network and conforms to the Open Systems Interconnection (OSI) model that is defined in terms of layers. Actual communication between devices connected by the physical medium is defined by the physical layer of the model.
CAN bus is an asynchronous half-duplex communication protocol; thus, the CAN controller has TXD and RXD pins that are used for the transmission and reception of data, respectively. These pins are connected to the CAN transceiver for converting the digital signals to differential signals for the transmission of messages on the bus and vice-versa for the reception.
The table below summarizes the types of CAN transceivers, along with their key features and typical applications:
This table provides a clear overview of the distinct types, their key features, and typical applications, facilitating easy comparison and understanding of their respective capabilities and use cases.
CAN stands for Controller Area Network. It was developed by Robert Bosch in 1986 as a flexible, reliable, and robust solution for communication within the automotive vehicle. It is a serial half-duplex asynchronous communication protocol and follows a decentralized communication infrastructure.
The key features of a CAN (Controller Area Network) transceiver include:
- Signal Conditioning: The transceivers are designed to condition and amplify signals, ensuring reliable and robust communication over the CAN bus.
- Level Shifting: They incorporate level shifting capabilities to interface between the low-voltage logic of microcontrollers and the higher voltage levels on the CAN bus, enabling seamless compatibility.
- Protection Circuitry: The transceivers often include protection circuitry, such as overvoltage protection and electrostatic discharge (ESD) protection, to safeguard the network from electrical faults and transient events.
- Fail-Safe Operation: Many transceivers feature fail-safe operation, which ensures that the network can continue to function in the event of a fault or communication disruption.
- Isolation (in some cases): In applications requiring galvanic isolation, certain transceivers integrate isolation features to provide protection against electrical noise and ground potential differences.
- Diagnostic and Fault Detection: Some transceivers offer diagnostic capabilities and fault detection mechanisms, allowing for the monitoring and identification of network issues.
Using a CAN (Controller Area Network) transceiver offers several benefits, including:
- Robust Communication: It enable robust and reliable communication over the CAN bus, ensuring data integrity and fault tolerance in challenging environments.
- Noise Immunity: They provide high noise immunity, allowing for consistent communication even in electrically noisy industrial or automotive environments.
- Low Power Consumption: Many CAN transceivers are designed for low power consumption, making them suitable for battery-powered or energy-efficient applications.
- Fault Detection and Diagnostics: Some transceivers include features for fault detection and diagnostics, allowing for efficient troubleshooting and maintenance of the CAN network.
- Protection Circuitry: Integrated protection circuitry, such as overvoltage and ESD protection, safeguards the network from electrical faults and transient events, enhancing overall reliability.
- Temperature and Environmental Robustness: They are often designed to withstand a wide temperature range and harsh environmental conditions, making them suitable for diverse application scenarios.
- Compatibility and Interoperability: They offer seamless interfacing with microcontrollers and other CAN devices, ensuring compatibility and interoperability within the network.
- Cost-Effective Communication: It provides a cost-effective solution for establishing communication networks, particularly in applications where dedicated wiring for communication is impractical.
- Scalability: They allow for scalable deployment and expansion of CAN networks, accommodating additional nodes and communication requirements as needed.
- Standard Compliance: They adhere to industry standards such as ISO 11898 for CAN, ensuring conformity and compatibility with existing CAN-based systems.
CAN transceivers find applications in various industries and systems where robust and reliable communication over the Controller Area Network (CAN Network) bus. Some common applications include:
- Automotive Systems
- Industrial Automation
- Commercial Vehicles
- Medical Devices
- Avionics and Aerospace
- Marine and Off-Highway Vehicles
- Home Automation and Building Management
- Renewable Energy Systems
These diverse applications highlight the versatility and importance in enabling reliable and efficient communication and control within a wide range of systems across different industries.