image-hero

Register or log in to access our webinar recording

Steer-by-wire eliminates the traditional mechanical connection between the steering wheel and the road wheels. Instead of a steering column, the steering wheel actuator's sensors capture driver intent and send it electronically to the road wheel actuator, and vice versa, providing road condition feedback to the driver. The result is a smarter, more adaptable system — with no physical link required.

 

But this is more than a steering story. The demo featured in this video is built on a reference design that scales across chassis applications, from electromechanical braking to active suspension. The demo software environment is also fully tunable, giving you the ability to adapt and fine-tune parameters to match specific motor configurations and steering feel/ratio requirements.

 

Register now to watch the 10-minute Steer-by-Wire breakdown

  • Understand how steer-by-wire actually works — from driver input to wheel movement, including how sensors, actuators, and software replace the steering column
  • See it in action — follow two engineers as they demonstrate a working system and explain the technology in real terms
  • Learn how variable steering ratios improve both safety and comfort — and how the system adapts behavior from low-speed maneuvering to highway driving
  • Discover how road feel is simulated — and why customizable steering feedback is key to driver confidence
  • Get the essentials on safety and redundancy — including how dual data paths and redundant power supplies keep the system reliable and road-ready
Laura Indraccolo
Laura Indraccolo
Laura Indraccolo

System Application Engineer - Chassis & ADAS

Hugo joined Infineon in 2018 after completing his master's thesis at a leading European automotive OEM. He began his career as a member of the AURIXTM microcontroller support team, where he specialized in ADAS & Radar applications and DSP low-level optimizations. Hugo further developed his expertise in Radar technology during his time at Infineon's 60 GHz Radar department. Currently, he is the System Application Engineer for chassis & ADAS applications in the EMEA region, leveraging his technical expertise to drive innovation and support customers.

Johannes Buchhold
Johannes Buchhold
Johannes Buchhold

Field Application Engineer

Matthias Marquardt has spent over a decade in the automotive semiconductor industry, evolving from a Microcontroller Field Application Engineer since 2012 into a specialized Functional Safety System Application Engineer. His recent transition to System Architect for Chassis Microcontrollers builds upon a deep technical foundation in safety-critical embedded systems and real-time control applications. He has successfully assisted numerous high-stakes customer projects, ensuring rigorous compliance with functional safety standards while delivering robust system solutions. Currently serving as the technical lead for the strategic partnership with Arnold NextG, he drives innovation in next-generation chassis control architectures. His career is defined by a consistent track record of bridging complex hardware capabilities with evolving customer requirements to deliver reliable, safety-first automotive systems.

 

Webinar related documents
Steer-by-Wire 10 Minute Breakdown
May 13, 2026
00:00 ( CET )