Bringing EV charging everywhere
Infineon’s SiC-based power modules enable the infrastructure for fast, efficient, and convenient EV charging
May 29, 2025
Most of what we use and do every day relies on mobility. Whether it is commuting to work or delivering packages across the country – nearly everything gets from point A to B by road. And almost all that traffic still runs on gasoline. Electric vehicles hold the promise of cleaner, greener transportation – but there is a catch. Charging needs to feel just as simple, fast, and convenient as refueling, and terminals need to be as prevalent as gas stations – no matter where you live.
For people like Philipp at South Tyrol’s Alpitronic, that challenge is deeply personal. He is working to make EV charging just as fast and seamless as a trip to the gas station – whether you are in the hustle and bustle of a major metropolis or amidst the awe-inspiring beauty of the Tyrolean alps.
To make Philipp’s vision a reality, his team is building ultra-fast, compact chargers that fit just about everywhere and power up EVs in mere minutes. Modern electric vehicles can now charge to 80 percent in around 10 to 15 minutes. But that kind of speed only works with the right technology behind it – from the grid to the car and everything in between.
Alpitronic’s cutting-edge power electronics draws on the very latest silicon-carbide (SiC) semiconductor technology by Infineon. Ideal for both urban and residential use, the silicon carbide in the modules allows for significantly lower energy losses and quieter operation. This not only shortens charging times but also ensures greater system reliability under continuous use and harsh conditions.
The revolutionary SiC modules, in comparison to the IGBT technology used in earlier models, offer unmatched efficiency by halving power losses. Additionally, they provide increased power density and significantly reduce noise levels.
Infineon’s high-performance components are at the core of an ultra-fast EV charging infrastructure, helping drivers get back on the road faster – while enabling compact, quiet, and scalable charging systems that meet the demands of a growing e-mobility ecosystem. Through powerful partnerships and advanced technology, Philipp, and his team are not just building chargers. They are building trust in electric mobility.
Infineon’s EasyPACK™ 1B and 2B modules are engineered to meet the demands of ultra-fast, compact, and efficient EV charging. With outstanding power density, low conduction and switching losses, as well as system efficiency above 97 percent at full load, they form the foundation for advanced charging solutions for different power classes and topologies.
Designed to thrive where space is tight, these SiC-based power modules are conducive to sleek, wall-mounted DC chargers like the HYC50 by Alpitronic. With up to 50 percent higher power density and reduced cooling requirements, they support scalable infrastructure with minimal construction effort.