Infineon launches ModusToolbox™ Motor Suite for simplified motor control development
Infineon launches ModusToolbox™ Motor Suite for simplified motor control development
Technology news
Munich, Germany – 8 November – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced the launch of the ModusToolbox™ Motor Suite, a comprehensive solution of software, tools and resources for developing, configuring and monitoring motor control applications. With its versatility across motor types, the solution enables developers to bring high-performance motor control applications to market quickly and efficiently. The suite supports industrial, robotics, and consumer applications such as home appliances, HVAC, drones, and light electric vehicles.
“With the launch of ModusToolbox Motor Suite, we are empowering developers to create innovative motor control applications with ease and efficiency,” said Steve Tateosian, Senior Vice President of IoT and Industrial MCUs at Infineon. “By providing a comprehensive solution that expands the capabilities of our ModusToolbox ecosystem, we are giving developers the tools they need to focus on what matters most: building better products.”
The suite streamlines development and testing, providing real-time parameter monitoring for valuable insights into motor performance, efficiency, and reliability. This enables engineers to quickly identify issues, optimize designs, and enhance overall functionality. It offers effortless and accurate board setup, comprehensive signal analysis, and customized status monitoring. ModusToolbox Motor Suite features automatic detection and recognition of supported boards and kits, real-time visualization and monitoring of motor control related signals. It also provides optimized system performance with pre-configured algorithms and real-time monitoring of critical system parameters. Additionally, the solution offers sophisticated algorithms that ensure control robustness across many motor types and applications. It currently includes out-of-the-box support for Infineon’s XMC7000 microcontrollers and will further expand its capability to include industrial MCUs, with PSOC™ Control integration confirmed for upcoming releases.
In addition to its comprehensive feature set, the ModusToolbox Motor Suite is designed to be highly versatile and easy to use. It provides a seamless graphical user interface for motor control development and an easily adaptable, hardware-abstracted motor control core library.
Infineon will showcase a demo featuring the ModusToolbox Motor Suite at electronica 2024 in Munich from 12 to 15 November (Hall C3, Booth 502).
Availability
The ModusToolbox Motor Suite is now available for download. More information is available at www.infineon.com/motorsuite
Infineon at electronica 2024
At this year's electronica in Munich, Infineon presents innovative solutions that are helping to shape an all-electric society. Visitors can explore sustainable technologies that are transforming the mobility and automotive landscape, enabling sustainable buildings and smarter living, and promoting the growth of artificial intelligence with minimal environmental impact. The company will present intelligent and energy-efficient solutions for tomorrow's connected world from November 12 to 15 in Hall C3, Booth 502 under the motto “Driving Decarbonization and Digitalization. Together.” More information is available at www.infineon.com/electronica.
About Infineon
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Press Photos
Modustoolbox Motor Suite
ModusToolbox™ Motor Suite is a comprehensive solution of software, tools and resources for developing, configuring and monitoring motor control applications and supports industrial, robotics, and consumer applications such as home appliances, HVAC, drones, and light electric vehicles
JPEG
1500x1025 px
Modustoolbox Motor Suite on Laptop
ModusToolbox™ Motor Suite is a comprehensive solution of software, tools and resources for developing, configuring and monitoring motor control applications and supports industrial, robotics, and consumer applications such as home appliances, HVAC, drones, and light electric vehicles
JPEG
900x506 px
Information Number : INFCSS202411-022
Veronika Seifried
Spokesperson Industrial and Infrastructure, GIP Division
+49 89 234 61662