Sensor technology
Infineon XENSIV™ sensors – sensing the world in automotive, industrial and consumer markets
Sensor technology subcategories
Collapse all subcategories Expand all subcategories
Infineon’s XENSIV™ family was developed to meet today’s sensing challenges in automotive, industrial and consumer applications. Building on the company’s in-depth system understanding, it is the broadest portfolio of sensor types on the market, giving customers the widest selection of ready-to-use solutions offering fast time-to-market. Spanning magnetic sensors, current sensors, pressure sensors, acoustic sensors, 3D image sensors (REAL3™) and radar sensor MMICs (RASIC™ for automotive), XENSIV™ ensures the perfect fit for all performance and integrity needs – regardless of the industry.
XENSIV™ sensors are designed to “smartify” lives by enabling “things” to “see”, “hear”, “feel” and “understand” their environment. They empower customers to build more intelligence into their designs, thus paving the way for new and compelling applications offering more intuitive interaction and contextual awareness. Infineon also joins forces with its ecosystem partners to jointly develop innovative, synergized use cases that give customers a clear market lead in emerging areas such as robotics, autonomous driving and building automation.
Building on the 40 years of experience that Infineon has clocked up in developing sensor products and its world-leading sensing technology portfolio, XENSIV™ delivers exceptional accuracy and best-in-class measurement performance. All XENSIV™ sensors are designed for the utmost in reliability. Enhanced design and production standards coupled with extended testing under the harshest conditions are reflected in the field-proven quality of this portfolio. Because of this robustness, customers worldwide can rely on XENSIV™ for system stability, durability and integrity over their entire product lifetime. This is a key success factor for safety-critical applications in automotive designs, for instance.
In addition, customers have the added reassurance of a proven track record. Over the past 10 years, Infineon has shipped more than 20 billion units and clearly demonstrated its ability to develop ready-to-use sensor solutions that match real-world, customer-specific needs while optimizing system design overall. Looking ahead, Infineon is committed to a path of continuous innovation and technology excellence to keep its customers ahead of the sensing curve.
XENSIV™ - online simulation tools
Define and optimize the current sensing structure for your system. The tool supports design of lateral and vertical insertions for PCB (2 to 10 layer stack) or bus-bar based applications. The simulation will provide insertion resistance, field transfer factor, sensitivity range, measurement range and power dissipation as well as cross-talk in case of a 3-phase system. | |
XENSIV™ - 3D magnetic sensors | 3D magnetic field sensor for smaller, more accurate and robust designs. The sensor family, with low current consumption and cost-optimized design, specifically addresses the needs of new magnetic sensor applications in consumer, industrial and automotive. They are ideally suited for the measurement of three dimensional movement within a magnetic field, linear slide movement as well as 360° angle rotation.
User defined specification of the magnet-sensor system such as magnet type, dimension or application-specific tolerances allow the modelling of customer-specific setups. The simulation results provide appropriate information to optimize and accelerate further design activities. |
XENSIV™ - magnetic Hall switches | Discover Infineon´s broad energy saving portfolio of Hall switches in smallest package. Simulate your Hall switch applications and see the results in an accurate simulation of the magnetic field and the switching behavior of the Hall switch in the application. |
XENSIV™ - magnetic angle sensors | Highest variety - low end to high end, standardized and specialized in all four magnetic technologies: Hall, GMR, AMR and TMR. This tool calculates the valid distance from the magnet surface to the sensor and the assembly error, given certain parameters: magnetic properties , sensor specification and assembly tolerances. |
Discover all Infineon XENSIV™ videos
To make it more convinient for you, you find below direct links to the appropriate product family you are interested in. Enjoy watching our Infineon videos.
- Videos 3D Magnetic Sensors
- Videos Magnetic Speed Sensors
- Videos Angle Sensors
- Videos CO2 sensor
- Videos Current Sensors
- Videos Hall Switches
- Videos Linear Hall Sensors
- Videos MEMS microphones for consumer
- Videos MEMS microphones for automotive
- Videos Absolute Pressure Sensors MAP&BAP
- Videos Radar Sensors
Fast finder
Welcome to our new interactive sensor selection tool, designed to connect you with the best fit for your design as quickly and effortlessly as possible. Simply select the overarching industry (automotive or industrial/consumer) and drill down on the applications till you find your target use case. The selection tool will then tell you what Infineon XENSIV™ sensor is the best choice for your design. It couldn’t be easier.