- Drive Core for automotive software development
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
Dec 03, 2025
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
Dec 03, 2025
Unique Id (PDL_UID)
Device-Specific Potential: Harnessing the Power of Unique IDs for Seamless Firmware Development
-
On this page
About
The Unique ID is an unchanging read-only register that is set during manufacture. The value is unique to the device and can be used to implement device-specific firmware. This component automatically includes the required Peripheral Driver Library (PDL) module, which makes firmware development easy and less error-prone.
- API to access 41-bit device ID register (read-only)
- Automatically adds the UID PDL module to the project
The Unique ID is an unchanging read-only register that is set during manufacture. The value is unique to the device and can be used to implement device-specific firmware. This component automatically includes the required Peripheral Driver Library (PDL) module, which makes firmware development easy and less error-prone.
- API to access 41-bit device ID register (read-only)
- Automatically adds the UID PDL module to the project