Infineon TRAVEO™ T2G Cluster and Altia CloudWare™ software platform for display applications to be showcased at CES 2023

Technology news

Jan 05, 2023

Munich, Germany and Las Vegas, Nevada – 5 January, 2023 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and Altia, an international leader in graphical user interface (GUI) design and development tools, today announced their cooperation. Infineon’s TRAVEO™ T2G Cluster microcontroller (MCU) family will be enabled by the Altia CloudWare™ software platform for display applications in early 2023. A demonstration of the TRAVEO T2G Cluster will be available at Infineon’s booth in the Las Vegas Convention Center West Hall #3829, and a demonstration of Altia’s CloudWare will be showcased in their private suite at CES 2023.

 

“We are excited about our close collaboration with Altia and their CloudWare software and hardware-in-the-cloud solution,” said Marcelo Williams Silva, Director of Product Marketing and Business Development, Infineon. “Infineon’s TRAVEO T2G helps drive displays in all vehicles including commercial, construction, agricultural and cars. Generating graphics on displays generally is an intricate process. Customers can soon connect our evaluation boards and TRAVEO Cluster human-machine interface (HMI) graphics with Altia’s easy-to-use solution CloudWare software to facilitate this process.”

Altia CloudWare allows customers to test Infineon’s TRAVEO evaluation boards and develop HMIs with Altia’s software to quickly get embedded displays to market. With Altia’s cloud-based CloudWare, TRAVEO T2G can easily be configured, speeding up designs by providing a focused development portal for benchmarking and testing GUI designs on TRAVEO hardware. By utilizing the virtual CloudWare, there is no need for individual compliers, programs or debuggers.

Infineon’s TRAVEO T2G MCUs are based on the Arm® Cortex®-M4/M7 core and deliver high performance, enhanced HMIs, high-security and advanced networking protocols. They are tailored for a broad range of automotive applications including electrification, body control modules, gateway and infotainment applications.

Availability

The joint solution from Infineon and Altia will be available in early 2023.

More information on Infineon’s commitment to mobility: www.infineon.com/about/our-stories/mobility

Infineon at CES 2023

The Consumer Electronics Show (CES) 2023 will be held from 5 to 8 January 2023 in Las Vegas, Nevada. See how Infineon drives decarbonization and digitalization together with its partners and customers at the Venetian Titian Ballrooms 2204 & 2205 located at The Venetian Hotel, Level 2, and at the Las Vegas Convention Center, West Hall (Booth 3829).

Editors interested in an interview with an executive, can contact their respective regional Media Relations manager. Industry analysts interested in a briefing, can email: MarketResearch.Relations@infineon.com.

About Altia

Altia is a software company that provides graphical user interface design and development tools that can be used from concept to final product code. Graphics code generated by Altia is driving millions of displays worldwide – from automotive instrument clusters, HUDs, and radios to thermostats, washing machines and healthcare monitors. Its mission is to get the best automotive, medical and consumer interfaces into production in the shortest time on the lowest-cost hardware.

Altia was founded in 1991. Its customers include automotive OEMs and Tier 1s like Continental Automotive, Denso, Fiat Chrysler Automobiles, Ford Motor Company, General Motors, Honda, Renault, Magneti Marelli, Nippon Seiki, Valeo, Visteon and more – plus leading consumer device manufacturers like Electrolux, Whirlpool, NordicTrack and many others.

Altia Media Contact

Cheryl Falk
Director of Marketing Communications
cherylf@altia.com

Press Photos

TRAVEO Infotainment

TRAVEO Infotainment

Altia CloudWare™ allows customers to test Infineon’s TRAVEO™ evaluation boards and develop human-machine interface graphics with Altia’s software to quickly get embedded displays to market. With Altia’s cloud-based CloudWare, TRAVEO T2G Cluster can easily be configured, speeding up designs by providing a focused development portal for benchmarking and testing graphical user interface designs on TRAVEO hardware. By utilizing the virtual CloudWare, there is no need for individual compliers, programs or debuggers.

JPEG

2126x1196 px

Download
TRAVEO T2G LQFP

TRAVEO T2G LQFP

Altia CloudWare™ allows customers to test Infineon’s TRAVEO™ evaluation boards and develop human-machine interface graphics with Altia’s software to quickly get embedded displays to market. With Altia’s cloud-based CloudWare, TRAVEO T2G Cluster can easily be configured, speeding up designs by providing a focused development portal for benchmarking and testing graphical user interface designs on TRAVEO hardware. By utilizing the virtual CloudWare, there is no need for individual compliers, programs or debuggers.

JPEG

1500x1250 px

Download

Information Number : INFATV202301-046

avatar

Fabian Schiffer

Senior Manager Media Relations

+49 89 234 25869

Send email