- eFuses
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
- Gate Driver ICs for SiC MOSFETs
- Isolated Gate Driver ICs
- Gate driver ICs for GaN HEMTs
- Half-Bridge Gate Driver ICs
- High-Side Gate Driver Ics
- Level-Shift Gate Driver ICs
- Low-Side Gate Driver Ics
- Three-Phase Gate Driver Ics
- Transformer Driver ICs
- Overview
- AC-DC LED driver ICs
- Ballast IC
- DC-DC LED driver IC
- LED dimming interface IC
- Linear LED driver IC
- LITIX™ - Automotive LED Driver IC
- NFC wireless configuration IC with PWM output
- VCSEL driver
- Overview
- BLDC motor drivers
- BDC motor drivers
- Stepper & servo motor drivers
- Motor drivers with MCU
- Bridge drivers with MOSFETs
- Gate driver ICs
- Overview
- Automotive MOSFET
- Dual MOSFETs
- MOSFET (Si & SiC) Modules
- N-channel depletion mode MOSFET
- N-channel MOSFETs
- P-channel MOSFETs
-
Silicon carbide CoolSiC™ MOSFETs
- Overview
- Silicon Carbide MOSFET modules
- Silicon carbide MOSFET discretes
- Silicon carbide MOSFETs bare dies
- 400 V / 440 V Silicon Carbide MOSFETs
- 650 V Silicon Carbide MOSFETs
- 750 V Silicon Carbide MOSFETs
- 1200 V Silicon Carbide MOSFETs
- 2000 V Silicon Carbide MOSFETs
- 2300 V Silicon Carbide MOSFETs
- 3300 V Silicon Carbide MOSFETs
- 1700 V Silicon Carbide MOSFETs
- Small signal/small power MOSFET
- Overview
- IGBT modules
- MOSFET (Si & SiC) Modules
- Intelligent power modules (IPM)
- Diodes and thyristors (Si/SiC)
- Automotive IGBT and CoolSiC™ MOSFET modules
- High density power modules
- Overview
- Automotive transceivers
- Linear voltage regulators for automotive applications
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
May 29, 2026
Business & Financial Press
May 20, 2026
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
May 29, 2026
Business & Financial Press
May 20, 2026
Business & Financial Press
May 11, 2026
Business & Financial Press
May 07, 2026
Power infrastructure and renewables – managing the unpredictable forces of nature
Our power infrastructure is increasingly characterized by renewable energies like wind power and photovoltaics. How do semiconductors help the power grid adapt to ensure reliability and resilience?
Dec 10, 2025
You flip the switch – the light goes on. Your electric car charges overnight. Data centers run non-stop, powering Artificial Intelligence and processing our data streams. And it takes a stable flow of electricity to keep it all working.
As the share of renewable energies in the power network increases, the challenge is growing more complex: We have to stabilize the electric power grid with reliable semiconductor technology and scale it to meet the growing demands of energy-intensive applications.
Infineon semiconductor solutions capture, channel and manage the unpredictable forces of nature – turning them into reliable, on-demand power.
The video shows how.
We expect electricity to always be available and, at the same time, to be generated by renewable sources that help to achieve our climate targets. This poses new challenges for the energy infrastructure and for the power grids in particular. After all, the electricity supply must remain reliable for all of us, despite power fluctuations, long-distance transmission, bidirectional energy flows, and energy-intensive end uses.
Power fluctuations
Since electricity generation from renewable sources depends on weather conditions, future power grids will need to balance out fluctuations in electricity supply in order to deliver power reliably. Battery energy storage systems (BESS) and grid-forming inverters play an important role in balancing supply and demand, and in stabilizing the grid.
Bidirectional energy flows
Private green energy generation, like rooftop solar panels, is growing as we aim for energy independence. Surplus privately generated energy is fed back into the distribution grid which nevertheless has to stay stable and resilient. Intelligent technologies such as 3-phase hybrid solar inverters cover self-supply with on-site energy storage capacity and thus contribute to grid stability.
Geographical gap
Electricity is often generated far from where it is consumed, requiring efficient, low-loss transmission. For offshore wind energy, HVDC technology makes it possible to transport green energy with minimum loss over hundreds of kilometers to power homes, offices, and data centers.
Energy-intensive applications
Energy intensive applications like AI data centers are on the rise. This is why Infineon is revolutionizing the power delivery architecture required for future AI data centers. In collaboration with NVIDIA, Infineon is developing the next generation of power systems based on a new architecture with central power generation of 800 V high-voltage direct current.
Modern power infrastructure systems benefit from high-performance semiconductors. Compared to conventional electromagnetic transformers and electromechanical protection devices, they offer a smarter and more efficient grid. Improved power quality, robust performance, faster response times, higher energy efficiency, and smaller form factors make them ideal for meeting the challenges of modern power grids to fulfill the demands of energy-intensive applications like AI data centers.
In the spotlight: Infineon solutions for solid-state transformers and solid-state circuit breakers
A solid-state transformer (SST) is a power electronic stack which connects medium-voltage (MV) power grids at several tens of kilovolts to low-voltage (LV) levels without the need for conventional transformers. EV- charging stations, solar farms and more use cases will benefit from SSTs in the future. In AI datacenters, SSTs will revolutionize the connection of the power grid with the IT racks. In a gigawatt-scale data center a direct current (DC) microgrid powered by a SST enables the seamless and energy efficient integration of distributed renewable energy resources.
A solid-state circuit breaker (SSCB) is an electronic device that protects electrical circuits from damage caused by excessive current flow, such as short circuits or overloads. Unlike electromechanical circuit breakers, which rely on mechanical parts to interrupt the flow of current, SSCBs use semiconductor components to perform this function. This results in faster switching times and faster interruption of the current, which is crucial in applications where even a slight delay can cause significant damage.
When green electricity needs to travel far, it takes to the highway.
- High-Voltage Direct Current (HVDC) transmits power over hundreds of kilometers with minimal power losses compared to alternating current (AC) systems.
- At the center of this system: offshore and onshore converter stations. They convert AC to DC for the journey via underground/subsea cables or overhead lines and convert DC back to AC at the destination.
- HVDC transmission is typically used to interconnect two power grids or to connect remote renewable energy sources such as offshore wind farms to the main grid.
Why high-voltage direct current?
- HVDC offers several advantages such as reduced power losses, improved controllability and grid stabilization.
- When electricity is transmitted over long distances, some of it is lost as heat due to resistance in the wires. Increasing voltage makes it possible to decrease current, which in turn reduces the amount of energy lost as heat.
High-performance building blocks for HVDC
- Infineon products for power conversion such as 3.3 kV, 4.5 kV and 6.5 kV IGBT modules in IHV housing or 4.5 kV Press Pack IGBT are installed in converter stations, depending on the power level and technical requirements.
- A rough idea of the order of magnitude: More than 16,000 of Infineon 6.5 kV IGBT modules can be installed in a single 2 GW HVDC project.
The electricity grid of the future will have to do more than just deliver electricity. It will have to predict and compensate for power fluctuations, protect against unexpected overloads and communicate in real time.
Hidden in the background, yet essential, semiconductors ensure that energy gets where it is needed. Infineon is driving this development forward with innovative technology at all voltage levels.