CoolGaN™ technologies
Highest efficiency and power density at unmatched quality and reliability
Gallium Nitride (GaN) is a leading-edge material that's revolutionizing the way we power our daily lives. With its unique properties, GaN enables the creation of smaller, faster, and more efficient power systems that can operate with high voltages and temperatures. This means that electric vehicles can charge faster and travel farther, renewable energy systems like solar microinverters can convert energy more efficiently, and AI data centers require less energy. Additionally, GaN is also being used to create smaller and faster chargers for our smartphones and laptops, such as USB-C chargers that can charge devices up to 3 times faster than traditional chargers. In simple terms, GaN is helping to make our technology more powerful, more efficient, and more sustainable, which can lead to cost savings, reduced environmental impact, and a more reliable supply of power.
GaN plays a vital role in solving the contradiction between rising energy demand and a net-zero economy. It masters the needs for more power, higher efficiency, and reduced size across a wide range of industries and applications, including smartphone adapters, solar microinverters, electric vehicles, AI data centers, or robots.
Discover how our CoolGaN™ power semiconductors turn industry buzz into actionable insights, with real-world examples that deliver concrete facts, figures, and benefits to inform and inspire your next design innovation.
Gain more insights into each application, and see how GaN is delivering to the demands for more power, higher efficiency, and size reduction.
Building on our technology leadership, we at Infineon were the first semiconductor manufacturer to successfully develop 300-millimeter GaN power wafer technology. Chip production on 300-millimeter wafers is technically more advanced and significantly more efficient compared to established 200-millimeter wafers, as the larger wafer diameter allows 2.3 times more chips to be produced per wafer. Our fully scaled-up 300-millimeter GaN manufacturing will allow us to deliver highest value to our customers even faster while moving towards cost parity for comparable silicon and GaN products.
Additional Documents
Additional Documents
FAQ
FAQ
What is the primary reason for the adoption of Gallium Nitride (GaN) in power electronics?
It enables higher efficiency and faster switching speeds.
What is a key benefit of Infineon’s CoolGaN™ BDS technology?
It supports bidirectional switching.
What is the main reason GaN-based power devices are ideal for high-frequency applications?
They exhibit extremely low switching losses.
What is the impact of GaN technology on the future of power electronics?
GaN technology is revolutionizing power electronics by enabling higher efficiency, compact designs, and faster switching speeds. With its wide bandgap (3.4 eV) and high electron mobility, GaN outperforms traditional silicon-based power devices. It allows for higher switching frequencies, reducing the size of passive components, leading to smaller and more power-dense solutions. In applications like data centers, electric vehicles (EVs), and renewable energy systems, GaN significantly reduces power losses, enhances thermal performance, and contributes to overall energy efficiency. As manufacturing techniques improve, GaN adoption is expected to grow, further driving innovation in next-generation power applications.
What are the major challenges in GaN adoption, and how is Infineon addressing them?
While GaN offers numerous benefits, its widespread adoption faces challenges, including:
- Manufacturing complexity: GaN requires specialized fabrication techniques
- Cost: GaN devices are initially more expensive than traditional silicon components
- Integration with existing systems: Transitioning from silicon to GaN requires new design approaches
- Reliability concerns: Long-term durability and failure modes need further study
Infineon’s Approach:
- Dedicated GaN Business Line to drive innovation and cost reduction
- Advanced packaging solutions that improve thermal management and reliability
- Collaboration with industry leaders to accelerate adoption in consumer, automotive, and industrial markets
- Investments in large-scale manufacturing to make GaN more cost-competitive
What is the key role of the coupling capacitor (CC) in a GaN gate drive circuit?
It acts as a charge pump for fast-switching transients and negative gate bias.
What is a key consideration when designing a power loop for CoolGaN™ Transistors?
Positioning devices and input filtering capacitors on the same layer.
What are the design recommendations for minimizing gate loop inductance in CoolGaN™ Transistor layouts?
To minimize gate loop inductance and optimize switching performance in CoolGaN™ HEMT layouts, the following recommendations should be followed:
- Position the gate driver close to the GaN device to reduce parasitic inductance
- Use a low-inductance PCB layout, placing the return path on the layer directly below the component layer
- Minimize the trace length between the driver and the GaN transistor
- Use a Kelvin connection for accurate gate control
- Employ symmetric layouts when paralleling GaN transistors to avoid mismatched inductance
By following these techniques, designers can achieve faster switching, lower losses, and improved system efficiency.