Microelectronics – connecting the real with the digital world
Smart and connected devices have long since become part of our everyday lives – thanks to small but powerful microchips that make IoT work. Do you know what the core components are that make “things” smart? Enter our world of IoT and discover more.
Jun 30, 2025
Digital transformation and innovation are unimaginable without microchips such as sensors, microcontrollers, power semiconductors, communication modules and security components. They all work seamlessly together to make our lives more comfortable, more convenient – but also more sustainable, greener and more efficient. We at Infineon make IoT work and power tomorrow’s technologies with five different types of microchips:
Sensors capture environmental information and convert it into digital data. Ubiquitous sensors make IoT devices smarter and enable the “things” involved to “see”, “hear”, “feel”, “smell” and therefore understand their environment. They mark the starting point of each IoT system by picking up data from the environment surrounding a connected device.
Our image sensors are ideal for fast, seamless, and spoof-proof facial identification in applications like phone/app unlocking, mobile payments, and much more.
Applications like entrance control or presence detection for smart homes and smart buildings benefit from Infineon's complete turn-key radar presence detection solution.
It's amazing what a big role touch sensors already play in our daily lives, for example in the use of smart watches, smart phones, wireless earbuds and more.
Gaming, virtual e-Commerce, 3D online education: AR applications with three-dimensional depth sensors link the real with the digital world.
Microcontrollers make things smart by processing, analyzing and communicating data to generate control signals for the IoT device. Specifications for microcontrollers in IoT devices are as varied as the IoT applications themselves.
Infineon’s microcontroller families provide the matching solutions, offering a broad variety of MCUs based on 32-bit Arm® architecture, Infineon’s 32-bit TriCore™ architecture, and others. These include microcontrollers in the XMC™ family and PSOC™ family that were custom-designed for IoT applications – from extremely energy-saving to extremely high-performance. The microcontrollers are backed up by an extensive portfolio of reliable, high-performance memories for embedded systems.
Purpose-Built for the IoT: Our solutions bridge the gap between expensive, power-hungry application processors and low performance microcontrollers (MCUs).
Our portfolio includes a wide range of semiconductor solutions addressing all requirements for wireless charging, ranging from just a few watts up to kilowatts.
Our products target a large variety of automotive applications: control of combustion engines, electrical and hybrid vehicles, transmission control units and much more.
Infineon cutting-edge touch sensing technologies have enabled Infineon to be the market leader in capacitive- and inductive-sensing applications.
Reliable, fast and efficient: Depending on smart decisions, our actuators convert the control signals into actions – which is mostly motion, but also light and heat.
This actuation is performed by power semiconductors. Did you know that we are the market leader in power discretes and modules? We offer the broadest portfolio of all power technologies in the market containing a full-spectrum portfolio of all power technologies. This includes:
- silicon (Si),
- silicon carbide (SiC),
- gallium nitride (GaN).
Our customers benefit from our market leadership to provide technology for optimizing power generation, transmission, storage, and consumption. We deliver actuators with power semiconductor solutions from milliwatts to megawatts with superior energy efficiency and reliability. Irrespective of whether you have a design in a microamp or megawatt range, you can rely on the energy efficiency of our actuators
Modern home appliances are increasingly smart and connected, providing a seamless, remote user experience. Users control operation and receive live data from appliances.
Our market-leading and comprehensive portfolio for industrial robots system solutions for Industry 4.0 addresses the latest trends in robotics and adds value to every robot design.
Infineon offers a variety of IPMs, with different semiconductors in different packages and different voltage and current classes. We enable optimum PCB design, size and system costs.
Wide bandgap semiconductors differ significantly from conventional semiconductors since they have a larger bandgap. It allows power devices to operate even better.
Wireless technologies like Wi-Fi®, Bluetooth®, and Bluetooth Low Energy are the backbone of IoT. Only seamless communication between IoT devices, the cloud, and the network can ensure that the Internet of Things full potential is utilized.
We at Infineon deliver secured cellular connectivity based on eSIM solutions, Wi-Fi®, Bluetooth®, USB and USB-C products. We offer a broad portfolio and well-founded expertise in wireless solutions for IoT, including consumer, commercial, industrial, and automotive applications. But we are also a market leader in USB and USB-C technology, having shipped more than one billion of such units since 2008. Beyond that, we enable secure cellular connectivity for a wide range of applications like smart factories and consumer electronics.
- Customers choose between Bluetooth Low Energy and dual-mode Bluetooth solutions that support both Bluetooth Classic and Bluetooth LE.
- The SDK, along with the ModusToolbox IDE and configurator tools, form a powerful but easy to use toolset that helps you create amazing Bluetooth-enabled IoT solutions.
- To enable IoT designs with a very small form factor, we also offer AIROC™ Wi-Fi + Bluetooth combos: These integrate IEEE 802.11a/b/g/n/ac Wi-Fi and Bluetooth into a single-chip solution
A Wi-Fi connectivity solution for new IoT applications provides a simple, secure Wi-Fi networking subsystem to connect products to the cloud of their choice without extensive firmware development, testing, or maintenance.
With a new product series, Infineon is responding to consumers’ demand for secured and convenient wireless connectivity and helping to reduce congestion of home networks.
Robust software underpins the development of high-quality, secure, and reliable IoT products. That is why we offer a set of multiplatform development tools and a comprehensive suite of GitHub-hosted firmware libraries.
New sensor technologies and connectivity solutions have helped create entirely new opportunities in the lighting industry, enabling energy savings and creating new use cases that go far beyond just lighting control.
We may be able to connect to the internet from any device or location – but one thing remains unchanged: Security is key. Our security solutions are based on our market-leading competence in the field. It's simple: To function, IoT has to be secure.
Whether it’s about data processing or data storage – from smart watches to smart buildings: Our aim is to create trust in the digital world, so that users, enterprises, and organizations can unleash the full potential of the Internet of Things. Safe in the knowledge that their personal data, intellectual property, sensitive information, and industrial IP remain safe and unchanged. Security solutions can also contribute significantly to public safety.
Our security portfolio for IoT begins at the hardware-based root of trust to trusted execution environments and secured boot. At Infineon, we are able to offer personalization and injection of certificates and keys in a secured, certified environment. This makes security easy to implement while shortening development times – all without detracting from the ease of use
The dynamic ICT infrastructure behind IoT requires a system-level security solution to enable secured end-to-end communication. Our embedded security solutions answer the demand for reliable ICT security.
To connect IoT devices securely at scale to the cloud and other IoT services and smart things, embedded security is key. Consumers and manufacturers need to be sure that the identity of each and every device is genuine and secured.
We offer the right, easy to implement security solutions for smart, always-secured homes. Infineon meets the evolving security needs without compromising on convenience
Infineon enables users to securely provision, store, select, and use multiple credentials such as payment cards and transport tickets via smart wearables and IoT devices.
Small and sometimes secret to the eye but with a big impact: Microchips are key to many electronic and smart devices that make your life easier and better. By developing and producing the core components for the Internet of Things (IoT), we at Infineon shape the future of digital transformation and innovation. In daily life, this is well-known communication technology like your smart phone, which may also be connected to your smart home or wearables like fitness trackers or watches. No matter what the purpose is: IoT needs reliable, fast, and efficient components to work. In the future, microchips will play an increasingly important role. Whatever the future holds, our goal remains the same: As a state-of-the-art technology partner, we drive tomorrow’s IoT technologies.