集中式逆变器解决方案
集中式逆变器配合许多紧密相连的太阳能电池板转换功率。其额定功率从600 KW 到 3000 KW 不等。集中式逆变器通常基于单级功率转换,大部分逆变器采用变压器设计或隔离变压器设计。在直流转交流阶段,可变直流电可以转换成与电网兼容的交流电。
在该变换单元, 两电平或 三电平 NPC1、NPC2、ANPC 拓扑都可选用。三电平拓扑因其效率更高而被广泛使用。1000 V光伏 (PV) 系统通常首选 三电平 NPC2 拓扑。1500 V光伏系统越来越受欢迎,因为它们可以降低系统成本,提高端到端效率。三电平 NPC1 / ANPC 拓扑结构使逆变器设计更稳健,更能抵抗宇宙射线。开关频率和冷却要求是影响交流滤波器尺寸、系统容量和成本的关键因素。需要具有低损耗和高电流密度的功率模块。
英飞凌提供的产品可支持高达1000 KW 的设计
立即在此探索合适的产品:
集中式逆变器的系统设计挑战
制造商一直不懈努力,试图降低系统成本的同时,提高产品性能。因此,单台逆变器的功率等级逐步上升。而一个明显的趋势就是1500 V光伏阵列正越来越多的用于大型电站型项目。
得益于我们广泛的功率半导体产品组合,以及我们在硅( Si) 、碳化硅 (SiC) 和氮化镓 (GaN) 等先进技术方面的专业优势,我们可以定制芯片技术和封装,为您的光伏逆变器提供理想的解决方案。
Podcast4Engineers: Solar
Photovoltaic systems – commonly known as solar power – are driving the shift from fossil fuels and bringing us closer to having abundant, green energy. Innovative and reliable power semiconductors and inverter technologies ensure that harnessing solar power is more convenient, efficient, and attractive.
全新白皮书:太阳能、风能和储能系统的趋势和解决方案
了解太阳能、风能和储能系统的应用和对功率半导体的要求。理解英飞凌如何应对可再生能源和储能系统市场的发展趋势,例如,集成 CoolSiC™ MOSFET 的逆变器。简要浏览各种适用于太阳能、风能和储能系统的解决方案。
应用演示:开发太阳能的无限潜力
本报告将为您概述太阳能应用的拓扑结构、技术趋势和需求。了解更多关于我们所提供的针对不同逆变器种类的产品信息,包括微逆变器,集中式逆变器及组串式逆变器。查阅我们针对您的具体应用场景作出的建议,若有意向,您可以在 5 个月内获得定制模块。
网络研讨会:从太阳能、风能到储能
在网络研讨会上,您将了解可再生能源和储能的新兴应用。了解更多关于应用趋势和需求的信息,并认识英飞凌为这些应用提供的解决方案。
Our modern world has a huge electric energy demand. The Earth gets more solar energy in one hour than the entire world uses in a year. Stay tuned to learn more about residential solar energy set-ups and Infineon solutions.
Infineon’s Easy family’s tremendous growth in the past few years led Easy modules to become even more flexible and scalable in key areas, such as voltage class and topologies.
As a result, Easy modules are widely used, not only in industrial applications but also in automotive applications.
To continue the successful momentum created by Easy 3B, “the big brother of the family”, Infineon has successfully developed the Easy 4B package, extending the package’s capabilities even further!
The EasyPACK™ 4B is now the largest package in the Easy family, with three DCB substrates.
In this training, we will see how Infineon’s two-level slew-rate control (or 2L-SRC) gate driver IC can help overcome gate resistance dimensioning trade-offs in order to obtain reduced switching losses.
We will also see an example of gate resistor dimensioning, with an under-five V/ns voltage slope target, as usually seen in drive applications.
Let’s learn more about how solar inverters work, from the ones we have in our houses, to the ones that are applied in major factories. We will also see how Infineon innovates in power semiconductors for solar inverter technology and how that can help with reducing costs and time to market.
In this module, we will have a look at different solar inverter trends and how the technology is evolving.
And afterwards, we will see what Infineon’s comprehensive solutions for the positioning of solar applications are.
In this EiceDRIVER™ X3 digital isolated gate driver training you will learn how to install the software that aids you in the evaluation of X3 digital and its evaluation board.
Webinars
Key takeaways:
- Learn about the application and power semiconductor requirements for solar, wind and energy storage systems
- Understand how Infineon responds to the trends in the market of renewable energies and storage systems, e.g. inverter integration with CoolSiC™ MOSFETs
- Get an overview of different solution offerings for solar, wind and energy storage systems
Join the webinar to learn about the positioning of SiC for in solar and energy storage applications. We will talk about the benefits of using Infineon’s Silicon Carbide MOSFET for solar and energy storage power conversion supported by real application examples.
In joining the webinar you will get a better understanding of the main technology trends in solar inverters.
The trend toward smart homes and connected systems demands a common communication interface between all home appliances and a PV inverter to enable a better balance between energy generation and consumption.
The main objective of this webinar is to explain the key technical features and system-level benefits of Infineon's semiconductor solution for string and hybrid inverter systems up to 30 kW output power.
Key Takeaways
1. Discover key technical features and system-level benefits of Infineon's semiconductor solution for string and hybrid inverter systems
2. Examine key drivers and technological requirements in the trend toward higher integration and fan-less operation
3. Explore the role of the PV inverter in the context of the smart home
Keywords: Silicon carbide, SiC, power density, bidirectional, power conversion, efficiency, energy, solar, storage, cost-effective, cost-effective power density, bidirectional power flow capability, high-efficiency power conversion