On the Verge of a New Computer Revolution - Infineon Presents the World´s Most Powerful Magnetic RAM Prototype
Munich, Germany June 22, 2004 Computers that dont loose their data, even when the power supply fails; laptops with batteries that supply power for days without the need for recharging; handheld computers and cell phones with huge amounts of memory; and personal computers that, at the touch of a button, pick up again at the exact spot where you left off the day before - In just a few years, this vision of the future of computing could become reality.
The prerequisites for it are offered by new types of memory technologies that are intensive in research like the MRAM technology. At the prestigious VLSI Circuits Symposia in Hawaii, the German semiconductor manufacturer Infineon together with IBM have presented the most advanced prototype of this revolutionary computer memory made to date: The worlds first 16-Mbit Magneto-resistive RAM (MRAM) prototype.
Unlike conventional computer chips, MRAM chips use magnetization to store information, instead of electrical charges. Up until now, computers had to continuously supply the main memory chips with power in order to store data. The information on MRAM memories, however, remains intact even after the system has been powered down. The working concept is similar to the way that data is stored on a computers hard disk drive. In addition, they are very fast, which enables exceptionally rapid access to data. For comparison: Infineons 16-Mbit MRAM chip is approximately 1,000 times faster than the non-volatile flash memory used in USB sticks, handheld computers and digital cameras. Furthermore, information can be stored in an MRAM memory cell up to one million times more often than is possible with flash memory.
The high storage capacity of the 16Mbit Chip (16 million single cells) was enabled using a small 1.4 square microns cell. By comparison 5,000 storage cells would fit on a cross section of a human hair.
The announcement of the worlds first 16-megabit MRAM memory prototype, emphasized Dr. Wilhelm Beinvogl, Chief Technology Officer for the Memory Products Business Group at Infineon Technologies, is a significant breakthrough in the development of this new technology.
In light of its many advantages, MRAM has in todays sight the potential to enter many memory applications in a few years.
Infineon has been developing the MRAM chips in cooperation with IBM since the year 2000. The technology has been transferred recently to Altis, a joint venture of the two companies located in France.
Users would profit from the elimination of the annoying boot-up phase during which current computers load data from the hard disk drive to main memory. Additional advantages would be greater convenience, since the computer retains the current state of work, and, above all, longer battery run-times in mobile devices - from laptops to cell phones -, since non-volatility enables MRAM chips to consume less power than conventional DRAM does. In the long term, MRAM chips could also change computer architecture, which - since the early days of fast computers - has been characterized by the division of labor between the fast but volatile main memory and the slower but more permanent bulk memory.
The prerequisites for it are offered by new types of memory technologies that are intensive in research like the MRAM technology. At the prestigious VLSI Circuits Symposia in Hawaii, the German semiconductor manufacturer Infineon together with IBM have presented the most advanced prototype of this revolutionary computer memory made to date: The worlds first 16-Mbit Magneto-resistive RAM (MRAM) prototype.
Unlike conventional computer chips, MRAM chips use magnetization to store information, instead of electrical charges. Up until now, computers had to continuously supply the main memory chips with power in order to store data. The information on MRAM memories, however, remains intact even after the system has been powered down. The working concept is similar to the way that data is stored on a computers hard disk drive. In addition, they are very fast, which enables exceptionally rapid access to data. For comparison: Infineons 16-Mbit MRAM chip is approximately 1,000 times faster than the non-volatile flash memory used in USB sticks, handheld computers and digital cameras. Furthermore, information can be stored in an MRAM memory cell up to one million times more often than is possible with flash memory.
The high storage capacity of the 16Mbit Chip (16 million single cells) was enabled using a small 1.4 square microns cell. By comparison 5,000 storage cells would fit on a cross section of a human hair.
The announcement of the worlds first 16-megabit MRAM memory prototype, emphasized Dr. Wilhelm Beinvogl, Chief Technology Officer for the Memory Products Business Group at Infineon Technologies, is a significant breakthrough in the development of this new technology.
In light of its many advantages, MRAM has in todays sight the potential to enter many memory applications in a few years.
Infineon has been developing the MRAM chips in cooperation with IBM since the year 2000. The technology has been transferred recently to Altis, a joint venture of the two companies located in France.
Users would profit from the elimination of the annoying boot-up phase during which current computers load data from the hard disk drive to main memory. Additional advantages would be greater convenience, since the computer retains the current state of work, and, above all, longer battery run-times in mobile devices - from laptops to cell phones -, since non-volatility enables MRAM chips to consume less power than conventional DRAM does. In the long term, MRAM chips could also change computer architecture, which - since the early days of fast computers - has been characterized by the division of labor between the fast but volatile main memory and the slower but more permanent bulk memory.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for the automotive and industrial sectors, for applications in the wired communications markets, secure mobile solutions as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2003 (ending September), the company achieved sales of Euro 6.15 billion with about 32,300 employees world-wide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at
www.infineon.com.
Information Number
INFMP200406.073
Press Photos
-
CTO of Memory Products Business GroupWilhelm BeinvoglJPG | 1.02 mb | 1535 x 2126 px
Wilhelm BeinvoglJPG | 16 kb | 116 x 160 px
-
Infineon and IBM present world´s first 16 Mbit MRAM - Innovative Chip Design results in Highest Density Reported to DateWorld´s first 16 Mbit MRAMJPG | 461 kb | 1535 x 1063 px
World´s first 16 Mbit MRAMJPG | 22 kb | 160 x 111 px
-
Infineon and IBM present world´s first 16 Mbit MRAM - Innovative Chip Design results in Highest Density Reported to DateWorld´s first 16 Mbit MRAMJPG | 402 kb | 1535 x 1063 px
World´s first 16 Mbit MRAMJPG | 22 kb | 160 x 111 px