- AMD CPU voltage regulator Ics
- Ampere CPU voltage regulator Ics
- Intel CPU voltage regulator Ics
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
Oct 01, 2026
Business & Financial Press
Sep 29, 2026
Business & Financial Press
Sep 23, 2026
Business & Financial Press
Sep 16, 2026
- Company
- Our stories
- Events
- Press
- Investor
- Careers
- Quality
- Latest news
Business & Financial Press
Oct 01, 2026
Business & Financial Press
Sep 29, 2026
Business & Financial Press
Sep 23, 2026
Business & Financial Press
Sep 16, 2026
Trapped ion quantum computing
Taking quantum computing to the next level
- We help in bringing a meaningful and powerful trapped-ion quantum computer (TIQC) to life to solve the optimization problems that have been waiting for decades to be solved.
- We help our academic partners to focus on what they do best: push the boundaries of science and research.
- We help our startup partners to focus on what they do best: find new ways and integrate them into a successful and winning system.
We know how to industrialize and combine novel materials and technologies. Infineon traps and trap designs are predictable, repeatable and reliable. We’re paving the road towards thousands of qubits by working with our partners on cryogenic control electronics and optics integration.
To that end, we verify and characterize our ion trap modules in our in-house quantum laboratory.
At our Villach fab we are capable of working with wafer diameters from 6 to 12 inch, many different substrates, and a broad variety of process materials.
Therefore, we can meet the particular needs of trapped ion quantum processors in terms of substrate materials, metal properties, and surface conditioning, supporting our academic partners in pushing the boundaries of science and research.
So far, Infineon ion traps with a storage capacity of 18 ions have demonstrated parallel shuttling of two ion-arrays. In order to arrive at high qubit counts of 100 or more, it’s all about scalability and further improving stability. Physics has come a long way. With each step we take in scaling, we have to solve the myriad of engineering challenges that come with it.
We’re working with our academic and start-up partners on cryogenic control electronics and optics integration to pave the road towards thousands of qubits.
Infineon is now into Gen.3 of their ion traps. It adds electrodes in the third dimension to increase ion confinement by a factor of ten compared to standard surface traps.
It is manufactured using Infineon's ample experience in anodic wafer bonding assuring industry leading precision. The trap has been successfully tested at the TIQI group at ETHZ and documented in this free paper.
To enable fast progress, the ion trap on carrier is installed into the ion trap socket as a defined and stable element to be in turn mounted into the cryostat or vacuum chamber. Fast-paced evolution will happen on the ion trap chip, whilst the socket will only evolve slowly.
To facilitate scaling, the ion trap on carrier will evolve into a Quantum Processing Module (QPM) that integrates control electronics and optics. Some of the electronic components currently positioned on the socket PCB will integrate onto the QPM. Our socket has been successfully employed by our academic partners.
To move to higher numbers of qubits, the integration of control electronics into the QPM is essential. This includes Digital-to-Analogue-Converters (DACs) and other components. The DACs are the most obvious: As with increasing qubit count, more of the electrodes that trap and move the ions are needed, and their voltages have to be generated close to the ion trap. Therefore, these components will have to operate at a temperature of around 10K.
Single ions are created by local ionization of neutral atoms, for example Ca, Ba or Be. Since ions are charged, they are controllable by electric fields and can be used for fundamental research as atomic clocks, sensors or for quantum computing.
Trapped ion benefits include
- Highest gate fidelities
- Full connectivity between qubits
- Longest coherence time
- Most entangled qubits: 24*
- Moderate temperature: 10K
- Shuttling capability
In a trapped ion quantum computer (TIQC) the qubits are implemented using charged atoms in a cryogenic vacuum. The ion, for example Ca+, Ba+ or Be+, is captured with DC and RF fields and manipulated with lasers or microwaves.
The qubit is defined by the electron‘s quantum-mechanical state: the ground state is defined as a logical 1, the qubit laser or a microwave pulse elevates the electron into an excited state to implement a logical 0.
Then after the calculations or gate operations have been performed, the resulting state of the qubit has to be read. That is done by employing the readout laser to elevate the electron to a higher electron orbit from which it will immediately decay and emit one photon that can be detected. Since the readout laser is tuned to excite the ground state, detected photons indicate that the qubit was a logical 1 before the readout.
Shuttling of ions provides the means to bring arbitrary combinations of qubits together for calculations. Therefore, it constitutes an important ingredient towards large-scale trapped-ion quantum processors.
Employing Infineon’s ion trap chip, scientists at the University of Innsbruck have been the first to demonstrate parallel shuttling of two ion chains.
Read more about 2D Linear Trap Array for Quantum Information Processing
This video demonstrates an array of 2x2 ions being transported simultaneously (low speed shuttling on purpose).
ATIQ (Implementierung von Quantenalgorithmen aus Finanzwesen und Chemie auf einem Quantendemonstrator):
More information
OptoQuant:
More information
On June 26th Infineon and eleQtron announced their partnership to jointly develop trapped ion Quantum Processor Units (QPUs) for scalable quantum computers.
In this collaboration, Infineon will provide eleQtron with three progressively improved generations of ion traps as well as the necessary expertise to adapt them to the MAGIC concept. Additionally, Infineon will enable eleQtron to build ion trap-based quantum computers with successively increasing functionality.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
On July 6th Oxford Ionics and Infineon announced a collaboration to build high-performance and fully integrated quantum processing units (QPUs).
In this partnership, Infineon contributes their advanced technology platform for customized traps that are predictable, repeatable, and reliable in order to pave the way towards the industrial production of QPUs offering hundreds of qubits within the next five years .
Browse our open positions and become part of our team! Participate in further developing the future of quantum computing.
Follow this link and type 'quantum computing' in the search field
So far, Infineon ion traps with a storage capacity of 18 ions have demonstrated parallel shuttling of two ion-arrays. In order to arrive at high qubit counts of 100 or more, it’s all about scalability and further improving stability. Physics has come a long way. With each step we take in scaling, we have to solve the myriad of engineering challenges that come with it.
We’re working with our academic and start-up partners on cryogenic control electronics and optics integration to pave the road towards thousands of qubits.
Infineon is now into Gen.3 of their ion traps. It adds electrodes in the third dimension to increase ion confinement by a factor of ten compared to standard surface traps.
It is manufactured using Infineon's ample experience in anodic wafer bonding assuring industry leading precision. The trap has been successfully tested at the TIQI group at ETHZ and documented in this free paper.
To enable fast progress, the ion trap on carrier is installed into the ion trap socket as a defined and stable element to be in turn mounted into the cryostat or vacuum chamber. Fast-paced evolution will happen on the ion trap chip, whilst the socket will only evolve slowly.
To facilitate scaling, the ion trap on carrier will evolve into a Quantum Processing Module (QPM) that integrates control electronics and optics. Some of the electronic components currently positioned on the socket PCB will integrate onto the QPM. Our socket has been successfully employed by our academic partners.
To move to higher numbers of qubits, the integration of control electronics into the QPM is essential. This includes Digital-to-Analogue-Converters (DACs) and other components. The DACs are the most obvious: As with increasing qubit count, more of the electrodes that trap and move the ions are needed, and their voltages have to be generated close to the ion trap. Therefore, these components will have to operate at a temperature of around 10K.
Single ions are created by local ionization of neutral atoms, for example Ca, Ba or Be. Since ions are charged, they are controllable by electric fields and can be used for fundamental research as atomic clocks, sensors or for quantum computing.
Trapped ion benefits include
- Highest gate fidelities
- Full connectivity between qubits
- Longest coherence time
- Most entangled qubits: 24*
- Moderate temperature: 10K
- Shuttling capability
In a trapped ion quantum computer (TIQC) the qubits are implemented using charged atoms in a cryogenic vacuum. The ion, for example Ca+, Ba+ or Be+, is captured with DC and RF fields and manipulated with lasers or microwaves.
The qubit is defined by the electron‘s quantum-mechanical state: the ground state is defined as a logical 1, the qubit laser or a microwave pulse elevates the electron into an excited state to implement a logical 0.
Then after the calculations or gate operations have been performed, the resulting state of the qubit has to be read. That is done by employing the readout laser to elevate the electron to a higher electron orbit from which it will immediately decay and emit one photon that can be detected. Since the readout laser is tuned to excite the ground state, detected photons indicate that the qubit was a logical 1 before the readout.
Shuttling of ions provides the means to bring arbitrary combinations of qubits together for calculations. Therefore, it constitutes an important ingredient towards large-scale trapped-ion quantum processors.
Employing Infineon’s ion trap chip, scientists at the University of Innsbruck have been the first to demonstrate parallel shuttling of two ion chains.
Read more about 2D Linear Trap Array for Quantum Information Processing
This video demonstrates an array of 2x2 ions being transported simultaneously (low speed shuttling on purpose).
ATIQ (Implementierung von Quantenalgorithmen aus Finanzwesen und Chemie auf einem Quantendemonstrator):
More information
OptoQuant:
More information
On June 26th Infineon and eleQtron announced their partnership to jointly develop trapped ion Quantum Processor Units (QPUs) for scalable quantum computers.
In this collaboration, Infineon will provide eleQtron with three progressively improved generations of ion traps as well as the necessary expertise to adapt them to the MAGIC concept. Additionally, Infineon will enable eleQtron to build ion trap-based quantum computers with successively increasing functionality.
Share in WeChat
Scan the QR code with your WeChat App to share this page.
On July 6th Oxford Ionics and Infineon announced a collaboration to build high-performance and fully integrated quantum processing units (QPUs).
In this partnership, Infineon contributes their advanced technology platform for customized traps that are predictable, repeatable, and reliable in order to pave the way towards the industrial production of QPUs offering hundreds of qubits within the next five years .
Browse our open positions and become part of our team! Participate in further developing the future of quantum computing.
Follow this link and type 'quantum computing' in the search field
- Infineon teams up with eleQtron to deliver three generations of trapped-ion quantum processor units
- Infineon and Oxford Ionics join forces to develop leading Trapped Ion Quantum Processors
- Infineon and Quantinuum announce partnership to accelerate quantum computing towards meaningful real-world applications
- Quantum computers: New Infineon quantum test lab boosts research
- Infineon opens laboratory for quantum electronics and Power AI
- Infineon partners with Nu Quantum, University of Sussex and Cisco
- Infineon Innovation Impact Video: Quantum Computing: What & When
- Munich Quantum Valley (MQV)
- Quantum Valley Lower Saxony (QVLS)
- German Quantum Computer based on Superconducting Qubits (GeQCoS)
- Digital-Analog Quantum Computer (DAQC)
- Semiconductor Quantum Processor with Shuttling-Based Scalable Architecture (QUASAR)
- Quantum Large-Scale Integration with Silicon (QLSI)
- European Project ISOLDE