Infineon Ready to Appeal European Commission Decision in Antitrust Investigations against Smart Card Chip Producers; Among Other Companies EC fined Infineon Euro 82.8 Million

2014/09/03 | ビジネス&フィナンシャルプレス

Neubiberg, Germany – September 3, 2014 – Today, the European Commission adopted a decision in its antitrust investigation against four semiconductor companies active in the smart card industry including Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY). The European Commission believes that the companies involved infringed European antitrust rules through the alleged sporadic exchange of competitively sensitive information. The fine for Infineon is Euro 82.8 million, while the total fine was set at Euro 138 million.

 

Infineon rejects the allegations as unfounded. Further, Infineon believes that its procedural rights were violated by the European Commission. Therefore, Infineon will review the decision very closely and is ready to appeal at the General Court of the European Union in Luxembourg.

 

As is typical in such antitrust proceedings, the fine is apportioned according to the revenue of each of the affected companies during the relevant timeframe. Consequently, Infineon was attributed the greatest portion of the total fine, simply because of its higher share in the European market for smart card chips in the relevant period between September 2003 to March 2005.

 

About the case

 

The investigation of the European Commission began in 2008. When the allegations were raised, Infineon conducted a thorough investigation and concluded that none of its personnel acted improperly in handling competitively sensitive information regarding smart card chips. Since that time, Infineon has been presented with no credible evidence contrary to that conclusion.

 

In 2011, the European Commission initiated settlement discussions with the three other semiconductor companies. The European Commission invites companies to discuss settlement only if it believes they were part of a cartel. Infineon was not invited to the settlement talks. The settlement discussions ended unsuccessfully in 2012, and the European Commission surprisingly resumed the proceedings against Infineon in April 2013.

 

Further information

Link to the press release of the European Commission of September 3, 2014.

インフィニオンについて

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2013 fiscal year (ending September 30), the Company reported sales of Euro 3.84 billion with around 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).Further information is available at www.infineon.com

Information Number

INFXX201409-057

Press Photos

  • Logo Infineon Technologies AG
    Logo Infineon Technologies AG
    Infineon_Logo

    JPG | 402 kb | 2361 x 1033 px