英飞凌推出专为工业设备和风车而优化的1200伏和1700伏功率模块PrimePACK

2007-5-22 | 技术媒体

2007年5月22日,德国慕尼黑与纽伦堡讯——英飞凌科技股份公司(FSE/NYSE:IFX)推出全新1200伏和1700伏电压级功率模块PrimePACKTM ,其重量比同等功率的模块低45%。 英飞凌是目前唯一一家能够生产如此紧凑高效的IGBT(绝缘栅双极晶体管)模块的半导体厂商。该公司在PCIM 2007展会暨研讨会上推出的这种紧凑型IGBT模块系列,可优化功率转换系统,广 泛适用于各种工业传动装置、风车、电梯、牵引机或辅助传动装置、火车与牵引车的电源和加热系统等。

PrimePACK 模块采用创新的封装概念,充分利用英飞凌IGBT4芯片的优势,具备出众的电气可靠性。这种独特的模块设计具备诸多优点,例如模块内IGBT芯片的特殊版图大大改善了散热效能。这 些IGBT芯片更靠近基板的螺钉固定点,有效降低了基板与散热片之间的热阻效应。此外,该模块的内部杂散电感也比同类模块低60%左右。

PrimePACK 模块采用半桥配置和模块化设计,只要采用不同尺寸的模块或者将特定类型的模块并联在一起,即可轻松调整转换器的功率。目前,英 飞凌已经推出了1,200V和1,700V两个电压级别的PrimePACK模块,每个模块都有两种尺寸规格(89毫米x 172毫米的PrimePACK2和89毫米x 250毫米的PrimePACK3)。这 些模块的重量比同等功率的模块低45%。由于重量减轻,制造和安装功率转换器更加轻松。

“PrimePACK模块的推出表明英飞凌已根据用户的需求,对这些产品进行了切实的优化,”英飞凌科技高级主管兼工业电源部负责人Martin Hierholzer表示,“ 这种创新的模块化设计专为系统集成进行了优化,可提高各类工业 传动系统的效率和耐用性。”

供货情况
目前,1700伏的PrimePACK模块已实现批量生产。1200伏的PrimePACK模块预计将于2007年9月开始投入量产。这些模块在德国瓦尔施泰生产,I GBT二极体与IGBT芯片则在奥地利菲拉赫制造。该系列模块符合欧盟RoHS环保规范,并且满足NFF16-101 与16-102防火标准要求。

英飞凌在PCIM 2007展会(德国纽伦堡、5月22日至24日)的12号展厅的404号展台,展出了PrimePACK模块系列和其它创新功率产品。

欲获得这种全新模块的更多信息,敬请登录:www.infineon.com/primepack

About Infineon

总部位于德国慕尼黑的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、连通性和安全性提供半导体和系统解决方案。2006财年(截止到9月份),公司实现销售额79亿欧元( 包括奇梦达的销售额38亿欧元),在全球拥有约42,000名雇员(其中奇梦达雇员约12,000人)。英飞凌科技公司的业务遍及全球,在美国圣何塞、亚太地区的新加坡和日本东京等地拥有分支机构。英 飞凌公司已列入法兰克福股票交易所的DAX指数,并在纽约股票交易所挂牌上市,股票代号:IFX

Information Number

INFXX200705.057

Press Photos

  • The PrimePACK(tm) family of compact IGBT (Insulated Gate Bipolar Transistor) modules enable power converter system solutions optimized for various industrial drives, as well as for windmills, elevators or auxiliary drives, power supplies and heating systems in trains and tractors. There are two module sizes: PrimePACK 2 (89mm x 172mm) and PrimePACK 3 (89mm x 250mm).
    The PrimePACK(tm) family of compact IGBT (Insulated Gate Bipolar Transistor) modules enable power converter system solutions optimized for various industrial drives, as well as for windmills, elevators or auxiliary drives, power supplies and heating systems in trains and tractors. There are two module sizes: PrimePACK 2 (89mm x 172mm) and PrimePACK 3 (89mm x 250mm).
    PrimePack_2_3

    JPG | 1.8 mb | 2126 x 1535 px