Infineon launches SLC26P security controller based on 28 nm technology for payment applications; expands its supply option to enable long-term, dependable sourcing for smart card and embedded security ICs

2022-11-29 | 市场新闻

Munich, Germany – 29 November, 2022 – Commercial production of integrated circuits using 28 nm technology node began several years ago. As the process technology has matured, market demand for 28 nm products has also increased. Although offering numerous advantages, security applications have not been among the main applications of this technology, thus far. Today, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is introducing SLC26P, the first security IC targeting high volume payment applications based on the future-proof 28 nm technology node.

“Infineon is the first to make use of the 28 nm technology node for smart card ICs. This step emphasizes our long-term commitment to the security IC market,” said Ioannis Kabitoglou, Head of Digital Security & Identity Business Line of Infineon. “The SLC26P is the first smart card IC product that will be manufactured in 28 nm technology. We are planning for a fast ramp of production in the first half of 2023. This will help us deliver to the continued high demand for cutting-edge security solutions and relieve the negative impact of the semiconductor shortages in security ICs.”

Infineon has been working with long term partner TSMC to develop security IC products based on 28 nm technology node. Capacity issues at mature technologies like 90 nm, 65 nm and 40 nm have been a limiting factor for the strong demand in security applications. Silicon foundries, for this reason, have been building new capacity to address these limitations. By enabling the 28 nm technology node for security ICs, Infineon not only offers the market an increased sourcing flexibility, but also empowers higher performance as well as more energy efficient and environmentally friendly products for this segment. The portfolio of products based on 28 nm will serve state-of-the-art smart card and embedded security IC applications in the coming years, including payment and transportation markets as well as identity and authentication solutions.

Infineon’s SLC26P is the first security controller optimized for payments based on the 28 nm technology – an EMVCo certification is expected to be available within December 2022. The IC delivers unmatched performance for the payment industry, combined with highest security standards. It features state-of-the-art Arm® v8-M architecture optimized for deeply embedded systems and designed for low-latency processing.

Availability

SLC26P is planned to ramp-up in production the first half of 2023 targeting to enable EMV payment card issuance with the new technology beginning in Q2 2023. Samples based on SLC26P are available upon request.

Note to the editor

Infineon will be at TRUSTECH (booth G035, 5.2) in Paris, Porte de Versailles, from 29 November until 1 December 2022. Experts will be available for one-on-ones about Infineon’s security controller offering based on 28 nm technology during and after TRUSTECH.

Information Number

INFCSS202211-034

Press Photos

  • Infineon’s SLC26P is the first security controller optimized for payments based on the 28 nm technology – an EMVCo certification is expected to be available within December 2022. The IC delivers unmatched performance for the payment industry, combined with highest security standards. It features state-of-the-art Arm® v8-M architecture optimized for deeply embedded systems and designed for low-latency processing.
    Infineon’s SLC26P is the first security controller optimized for payments based on the 28 nm technology – an EMVCo certification is expected to be available within December 2022. The IC delivers unmatched performance for the payment industry, combined with highest security standards. It features state-of-the-art Arm® v8-M architecture optimized for deeply embedded systems and designed for low-latency processing.
    Application_payment

    JPG | 537 kb | 2126 x 1418 px