Infineon Launches Windows Server 2008-compatible Trusted Computing Management Server Software Suite for Complete Enterprise Security

Visit us in Booth #66 at the Microsoft Windows Server 2008 Launch

Feb 27, 2008 | Technology Media

Microsoft Windows Server 2008 Launch, Los Angeles, California – February 27, 2008 – Infineon Technologies (FSE/NYSE: IFX), a leading supplier of integrated circuits and supporting software for secure computing and communications devices, today announced the Trusted Computing Management Server (TCMS) software suite for central management of Trusted Platform Modules (TPM)-equipped PCs in enterprise environments.

The TCMS software suite can be bundled with Infineon’s TPM Professional Package Software V3.5 for a complete hardware and software solution for enterprise professionals to safely protect their client data.

The Infineon TCMS software enables enterprise customers to easily deploy and manage TPM-equipped PCs, enabling a fully “trusted computing” experience for the user. Targeting medium and large companies, this software suite allows enterprises to take full advantage of TPM-based security on a heterogeneous PC infrastructure, which enables central management of Microsoft Windows®-based clients within the enterprise. The upgraded version of the TPM Professional Package software offers users the same user interface, despite the heterogeneous TPM hardware they may have on their PCs. Hardware can either be an Infineon TPM or a qualified 3rd party Trusted Computing Group (TCG)-compliant TPM.

“HP has been a leader in TPM adoption by providing the HP Embedded Client Solution as a standard feature across many of our business desktop and notebook PCs,” said Carolyn Bosco, Worldwide Security Marketing Manager for HP Business PCs. “The Infineon TCMS will now allow HP customers to seamlessly integrate and manage HP security solutions through their central IT management infrastructure.”

Microsoft is pleased to be working with Infineon to expand the offerings for Windows Server 2008 customers,” said Ward Ralston, Group Technical Product Manager for Windows Server Marketing at Microsoft Corp. “Our industry partners play an essential role in ensuring that our customers have the best technology foundation available and Infineon’s TCMS software suite helps deliver valuable new functionality to our joint customers.”

“Security continues to be a growing concern for professional PC users especially for notebook users,” said Josef Kohn, Product Manager of Infineon Technologies North America. “As a leader in security and with over 15 years of security expertise, Infineon understands the importance of data security from a hardware and software perspective. With the new Professional Package Software supporting TCG-compliant TPM hardware and the TCMS as the central management solution, this will allow corporate customers to efficiently deploy and manage TPM based security applications.”

According to a study of US market research company IDC, today more than 150 million notebooks and desktops are equipped with a Trusted Platform Module (TPM). IDC also anticipates the TPM market will increase to more than 250 million pieces shipped in the year 2010 alone. This equals an attach rate of more than 90 percent of all notebooks and desktops.

Sales Partners

Infineon will sell the TCMS software suite via sales and service partners in North America with plans to expand to Europe, Japan and other regions. If you are interested in being a sales or service partner, please visit www.infineon.com/tpm for more information.

Availability

The Infineon TCMS software suite will be shipped in Q2 2008. The suite is currently being tested and piloted by various customers.

Infineon is showing its Trusted Computing Management Server (TCMS) software suite for central management of TPM-equipped PCs in Booth #66 in the Partner Pavilion at the Microsoft Windows Server 2008 Launch.

About TCG Specifications

The Trusted Computing Group (TCG), with more than 100 member companies, is a not-for-profit organization formed to develop, define, and promote open standards for hardware-enabled trusted computing and security technologies, including hardware building blocks and software interfaces, across multiple platforms, peripherals, and devices. TCG specifications will enable more secure computing environments without compromising functional integrity, privacy, or individual rights. The primary goal is to help users protect their information assets (data, passwords, keys, etc.) from compromise due to external software attack and physical theft.

The Group was formed as a successor to the Trusted Computing Platform Alliance (TCPA), which was founded in 1999 by Compaq, HP, IBM, Intel and Microsoft. TCG has adopted the specifications of TCPA and will both enhance these specifications and extend the specifications across multiple platforms such as servers, PDA's, and digital phones. Further information on Trusted Computing Group (TCG) is available at www.trustedcomputinggroup.org.

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, communications, and security. In the 2007 fiscal year (ending September), the company reported sales of Euro 7.7 billion (including Qimonda sales of Euro 3.6 billion) with approximately 43,000 employees worldwide (including approximately 13,500 Qimonda employees). With a global presence, Infineon operates through its subsidiaries in the U.S. from Milpitas, CA, in the Asia-Pacific region from Singapore, and in Japan from Tokyo. Infineon is listed on the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX).

Information Number

INFAIM200802-047