Analog Resource Constraint (Cy_Analog_Constraint)
概要
General Description
The Analog Resource Constraint component allows you to define the route of the analog signal to which it is connected. This is an advanced feature that is not needed for most designs, and should be used with caution.
Note: Routing is strict. All of the devices connected to the net with the resource constraint must have a direct hardware connection to the resource. If the resources do not have a hardware connection to the specified constraint, an error will occur.
- Limits analog routing of a signal to a specific routing resource
- All terminals on the signal must connect directly to the routing resource
サポート