インフィニオン、迅速で簡単なモーター駆動設計キット、MADKをリリース

2016/05/06 | マーケットニュース

2016年5月6日、ミュンヘン(ドイツ) 

独インフィニオンテクノロジーズは、パワーエレクトロニクス機器の展示会PCIMにおいて、20 W~300 Wの3相モーター駆動用の評価プラットフォーム「iMotion™モジュラアプリケーションデザインキット(MADK)」をリリースすると発表しました。このキットは、コントローラ基板とパワー基板で構成されており、センサレス、またはオプションでセンサーを備えた駆動回路にも対応できます。このキットを使えば、わずか数ステップの手順でモーターを動かことができます。すなわち、パソコンに評価システムを接続し、ソフトウエアをダウンロードしてインストールし、パラメータを入力すれば済みます。その結果、モーターシステムを1時間以内に動作させられるので、より迅速な製品の市場投入に寄与します。 

インフィニオンは、異なるモーター容量に対応した4種類のキットを用意しています。すべてのキットは、デバッグ用インタフェース付きの制御カード、整流器などを備えた完全なパワーステージ、EMI(電磁干渉)フィルタなどで構成されています。モーター制御ソフトウエアは、事前に搭載するか、またはダウンロードして利用できます。また、GUI(グラフィカルユーザーインタフェース)によりパラメータ設定やチューニングを簡単に行えます。M1 20ピンMADKプラットフォームの標準化されたインタフェースコネクタと、多彩な制御基板とパワー基板の組み合わせにより、異なるアプリケーションの要求に対して最適化できます。 

フィールドオリエンテッドコントロール(FOC)のソフトウエアは、弊社産業用マイクロコントローラXMC1302によるセンサレスモーター制御および、ホールセンサーや3次元磁気センサーを用いた制御もサポートしています。このXMC1302を搭載した制御カードは、独Segger 社のJ-Link技術に基づいたデバッガを搭載しています。さらに、このツールのソフトウエアには簡単に使えるμC-ProbeベースのGUIが搭載されています。更なるアプリケーションの開発には、インフィニオンが無償で提供する統合開発環境(IDE)DAVE™か、または、米Keil社、スウェーデンIARシステムズ社、スウェーデンAtollic社のような主要なARM ®用IDEを使うことができます。 

今回用意したキットは、XMC1302制御カードと、4種類のパワー基板、μIPM™のIRSM836シリーズやμIPM-DIPのIRSM505シリーズ(500Vまたは250V)の組み合わせになります。制御部の他のオプションとして、ハードウエアベースのセンサレスFOC制御を備えたモーター制御用ASIC(特定用途向けIC)であるIRMCK099Mを搭載したボードもあります。こちらには個別のデバッグインタフェースカードが付属しています。 

提供状況

4種のキットと6種の異なる単一基板は、 www.infineon.com/MADKや世界中の代理店で5月中に提供する予定です。上記リンクより、各キットの完全なソフトウエアパッケージやiMotion MADKに関する詳細情報にアクセスできます。 

インフィニオン、「 PCIM 2016 」に出展

インフィニオンは「PCIM 2016」見本市(於:ドイツニュルンベルク、会期:2016年5月10~12日)のホール9、ブース#412にて、産業用、家電用、車載用アプリケーションにおける効率的なシステムに向けた最先端技術を紹介しています。「PCIM」でのインフィニオンの主な展示内容は、 www.infineon.com/pcimをご覧ください。

Information Number

INFIPC201605-054

Press Photos

  • Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    IRMCSDebugTools_Eval_M1_99M

    JPG | 918 kb | 2126 x 1416 px

  • Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    Eval_M1_36_84A

    JPG | 1015 kb | 2126 x 1417 px

  • Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    Eval-M1-1302

    JPG | 935 kb | 2126 x 1417 px

  • Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    Using the iMotion™ Modular Application Design Kit, a full functioning motor system will be running in less than one hour, enabling fast time to market. Designers only need a few steps to run the motor: plug the cards into their PC, motor and grid, download, install and parameterize the software.
    Eval-M1-05-65D

    JPG | 1.15 mb | 2126 x 1416 px