How to program the microcontroller:
1. Build project in DAVE
2. Pack together the project folder into a .zip
(usually found in the workspace folder)
3. Click on the microcontroller symbol
4. Click on the "MCU-code" details
5. Select "Upload"
6. Select the .zip file created earlier
7. Click "Upload"
8. Click "OK"
This circuit boosts a voltage from 12V up to 24V with an output-power of 12W. The output
voltage is measured by the ADC of the XMC1100 and depends on the duty cycle of the
PWM-Signal.
The PWM-Signal is generated by the microcontroller. The frequency of the PWM-Signal is
32kHz and the duty cycle is controlled by a PI-controller.