The conference will take place at the headquarters of Infineon

Location

Infineon Technologies AG
Conference Zone, Building 2, 1st floor
Am Campeon 1-15
85579 Neubiberg near Munich
Germany
Visitor Information

GPS       

48° 4′ 45″ N |  11° 36′ 57″ O

How to get there

Campeon is located southeast of Munich, close to the freeway. It can also be reached using public transportation.

By car:
Take the Munich-Salzburg freeway A8, exit 92b (Neubiberg), follow the signs to “Campeon”. At the “Campeon” roundabout take the second exit to the big carpark next to building 2.

Visitors who arrive by taxis can be dropped off in front of the Visitor  Reception (Building 1) or at the Kubus Reception.

By public transportation:
Take the S3 [S-Bahn] which leaves to the city aerea in the direction of Holzkirchen/Deisenhofen (from Holzkirchen going towards Munich, take the S3 to Mammendorf). Exit the train at the Fasanenpark station; Campeon is about 300 m away. The pathway from the S-Bahn station to Campeon is entirely covered.