ITON
ITON Technology Corp. was established in 2006 and is headquartered in Shenzhen, China. ITON has an R&D team of over one hundred engineers with expertise in RF design, wireless connectivity, embedded systems, cloud connection middleware and mobile Application development. In addition to a strong R&D capability, ITON also maintains an Apple MFi manufacturing license.
Previously with Broadcom and now with Infineon, ITON has specializes in providing Wi-Fi, Bluetooth and Combo module solutions. Application support includes Bluetooth keyboard & mice, voice remote control, portable thermal printers, BLE mesh for appliance or industrial applications, STB and VoIP systems, phone accessories, etc. Leveraging their extensive offering, ITON's engineering team has accumulated over 10 years’ experience developing solutions with Infineon connectivity ICs.
Lastly, ITON has shipped over one hundred million of their Wi-Fi, Bluetooth and Combo modules globally, and will continue to take IoT customers of all sizes to production using their solutions that are now integrated into the Infineon partner ecosystem.
EVBs
Features:
- The ITON BB2706 Series Audio plus BLE EVB is a low-cost hardware platform that enables design and debug of CYW20706A2 Soc chip. It is integrated with a BB2706-32 module, NuvoTon NAU88C22 audio codec, 3 buttons and 2 LEDs.
- The PCM/I2S interface between the BB2706-32 module and internal Audio Codec can be easily disconnected by a jumper cap and then be connected to an external codec or the PCM/I2S interface of Client MCU, which is very easy to debug.
- The default ITON firmware used by the EVB implements A2DP sink and A2DP source applications. The A2DP sink mode and the A2DP source mode can be switched alternatively by pressing the mode button.
- There are three buttons and a knob with a button on the board, which is used to adjust volume and switch mode. Due to the limited number of GPIO, you can only choose either knob control or button control.
For more details, please contact us at sales@sziton.com.
Features:
- The ITON CW24XX-44P EVB Kit integrates a CW2438-44P or CW2455-44P module and STM32F412 MCU.
To match with a JTAG Tool provided by ITON, the Cypress WICED Studio can be used to debug code and download programs. - There are USB, SDIO, UART, PCM and other interfaces on the board, which can be extracted to external interface through 2.54mm pin header connectors. The SDIO signal between the MCU and the Wi-Fi module can be disconnected by DIP switch, which is very east to debug.
- Support for ThreadX and FreeRTOS real-time Operating Systems (RTOS), and NetX/NetXDuo IPv4/IPv6 and LwIP IPv4 TCP/IP network stack implementations via WICED Studio
Open On Chip Debugger (Open OCD)
For more details, please contact us at sales@sziton.com.
Features:
- The ITON Bluetooth SIG Mesh EVB Kit is consist of five sets of minimum system boards based on the BB1735-46 module, each of which is included with a white LED, RGB LED, Reset IC, HCI UART interface, PUART interface, reset button and user button.
- The default ITON firmware implements all Mesh features, such as supporting Proxy, relay, Friend, low power as well as the AT command over PUART developed by ITON. It is used to transfer data between any nodes through command operations, such as using the AT command to obtain all online node addresses, and send a message to specified device through the obtained node address.
- ITON provides technical support for APP SDK of Android and iOS versions. The DEMO APP enables Group operations (to create new, delte, switch group), scene, schedule, OTA, online/off line, fast provision, connect to network in batch, and etc.
For more details, please contact us at sales@sziton.com.
Bluetooth Modules
Bluetooth 5.0 BR/BLE
Size: 15.2 x 18.8 x 1.7mm
Chipset: CYW20735B1
Interfaces: UART, SPI, 6 x PWM
Highlights:
External antenna, no shield cover, 1.75~3.6V
384KB RAM, 4Mbit SPI flash, Max 12dBm (>100m)
SIG Mesh, Alexa Gadgets, BLE Device/Client (1 to 4), MFi
For more details, please contact us at sales@sziton.com.
Bluetooth 4.2 BR/EDR/BLE
Size: 10.1 x 6.0 x 1.2mm
Chipset: CYW20704
Interfaces: HCI over USB, HCI over UART
Highlights:
Bluetooth controller, Max 10dBm, 3.0~3.6V,
Linux, RTOS
For more details, please contact us at sales@sziton.com.
Bluetooth 5.0 BR/EDR/BLE
Size: 21.2 x 12.2 x 2.85mm
Chipset: CYW20706
Interfaces: UART, SPI, 4*PWM, I2S/PCM
Highlights:
PCB antenna, with shield cover, 2.7~3.6V,
352KB RAM,4 Mbit flash, Max 10 dBm
MFi, GATT, SPP, A2DP Sink, A2DP Source, HFP AG, HFP device
For more details, please contact us at sales@sziton.com.
Bluetooth 5.0 BR/EDR/BLE
Size: 15 x 12 x 2.17mm
Chipset: CYW20706
Interfaces: UART, SPI, 4*PWM, I2S/PCM
Highlights:
External antenna, no shield cover, 2.7~3.6V,
352KB RAM,4 Mbit flash, Max 10 dBm
MFi, GATT, SPP, A2DP Sink, A2DP Source, HFP AG, HFP device
For more details, please contact us at sales@sziton.com.
Wi-Fi Modules
2.4G 802.11b/g/n BR/EDR/BLE
Size: 12 x 12 x 1.7mm
Chipset: CYW43438
Interfaces: SDIO,UART
Highlights:
External Antenna, Host interfaces include SDIO/SPI for Wi-Fi, HCI for Bluetooth
Linux , Android, RTOS
For more details, please contact us at sales@sziton.com.
2.4G/5G 802.11b/g/n/ac BR/EDR/BLE
Size: 12 x 12 x 1.7mm
Chipset: CYW43455
Interfaces: SDIO,UART
Highlights:
External Antenna, Host interfaces include SDIO/SPI for Wi-Fi, HCI for Bluetooth
Linux, Android, RTOS
For more details, please contact us at sales@sziton.com.