The following Code Examples are integrated with CY3655 enCoRe II Development Kit.
| Title |
Part# |
Kits |
Description |
| DrawUSB Example |
CY7C63310,
CY7C638xx,
CY7C601xx,
CY7C602xx |
CY3655-EXT,
CY3668 |
DrawUSB example demonstrates the basic functionality of a USB HID mouse. The example application contains a USB HID mouse descriptor that works on any USB host with HID driver. This example application enumerates as a three button USB mouse (HID class) and moves the mouse cursor in the shape of the letters U, S, and B. It demonstrates the use of the USB User Module API. |
|
The following Code Examples are integrated with CY3664 enCoRe III Development Kit.
| Title |
Part# |
Kits |
Description |
| Bulk Example |
CY7C64215 |
CY3664-EXT |
This project demonstrates USB loopback using BULK endpoints. |
| HID Example |
CY7C64215 |
CY3664-EXT |
This project demonstrates the basic functionality of USB HID mouse. A complete USB HID descriptor is provided,which allows enumerations on any USB host that supports a HID class. |
| ISOC Example |
CY7C64215 |
CY3664-EXT |
This project shows how to create an alternate interface for isochronous applications. This example uses the streamer application to send data over ISOC IN endpoint. |
|
The following Code Examples are integrated with CY3660 enCoRe V Development Kit.
| Title |
Part# |
Kits |
Description |
| Bulk Example |
CY7C6434X |
CY3660,
CY3668 |
This project demonstrates USB loopback using BULK endpoints. |
| HID Example |
CY7C604XX |
CY3660,
CY3668 |
This project demonstrates the basic functionality of USB HID mouse. A complete USB HID descriptor is provided,which allows enumerations on any USB host that supports a HID class. |
| ISOC Example |
CY7C604XX |
CY3660,
CY3668 |
This project shows how to create an alternate interface for isochronous applications. This example uses the streamer application to send data over ISOC IN endpoint. |
| WUSB (Wireless USB) Example |
CY7C604XX |
CY3660,
CY3668 |
The WUSB_Example demonstrates the functionality of a WirelessUSB HID keyboard. Twodevelopment boards with LP radio modules are used for this example. One board is used as abridge, which enumerates on the PC as a bus-powered USB composite device supporting keyboardand mouse. The other board is used as a keyboard, which simulates a simple keyboard with threekeys (Num Lock key, Caps Lock key, and Scroll Lock key) and three LEDs (Num Lock LED, CapsLock LED, and Scroll Lock LED). |
|
The following Code Examples are integrated with CY3674 EZ-USB FX1 Development Kit.
| Title |
Part# |
Kits |
Description |
| hid_kb |
CY7C64713 |
CY3674 |
Example firmware that emulates a HID-class keyboard using the buttons and 7-segment display on the DVK board. |
| bulkloop |
CY7C64713 |
CY3674 |
Contains a bulk loopback test that exercises the EZ-USB bulk endpoints. It loops back EP2OUT to EP6IN and EP4OUT to EP8IN. |
| bulkext |
CY7C64713 |
CY3674 |
Contains a bulk loopback test that exercises the EZ-USB bulk endpoints. The loopback is performed using the external auto pointer. Data is copied from the OUT endpoint buffer to external RAM and then to the IN endpoint buffer. It loops back EP2OUT to EP6IN and EP4OUT to EP8IN. |
| bulksrc |
CY7C64713 |
CY3674 |
Contains bulk endpoint endless source/sink firmware. It can be driven using the CyConsole or CyBulk. EP2OUT always accepts a bulk OUT; EP4OUT always accept a bulk OUT; EP6IN always returns a 512-byte packet, 64 bytes at full-speed. Based on buffer availability in EP8IN, the most recent packet of EP4OUT is written to EP8IN. |
| dev_io |
CY7C64713 |
CY3674 |
Contains the source files to build simple development board I/O sample. This software demonstrates how to use the buttons and LED on the EZ-USB development kit. |
| EP_Interrupts |
CY7C64713 |
CY3674 |
Bulk loopback firmware that demonstrates use of endpoint interrupts using EZ-USB FX2LP. |
| extr_intr |
CY7C64713 |
CY3674 |
Firmware that demonstrates external interrupt handling INT0, INT1, INT4, INT5 and INT6. |
| Ibn |
CY7C64713 |
CY3674 |
Contains firmware to perform bulk loopback of EP2OUT to EP6IN and EP4OUT to EP8IN using the IBN (In Bulk Nak) interrupt to initiate the transfer. |
| LEDCycle |
CY7C64713 |
CY3674 |
Simple firmware example to demonstrate use of the general purpose indicator LEDs (D2, D3, D4, D5) on the Development Kit board. |
| Pingnak |
CY7C64713 |
CY3674 |
Contains firmware to perform bulk loopback of EP2OUT to EP6IN and EP4OUT to EP8IN using the PING NAK interrupt to initiate the transfer. |
| iMemtest |
CY7C64713 |
CY3674 |
Memory test firmware example. Tests on-chip RAM. |
| vend_ax |
CY7C64713 |
CY3674 |
Contains the source files to build a vendor specific command sample. This example demonstrates how to implement different vendor commands. |
|
The following Code Examples are integrated with USB-Serial Software Development Kit , CYUSBS232 Reference Design Kit, CYUSBS234 Development Kit and CYUSBS236 Development Kit. To access these code examples, follow the path \\1.0\Examples
| Title |
Part# |
Kits |
Description |
Device
Enumeration |
CY7C64225,CY7C65213,
CY7C65211,CY7C65215 |
CYUSBS232,
CYUSBS234,
CYUSBS236 |
This host application demonstrate how to enumerate USB-Serial devices using the cyusbserial API and display device details. |
| UART |
CY7C64225,CY7C65213,
CY7C65211,CY7C65215 |
CYUSBS232,
CYUSBS234,
CYUSBS236 |
This host application demonstrates how to communicate with UART on the USB-Serial RDK/DVK using the cyusbserial API. |
| I2C Master |
CY7C65211,CY7C65215 |
CYUSBS234,
CYUSBS236 |
This host application demonstrates how to communicate with EEPROM connected to I2C on the USB-Serial DVK using the cyusbserial API. |
| SPI Master |
CY7C65211,CY7C65215 |
CYUSBS234,
CYUSBS236 |
This host application demonstrates how to communicate with EEPROM connected to SPI on the USB-Serial DVK using the cyusbserial API.of EP4OUT is written to EP8IN. |
| GPIO Control |
CY7C65213,CY7C65211,
CY7C65215 |
CYUSBS232,
CYUSBS234,
CYUSBS236 |
This host application demonstrates how to configure the GPIOs available on USB-Serial device using the cyusbserial API. |
|