Safe Through Night and Fog: Market Leader Infineon Delivers Ten Millionth Radar Chip for Cars
Munich, Germany – July 28, 2015 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) announced that it has shipped its ten millionth high-frequency radar chip. The 77-GHz chips are used in radar-based driver assistance systems that recognize objects at ranges of up to 250 meters. Infineon estimates that in the year 2014 nearly 50 percent of 77-GHz radar systems in vehicles were equipped with Infineon technology.
In a recent study, the market research firm IHS Technology declared Infineon the global market leader in 77-GHz chips, which is the standard frequency range for radar applications such as adaptive cruise control and collision warning. The first ten million of these radar chips from Infineon were primarily built into premium and luxury vehicles over the past six years. Infineon anticipates increasing demand and expects that, within the next year, up to ten million radar chips will also be used in mid-sized and compact cars. This means that statistically one out of every twenty cars will be using a driver assistance system with a 77-GHz radar chip from Infineon.
The market research firm Strategy Analytics also confirmed this trend towards safety systems in cars. They expect that in the next five years applications such as distance warning systems and automatic emergency braking will grow by more than 25 percent annually. This growth is in part attributable to the rating scheme from the independent organization Euro NCAP (European New Car Assessment Programme), that reviews the safety of new vehicles sold in Europe. To achieve the highest rating of five stars a new car must have a radar-based driver assistance system. Strategy Analytics forecasts that of the 105 million new vehicles expected to be built in 2020 more than 20 million will use a radar-based distance warning system. That would mean that about 20 percent of all new vehicles worldwide would be equipped with such a system.
”Our chips make driver assistance systems increasingly accurate and more cost-effective,” says Jochen Hanebeck, President of the Automotive division at Infineon Technologies AG. ”Radar-based driver assistance systems using Infineon chips now are becoming the standard in mid-range and compact cars. They are an important growth market for Infineon. Our high system knowledge and close cooperation with leading system suppliers and car manufacturers around the world are key elements to our success,” says Hanebeck.
Broad product portfolio for radar-based driver assistance systems from short to long vicinity range
Even in poor visibility situations, radar chips in the 77-GHz range make it possible for vehicles to ”recognize” other road users at a distance of up to 250 meters (approx. 275 yards). This allows a car to indicate a hazardous traffic situation in time and brake automatically. If radar-based driver assistance systems continue to become widely adopted, then those dreaded collisions you get when stuck in a traffic jam – especially around vacation time – could well be a thing of the past.
In addition to 77-GHz radar chips for active safety systems, Infineon also offers radar chips in the 24-GHz frequency range for distances up to 100 meters (approx. 110 yards). 24-GHz radar chips are most often used to monitor the blind spot. With them, the radar system alerts drivers to vehicles behind them when passing or changing lanes. When parking, the radar detects cross-traffic in the rear and prevents collisions.
How radar technology works in the car
A vehicle driver assistance radar system sends out radio-frequency electromagnetic waves, which are reflected back by vehicles or other objects ahead. Radar chips of Infineon send and receive these high-frequency signals and pass them on to the radar electronic control unit (ECU). The radar ECU then determines the distance of the car to other vehicles and their speed in order to warn the driver in good time and to initiate the braking maneuver in case of emergency.
“Made in Germany” innovation
Ever since 2009, Infineon manufactures its radar chips in Regensburg, the company’s innovation center for high frequency technology in Germany. Here the radar chips are integrated in special chip packaging and tested. The use of the silicon germanium manufacturing technology developed by Infineon helps make radar sensor systems that are more compact and cost-effective.
For more information
You can find more information on Euro NCAP at www.euroncap.com
Technical information about radar chips from Infineon is available at www.infineon.com/radar, www.infineon.com/rasic and www.infineon.com/shortrange-radar
About Infineon
Infineon Technologies AG is a world leader in semiconductors. Infineon offers products and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2014 fiscal year (ending September 30), the company reported sales of Euro 4.3 billion with about 29,800 employees worldwide. In January 2015, Infineon acquired US-based International Rectifier Corporation, a leading provider of power management technology, with revenues of USD 1.1 billion (fiscal year 2014 ending June 29) and approximately 4,200 employees.
Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).
Follow us: twitter.com/Infineon - facebook.com/Infineon - plus.google.com/+Infineon
Information Number
INFATV201507-073
Press Photos
-
Jochen Hanebeck, President of the Automotive division at Infineon Technologies AGHanebeck_JochenJPG | 323 kb | 823 x 1140 px