Infineon SEMPER™ NOR Flash memory family achieves ASIL-D functional safety certification
Munich, Germany – 8 May , 2025 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced that SGS-TÜV has certified Infineon’s industry-leading SEMPER™ NOR Flash memory to ASIL-D, the highest certification level for functional safety. Following a detailed analysis of product safety documentation under the ISO 26262:2018 standard, external experts from this leading assurance organization have validated that SEMPER devices meet the most stringent safety performance targets for automotive applications.
With the rapid emergence of software-defined vehicles where microelectronic components drive vehicle functionality, performance, and safety, global OEMs and regulators insist on the highest levels of safety in electronic systems, from motor control and battery management to advanced driver assistance and autonomous driving.
“Automotive electronics require the highest levels of functional safety and reliability, and the ASIL-D certification of our SEMPER NOR Flash devices demonstrates our commitment to providing the best memory products for the automotive industry,” said Rainer Hoehler, Senior Vice President and General Manager, Memory Solutions, Infineon. “Infineon is the world leader in automotive NOR Flash memory products and was the first NOR manufacturer to launch products developed in compliance with the ISO26262 functional safety standard. We are proud that the experts at SGS-TÜV have certified our achievements in functional safety and invite our customers to design SEMPER NOR products into their most demanding applications.”
The ASIL-D certification applies to the full range of SEMPER NOR products, including QSPI, HYPERBUS™, and JEDEC xSPI octal interfaces; 256-megabit to 2-gigabit densities; and BGA, WSON, and SOIC packages. These products are qualified to AEC-Q100 grade 1 standard and are widely deployed today in automotive applications including ADAS, zone control, gateway, and digital cockpit. To streamline the integration of functional safety features into customer systems, Infineon offers the Memory Solutions Hub web portal and the “SEMPER SDK Safe” software development package, both available at infineon.com.
Availability
ASIL-D certified SEMPER products, including the S25HS/HL-T QSPI family, S26HS/HL-T HYPERBUS family, and S28HS/HL-T JEDEC xSPI octal family, are available today from Infineon and its authorized distributors. Infineon offers the industry’s broadest array of specialty memory products and technologies, including NOR Flash, SRAM, FRAM, nvSRAM, and HYPERRAM™ devices, to serve the widest array of applications across automotive, industrial, and data center markets. For high-reliability applications, the company also offers a wide range of radiation-tolerant and radiation-hardened memory products.
For more information about Infineon memory products, visit https://www.infineon.com/cms/en/product/memories/.
About Infineon
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The Company had around 58,060 employees worldwide (end of September 2024) and generated revenue of about €15 billion in the 2024 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Information Number
INFATV202505-101
Press Photos
-
The ASIL-D certification applies to the full range of Infineon SEMPER™ NOR products.Infineon_SEMPER_NOR_flash_BGA-24_8x8
JPG | 517 kb | 2126 x 1098 px