Strengthening the power of collaboration: Zwipe and Infineon extend their partnership
Munich, Germany, and Oslo, Norway – 18 June 2019 – Biometric technology company Zwipe and the world’s leading provider of semiconductor solutions in the payments market, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY), have extended their partnership through a long-term agreement. The cooperation is non-exclusive. The agreement outlines both technical and commercial collaboration between the two companies. The two parties will co-define and develop advanced system-on-chip solutions and related card system designs for mass deployment of biometric smart devices, including payment cards and wearables.
The cooperation is concentrating on so called “Tap and go payments” with biometric cards which are gaining in popularity. They can significantly improve the user experience without compromising on security while meeting the strong customer authentication (SCA) requirements demanded by the second Payment Service Directive (PSD2) in Europe.
Zwipe and Infineon have a long-standing relationship. Infineon’s Secure Element is now deployed in all pilot projects featuring Zwipe’s biometric payment platform, currently supporting multiple leading payment networks run by 12 major banks in various countries across Europe and the Middle East. Card manufacturers plan to certify fully biometric payment cards and make them commercially available this year.
Commenting on this partnership, André Løvestam, CEO of Zwipe, said, “We are proud to strengthen our long-standing partnership with a global technology leader such as Infineon. This collaboration further enhances our ability to commercialize our technology and IP through competitive solutions for mass-volume deployment.” Bjoern Scharfen, Head of Payment & Wearables at Infineon added, “Our collaboration and joint offering with Zwipe is a key accelerator of mass deployment in the biometric payment market.”
Working together, the two technology companies will seek to develop advanced integrated solutions optimized to the volume requirements of biometric dual-interface payment cards. The platforms being developed combine simplified card design with reduced bill of material.
About Zwipe
Zwipe is a technology solution provider that enables battery-less, ultra-low-power, self-contained biometric authentication solutions. Together with an ecosystem of partners including global brands within security, financial services and ID applications, Zwipe is “Making Convenience Secure™” for banks, merchants and consumers.
Using advanced fingerprint recognition while protecting personal information, Zwipe’s solutions address the data theft pitfalls inherent in traditional authentication methods. Headquartered in Oslo, Norway, Zwipe has spent the last 10 years developing its unique power harvesting technology platform in combination with security solutions based on international infrastructure standards. To learn more, visit www.zwipe.com
Media Contact Zwipe:
André Løvestam, CEO
+47 930 44 040
info@zwipe.com
Information Number
INFDSS201906-079
Press Photos
-
Zwipe and Infineon are extending their partnership. Together, the two technology companies will seek to develop advanced integrated solutions optimized to the volume requirements of biometric dual-interface payment cards.zwipe_and_infineonJPG | 974 kb | 2126 x 1195 px
-
Zwipe and Infineon are extending their partnership. Together, the two technology companies will seek to develop advanced integrated solutions optimized to the volume requirements of biometric dual-interface payment cards.zwipe_paymentJPG | 1.48 mb | 2000 x 1333 px