Vehicle communication: Infineon and Elektrobit improve data security in the car
Erlangen and Munich, 27 February 2018 – New features in the car require electronic control units that are networked, with each other and the cloud. Embedded IT security is a vital aspect in that. That goes for assistance systems, updating software over the air (SOTA) and autonomous driving functions. Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and Elektrobit Automotive GmbH (EB) are teaming up long term to work closely together on the issue of cybersecurity for vehicles. The companies offer a perfectly coordinated hardware-software solution that boosts the performance of on-board communication and satisfies current and future security requirements. It is based on the second generation of the multicore microcontroller family AURIX™ (TC3xx) from Infineon and, tailored to it, Elektrobit’s zentur HSM solution.
The microcontrollers from the AURIX family control communication processes, carry out monitoring and security tasks, and support security protocols in the vehicle. Every TC3xx microcontroller now has an integrated hardware security module (HSM), where the keys are generated and stored securely. The HSM uses hardware-based symmetric and asymmetric encryption algorithms as well as hash functions (AES-128, ECC 256, SHA2). As a result, the HSM not only enhances protection against manipulation, but also ensures a significant increase in speed. Thanks to hardware support, hash calculation (SHA256) is around 150 times faster than with a pure software solution.
That has a direct impact on RSA signature verification – an advantage when there are large volumes of data, as in applications such as SOTA and autonomous driving. The hardware-software combination – AURIX and EB’s zentur HSM – also enables more than 100 signature verifications per second (with ECDSA secp256r1, for example). In a current software implementation of RSA signatures, verification can take several seconds – depending on the key length and size of the data.
“AURIX microcontrollers are key components in current and future vehicles,” says Thomas Böhm, Senior Director, Chassis & ADAS Microcontrollers at Infineon. “The combination of AURIX and a coordinated software stack will ensure greater IT security in the vehicle and deliver a sharp increase in performance for system suppliers.”
The hardware-software solution is AUTOSAR-compliant with regard to the latest 4.3 stack and prior versions such as 4.2 and 4.0. That means it is easy to implement and integrate EB’s zentur HSM software in existing projects.
Secure Boot is the basis for all subsequent security functions. It is a time-critical function that demands a great deal of computing power, since the individual control units must log on to the network in a very short space of time. When the systems are booted, the memory contents are checked for any manipulation. Thanks to the hardware-software solution, CMAC values of 62 MB/s are achieved. Elektrobit’s software stack, which has been tuned specially to AURIX and the HSM, thus allows 1 MB of data to be checked in 16.2 ms. No other vendor in the industry achieves that performance, which is two-and-a-half-times the best value recorded to date.
“The growing complexity of software and steadily increasing number of on-board systems and sensors that communicate with each other in a vehicle mean that efficient security mechanisms to prevent unauthorized external access are indispensable,” says Martin Schleicher, Executive Vice President Business Management at EB. “Thanks to Infineon’s hardware know-how and our experience in developing software security solutions, we’ve jointly been able to create an ideal solution that protects control units reliably.”
More information
Information on AURIX can be found at www.infineon.com/aurix
Information on EB zentur HSM firmware can be found at https://www.elektrobit.com/products/ecu/technologies/security/hardware-specific/
About Elektrobit (EB)
Elektrobit (EB) is an award-winning and visionary global supplier of embedded and connected software products and services for the automotive industry. A leader in automotive software with over 30 years serving the industry, EB’s software powers over 1 billion devices in more than 90 million vehicles and offers flexible, innovative solutions for connected car infrastructure, human machine interface (HMI) technologies, navigation, driver assistance, electronic control units (ECUs), and software engineering services. EB is a subsidiary of Continental.
Learn more by visiting us at elektrobit.com
Press contact for Elektrobit
Nicole Donhauser
Head of Marketing & Communications
Phone: +49 9131 7701-6446
Mobile: +49 173 532 03 27
E-mail: Nicole.Donhauser@elektrobit.com
Stephannie Depa
Breakaway Communications for EB
Phone: +1 415 358-2485
Mobile: +1 530 864-0136
Email: sdepa@breakawaycom.com
Philipp Hanke
Weber Shandwick for EB
Phone: +49 89 380179-48
E-mail: PHanke@WeberShandwick.com
Information Number
INFATV201802-036
Press Photos
-
Thomas Böhm, Senior Director, Chassis & ADAS Microcontrollers, Infineon Technologies AG: “The combination of AURIX and a coordinated software stack will ensure greater IT security in the vehicle and deliver a sharp increase in performance for system suppliers.”Thomas_Boehm_InfineonJPG | 810 kb | 1024 x 1535 px
-
“The growing complexity of software and steadily increasing number of on-board systems and sensors that communicate with each other in a vehicle mean that efficient security mechanisms to prevent unauthorized external access are indispensable,” says Martin Schleicher, Executive Vice President Business Management at Elektrobit.Martin_SchleicherJPG | 403 kb | 2126 x 1417 px