Online prototyping made easy with Infineon Designer

Oct 27, 2016 | Market News

Munich, Germany – October 27, 2016 – Starting at electronica 2016, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) introduces Infineon Designer: the first online prototyping engine combining analog and digital simulation functionalities in an internet application. Requiring a web browser only, it is a perfect match for supporting customers in selecting the right product for a defined application. Infineon Designer works intuitively in a very short time, and neither installation nor licenses are needed.

Infineon Designer features a wealth of application circuits in the domain of Industrial Power, Lighting, Motor Control and Mobile/RF frontend design. It enables analog/digital co-simulation of the 32-bit XMC1000 industrial microcontroller ARM® Cortex®-M0 series, using the free-of-charge code generation platform DAVE™. The digital prototyping engine Infineon Designer aims at making the transition from idea to functional system as smooth and fast as possible. It allows for prototyping a “soft evaluation board” with all functional parameters. In an early stage, hardware for testing and iterations can thus be saved.

The prototyping tool is based on the easy-to-use TINACloud environment from DesignSoft, who partnered with Infineon in this project. TINACloud is the online version of the TINA circuit simulation software running on multiple platforms such as PC, laptop, mobile, and tablets. Analog circuits are modeled in SPICE and can be co-simulated with digital systems using hardware description languages such as VHDL and Verilog or C language. For a greater market penetration, the frontend supports multiple languages.

Infineon Designer can be accessed at www.infineon.com/ifxdesigner by November 8, 2016. At electronica 2016, Infineon will demonstrate the functionality of the prototyping engine with Arduino shields for lighting and motor control applications and compare the results with real hardware. The demonstration is part of the “Maker’s corner”.

Infineon at electronica 2016 (November 8–11, 2016, Munich, Germany)

The world is getting smarter and more connected by the day. At electronica 2016 Infineon presents exciting demos and product solutions that are making tomorrow’s cars, factories and homes smart, secure and energy-efficient. New products and demos can be discovered at booth 506 in hall A5; in-depth knowledge is offered through expert talks at the Infineon IoT Security Circle. Further information about this fair’s highlights is available at www.infineon.com/electronica.

Information Number

INFXX201610-008

Press Photos

  • Infineon Designer is the first online prototyping engine combining analog and digital simulation functionalities in an internet application. It features a wealth of application circuits in the domain of Industrial Power, Lighting, Motor Control and Mobile/RF frontend design.
    Infineon Designer is the first online prototyping engine combining analog and digital simulation functionalities in an internet application. It features a wealth of application circuits in the domain of Industrial Power, Lighting, Motor Control and Mobile/RF frontend design.
    Infineon-Designer

    JPG | 838 kb | 2126 x 1535 px