The Digital Power Explorer Kit of Infineon and Würth Elektronik provides easy entry into digital power control with XMC™ microcontrollers

May 11, 2016 | Market News

Munich and Waldenburg, Germany – May 11, 2016 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and Würth Elektronik eiSos present an easy and affordable entry into digital power control applications. The Digital Power Explorer Kit was developed for analog power supply designers and embedded software programmers to help them better understand and implement the capabilities of digital power control based on standard microcontrollers. Today, digital power control is well-established in the server und telecommunication power supplies and is proliferating in a much broader range of industrial products and applications, such as SMPS and motor control. As a complete out-of-the-box solution the Digital Power Explorer Kit brings together easy-to-use hardware and software that is based on the Infineon development platform DAVE™.

Analog performance with digital flexibility

The new XMC Digital Power Explorer Kit features two XMC microcontroller families which are tailored to digital power applications. Also, it includes power electronic components of Infineon such as 30 V Dual N-channel BSC0924NDI OptiMOS™ MOSFETs, IRS2011S gate drivers as well as IFX1763XEJ V33 and IFX90121EL V50 voltage regulators. Würth Elektronik’s new range of high performance capacitors, magnetics and other passive components integrated on this kit are carefully selected to provide optimal performance and robustness of the power supply board.

The power supply board features synchronous buck converter with on-board resistive load banks that can be switched between 10, 55 and 100 percent of the maximum load so that the transient response and the quality of the control loop under different load conditions can be easily tested. The kit also includes two control card options: the XMC1300 control card (with XMC1300 using the ARM® Cortex®-M0 processor) and the XMC4200 control card (using ARM® Cortex®-M4F). The isolated on-board debugger allows designers to easily evaluate both XMC microcontroller families and make the right price/performance choice for their application.

The XMC Digital Power Explorer Kit is available now. For further information and order details please go to www.infineon.com/xmc_dp_exp.

Further information on the XMC microcontrollers and DAVE is available at www.infineon.com/xmc and at www.infineon.com/dave.

Infineon will demonstrate the XMC Digital Power Explorer Kit at booth #412 in Hall 9 at the PCIM tradeshow (Nuremberg, Germany, May 10-12, 2016). An overview of Infineon‘s further PCIM show highlights is available at www.infineon.com/pcim.

Information Number

INFPMM201605-057

Press Photos

  • The Digital Power Explorer Kit of Infineon and Würth Elektronik provides easy entry into digital power control with XMC™ microcontrollers
    The Digital Power Explorer Kit of Infineon and Würth Elektronik provides easy entry into digital power control with XMC™ microcontrollers
    XMC_Digital_Power_Board

    JPG | 364 kb | 1500 x 1203 px