bauma 2016: Infineon increases safety and efficiency in trucks and construction vehicles and enables platooning

Apr 11, 2016 | Market News

Munich, Germany – April 11, 2016 – Radar systems in trucks and construction vehicles play an important role in increasing the safety of road transport. Because they monitor blind spots, alert drivers if they come too close to other road users and automatically initiate the braking process in case of emergency. Radar systems make it safe to drive in columns with short following distances. They can do this even at night, with glaring sunlight, during rain, fog or a snowstorm. These active safety systems can prevent accidents between turning trucks and bicyclists or pedestrians. And the necessary increases in productivity in the construction and logistics industries also become reality with chip-based assistance systems: Trucks and construction vehicles reach their destination faster, can be maneuvered more quickly and feature optimal loading and unloading.

At bauma 2016 in Munich, Infineon presents its latest 24-GHz radar solution, which was developed for the modern, radar-based assistance systems in trucks and construction machines. It is a highly integrated system, which contains not only the 24-GHz radar chip (BGT24ATR12) but also the corresponding AURIX™ microcontroller, specifically customized for radar applications (TC264DA), and the appropriate power supply (TLF35584).

Thanks to semiconductor solutions of Infineon, radar-based assistance systems are becoming more compact and cheaper to install. By 2020, the amount of such systems could be increased significantly, not only in the approximately 3.6 million produced trucks expected then, but also in busses, agricultural vehicles, construction and mining machines and in cars.

Chips for safe and precise assistance systems

Infineon’s radar chips send and receive the high-frequency 24-GHz signals and transmit them to the AURIX microcontroller in the radar electronic control unit for further processing. The AURIX ensures the reliable and quick processing of the information, which the radar chip captures around the vehicle and transmits to the driving assistance system.

Because the AURIX is so efficient, 24-GHz radar systems will be more compact, smaller and cheaper than today, since it will be possible to dispense with other chips that were previously needed. These redundant chips include, for example, the digital signal processor, memory chips and various analog-digital converters, which change the radar chip’s analog signals into digital signals that can be processed by the microcontroller. All members of the AURIX family have a very high data processing rate and thus a high real-time performance; they are among the best microcontrollers currently available on the market.

Infineon at bauma

At bauma 2016 in Munich (April 11-17, 2016), Infineon will present such products as the 24-GHz developer kit for assistance systems for trucks and construction machines. The kit can also be used to test the newly developed system.

More information at www.infineon.com/bauma

The product portfolio of Infineon for functional vehicles, construction and agricultural machines is available at www.infineon.com/cav and technical information about the AURIX at www.infineon.com/aurix

Information Number

INFATV201604-045