Infineon’s New Security Chip Solution Protects Connected Electronics
Neubiberg, Germany – March 31st, 2014 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced its OPTIGA™ Trust P, a programmable hardware-based solution for improved security of electronic devices in connected systems. The addition to the OPTIGA Trust family provides robust device authentication, protects computing systems from both intentional attacks and accidental damage from user error, and enhances security and privacy of stored data.
Allowing the connection to only known, legitimate devices is a key element to any system security, and it becomes crucial when there are more and more connected devices used by enterprises and consumers. By integrating the OPTIGA Trust P into their designs, electronics manufacturers add a security safe to their embedded system.
The OPTIGA Trust P generates and securely stores encryption keys for one-way and mutual authentication, thereby allowing to protect the device from malware, and to control access mechanisms for secure software updates. The programmability of the OPTIGA Trust P makes it a highly flexible solution, enabling these features to be adapted by a wide variety of connected systems. Any product that stores and exchanges confidential data - whether used in smart homes or factories - can rely on the encrypted communications capability of OPTIGA Trust P to enable information privacy. This helps to defend from attackers trying to obtain personal or company data or attempting to tamper with programming through Internet connections or machine-to-machine (M2M) communications links.
“The new addition to our OPTIGA Trust product series goes beyond brand protection and fighting counterfeit electronics which harm both ordinary people and companies,” said Juergen Spaenkuch, Vice President and head of Platform Security at Infineon Technologies. “It helps protect industrial electronics systems from risks of sabotage, provide secure updates of software and improve security through access control to increasing connected systems like the Internet of Things (IoT).”
OPTIGA™ Trust P Features
The OPTIGA Trust P is a Common Criteria EAL 5+ (high) certified secure trust anchor that addresses counterfeiting, privacy and security concerns. It uses public key cryptography to support both one-way and mutual authentication for anti-cloning applications. On-board key generation, key storage and secure key exchange allow creation of a secure communications channel and encryption of transmitted data. This can provide data privacy as well as the information verification between senders and receivers. The integrated key management and the access controls expand the use of the secure channel to encompass protection by permitting for secure remote updates and local access restrictions to the devices.
As a programmable device, the OPTIGA Trust P is very flexible and easy to integrate into existing systems. It includes a JavaCard operating system to run security applets that can be configured for the specific needs of the system. Infineon provides the reference JavaCard security applets for most common functions, host code, and development tools to minimize development efforts.
Product Data, Availability
The OPTIGA Trust P SLJ 52ACA authentication chip is offered in a VQFN-32 (5mm x 5mm) package, with 150 kB memory. It runs the JavaCard OS, supports ECC, RSA, AES, TDES and SHA cryptography and its system interface is an ISO7816 UART (400 kbps data rate).
Samples are available now. Further information is available at www.infineon.com/optiga-trust
About OPTIGA™
Infineon's OPTIGA™ embedded security chips provide different levels of security for electronic systems, ranging from complex IT-infrastructures with many servers and computers to single systems that consist of the device and the suitable accessory, such as a MP3 player and headphones. The chips are embedded in the electronic devices and authenticate the individual elements of the system. Because security requirements vary depending on the application, Infineon offers different product families including OPTIGA™ TPM, which secures the system integrity of IT networks and OPTIGA™ Trust for secure device authentication.
About Infineon
Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2013 fiscal year (ending September 30), the Company reported sales of Euro 3.84 billion with around 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).Further information is available at www.infineon.com
Information Number
INFCCS201403.032
Press Photos
-
Infineon's new OPTIGA Trust P provides robust device authentication, protects computing systems from both intentional attacks and accidental damage from user error, and enhances security and privacy of stored data.OPTIGA_Trust_PJPG | 540 kb | 2550 x 1650 px
-
Juergen Spaenkuch, Vice President and head of Platform Security at Infineon Technologies' Chip Card & Security Division.Juergen_SpaenkuchJPG | 528 kb | 1494 x 2244 px