Easy Switch from 8-Bit to 32-Bit with Infineon XMC1000 Microcontrollers: Launch of XMC1000 Volume Production; Offering of New, Compact Package Variants and a Free ARM® MDK Development Tool
Munich and Nuremberg, Germany – February 25, 2014 – The Embedded World Exhibition & Conference 2014 will see Infineon Technologies launching volume production of its XMC1000 microcontrollers that offer 32-bit performance at 8-bit prices and use the ARM® Cortex™-M0 processor. At the same time, Infineon will be presenting new, highly compact VQFN (Very Thin Quad Flat No Leads) package variants for the XMC1000 family and providing information on their new, free ARM® Microcontroller Development Kit (MDK). The XMC1000 microcontrollers are consistently optimized in line with their target applications: sensor and actuator applications, LED lighting, simple motor drives (e.g. for household appliances, pumps, fans) and digital power conversion (such as uninterruptible power supplies).
“With the XMC1000 microcontrollers, Infineon is creating a decisive incentive for switching architecture from 8 to 32 bit – particularly for motor drives, sensor and actuator applications that need to be highly compact”, says Maurizio Skerlj, Senior Director, Industrial and Multimarket Microcontrollers at Infineon Technologies AG. “No rival microcontroller of the XMC1000 in a VQFN-24 package currently offers this much functionality in such a confined space.”
With the new VQFN packages featuring 24 pins and 40 pins, Infineon is extending its portfolio for XMC1000 industrial microcontrollers, which currently includes more than 30 products. XMC1000 microcontrollers in the VQFN-24 package are only 4 mm x 4 mm in size. No one in the market currently offers this much functionality in such a small package, such as for example up to 200KB flash memory and application-optimized control peripherals. This makes the XMC1000 microcontrollers ideally suited for motor drives as well as sensor and actuator applications that need to have a highly compact design. In addition to the VQFN packages, the XMC1000 MCUs are also available in TSSOP packages with 16, 28 and 38 pins.
The XMC1000 family: 32-bit performance at 8-bit prices
The XMC1000 family addresses industrial applications which, to date, were reserved for 8-bit MCUs. The three series XMC1100 (Entry series), XMC1200 (Feature series) and XMC1300 (Control series) differ essentially in terms of their memory capacity and peripheral set. Their flash sizes range between 8KB and 200KB, which is a far broader memory range than is usual today for 8-bit MCUs used in industrial applications. In addition, the XMC1000 MCUs feature high-performance PWM timers, 12-bit A/D converters and programmable serial communication interfaces. All XMC1200 derivates feature e.g. a module for touch control and LED displays and a peripheral unit for the dimming and colour control of LEDs – otherwise known as the Brightness and Colour Control Unit (BCCU). The XMC1300 series has a mathematical coprocessor specifically for motor drive controls. In addition, the microcontrollers of the XMC1000 family (as well as those of the XMC4000 family) satisfy the requirements of the standard IEC60730 Class B, which is prescribed for the safety of household appliances sold in Europe. For example, XMC MCUs offer hardware error correction (ECC) and corresponding memory tests. A further unique feature is the flash loader with a 128-bit AES accelerator, which allows the software IP – so important especially in cost-sensitive applications – to be better protected.
Launch of XMC1000 series production, availability of development kits and ARM® MDK
For all XMC1000 series, volume production in TSSOP package variants with 16, 28 and 38 pins is already underway. Samples for VQFN-24 packages are available. Series production for both packages VQFN-24 and VQFN-40 is due to commence from Q4 2014.
Boot kits are available for all the XMC1000 series for simple and low-cost evaluation in addition to more comprehensive application kits for the XMC1000 target applications. The XMC MCUs are supported by powerful software tools and ready-made software solutions from third-party suppliers and Infineon. In addition, Infineon has licensed the “Silicon Vendor Edition” of the ARM® Microcontroller Development Kit (MDK). Developers of embedded software can download the ARM MDK free from www2.keil.com/infineon/mdk. The free licence comprises all the tools for the development of XMC1000 applications up to a code size of 128KB. An application library developed with DAVE™ can be imported with a few simple clicks via CMSIS-PACK interface into the ARM MDK.
Develop faster with DAVE™
DAVE is a free, integrated development platform for all XMC microcontrollers. Using DAVE, it is possible to develop an application library quickly, which abstracts all the hardware-related tasks and also offers middleware solutions. The some 170 plus DAVE apps currently available make it possible to combine and configure software components, to map these automatically to the available microcontroller resources and to generate the C code for an application library. The C code generated in this way can then either be further used within DAVE with the integrated GNU compiler and debugger for developing the application, or it can be imported into a third-party tool, such as for example ARM MDK, Atollic TrueStudio, IAR EWARM, TASKING or Rowley.
Further information
Further information on the products of the XMC1000 and XMC4000 families is available at www.infineon.com/xmc. DAVE is available as a free download from the Infineon website at www.infineon.com/dave.
Infineon will be presenting its novelties relating to XMC1000 and XMC4000 and further microcontroller topics at the Embedded World Exhibition & Conference (February 25-27, 2014, in Nuremberg, Germany) in Hall 4, Stand 550.
Further information on other exhibition highlights is available at www.infineon.com/embeddedworld
About Infineon
Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2013 fiscal year (ending September 30), the Company reported sales of Euro 3.84 billion with around 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).Further information is available at www.infineon.com
Information Number
INFATV201402.025
Press Photos
-
Maurizio Skerlj, Senior Director, Industrial and Multimarket Microcontrollers, Infineon Technologies AGMaurizio_Skerlj_0214JPG | 1.45 mb | 1417 x 2126 px
-
The 32-bit microcontroller family XMC1000 for low-end industrial applications offers 32-bit power for 8-bit prices. It addresses sensor and actuator applications, LED lighting, digital power conversion, such as uninterruptible power supplies, and simple motor drives, such as those used in household appliances, pumps and fans.XMC1000_Visual_package_overview_0214JPG | 1.4 mb | 1535 x 2126 px
-
The 32-bit XMC1000 family addresses industrial applications which, to date, were reserved for 8-bit MCUs.XMC1000_package_overview_ plain_0214JPG | 680 kb | 2126 x 1535 px
-
The 32-bit XMC1000 family addresses industrial applications which, to date, were reserved for 8-bit MCUs.XMC1000_package_overview_0214JPG | 4.39 mb | 2598 x 3602 px
-
The 32-bit XMC1000 family addresses industrial applications which, to date, were reserved for 8-bit MCUs.XMC_Class_B_0214JPG | 1.59 mb | 2126 x 1535 px