Infineon Introduces CoolMOS™ C7; Significant Step in Superjunction Technology Bringing the World’s Lowest RDS(on) to Hard Switching Applications

May 6, 2013 | Market News

Neubiberg, Germany - May 6, 2013 - Infineon Technologies (FSE: IFX / OTCQX: IFNNY) expands its High Voltage portfolio with CoolMOS™ C7, introducing a new 650V Superjunction MOSFET technology. The new C7 product family provides Best-in-Class R DS(on) for all standard packages and - thanks to its low switching losses - efficiency improvements over the full load range. C7 is optimized for hard switching topologies such as Continuous Conduction Mode Power Factor Correction (CCM PFC), Two Transistor Forward (TTF) and Solar Boost. Typical applications are Solar, Server, Telecom and UPS (Uninterruptible Power Supply). The 650V breakdown voltage also makes C7 suitable for applications which require extra safety margin.

“The C7 series continues a twelve year innovation path of high quality Superjunction CoolMOS technology strengthening Infineon’s leadership in high-end power conversion,” says Jan-Willem Reynaerts, Product Segment Head of High Voltage Power Conversion at Infineon Technologies. “With CoolMOS C7´s Best-in-Class Figure of Merit (R DS(on)*E OSS), our customers are enabled to design a new generation of power conversion systems with an unprecedented combination of improved power density as well as efficiency.”

The C7 series offers the world’s lowest R DS(on) of 19mΩ in a TO-247 package and 45mΩ in the TO-220 and D 2PAK packages. The fast switching performance of C7 now enables customers for the first time to operate at switching frequencies greater than 100 kHz whilst achieving Titanium levels of efficiency in Server PFC stages. This enables higher power density by reducing the space requirements for the passive components.

Furthermore, reduced energy in the output capacitance (E OSS) as well as the low gate charge (Qg) bring efficiency benefits also at light load conditions. Combining the Best-in-Class performance of C7 with Infineon’s new Silicon Carbide (SiC) thinQ!™ Generation 5 Schottky Diode series and the ICE2 / ICE3 Control ICs offers designers unrivaled performance for CCM PFC circuits.

Availability

Samples of the 650V CoolMOS C7 products are available now. Volume production will start in June 2013.

For additional information on Infineon’s new 650V CoolMOS C7 family please visit www.infineon.com/c7

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2012 fiscal year (ending September 30), the Company reported sales of Euro 3.9 billion with close to 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Information Number

INFPMM201305.041

Press Photos

  • Infineon Introduces CoolMOS™ C7; Significant Step in Superjunction Technology Bringing the World’s Lowest RDS(on) to Hard Switching Applications
    Infineon Introduces CoolMOS™ C7; Significant Step in Superjunction Technology Bringing the World’s Lowest RDS(on) to Hard Switching Applications
    650V_CoolMOS_C7_Series

    JPG | 324 kb | 2657 x 2067 px