Infineon Enhances Online Design Tool for LED Lighting, Adding Additional Features and Support for LED Driver ICs Used in General Lighting Applications

Feb 29, 2012 | Market News

Neubiberg, Germany – February 29, 2012 – Infineon Technologies (FSE: IFX / OTCQX: IFNNY) enhanced its online design solution Infineon Light Desk, adding additional features and the support for a new series of AC/DC off-line LED drivers.

The Infineon Light Desk is an interactive, cloud-based design and verification environment that enables selection and configuration of LED driver ICs in a broad range of applications. Using the Infineon Light Desk, design engineers can identify the LED driver ICs that meet their specific system requirements. For the selected LED driver, the tool creates a custom design displayed in an interactive web schematic. Users can analyze the design performance by running system simulation models based on the Transim WebSIM® remote simulation technology.

With the offered redesign functionality users can optimize the proposed LED driver design. Infineon Light Desk offers to download instantly the Bill of Material for the final design as well as a comprehensive design summary report that includes design data, schematic and simulation results. Users can save designs for future reference as well as collaborate on designs with other users within a secure shared workspace. Additionally, the tool has an offline simulator SimT powered by SIMetrix/SIMPLIS: The simulator allows users to run their reference designs offline which enhances the simulation time. Users can directly download the simulator from the Infineon Light Desk. The Infineon Light Desk already supports custom designs for new high power DC/DC LED driver ICs (ILD series) as well as linear LED driver ICs (BCR3x and BCR4x series) for general lighting applications.

Furthermore, the Infineon Light Desk now supports the design-in for the recently introduced series of AC/DC off-line LED drivers. Used in general lighting applications operated directly from the AC mains input, such as LED retrofit lamps, the new LED drivers support dimming and non-dimming applications. The ICL8001G and ICLSx LED driver family employs quasi-resonant and fixed-frequency operation modes with integrated power factor correction. Through the implementation of an innovative primary control technique, excellent system efficiencies with significant reduced component count can be achieved. This enables compact designs for integration in standard screw based form factors used in LED retrofit lamps.

You can find further information about the Infineon Light Desk for AC/DC LED drivers at www.infineon.com/lightdesk

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2011 fiscal year (ending September 30), the company reported sales of Euro 4.0 billion with close to 26,000 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY). Further information is available at www.infineon.com.

Information Number

INFPMM201202.029

Press Photos

  • Infineon Enhances Online Design Tool for LED Lighting, Adding Additional Features and Support for LED Driver ICs Used in General Lighting Applications
    Infineon Enhances Online Design Tool for LED Lighting, Adding Additional Features and Support for LED Driver ICs Used in General Lighting Applications
    Infineon_Light_Desk

    JPG | 130 kb | 708 x 208 px