Infineon Technologies and Fairchild Semiconductor Expand Compatibility Partnership for Power MOSFETs, Providing Customers Supply Chain Security
Neubiberg, Germany – February 7, 2012 – Infineon Technologies and Fairchild Semiconductor today announced the extension of their compatibility partnership to encompass Infineon’s proprietary 5x6 power stage asymmetric dual MOSFET package. Infineon’s PowerStage 5x6 is a leadless SMD package, which integrates the low-side and high-side MOSFET of a synchronous DC/DC converter into a 5x6mm² package outline. This allows reduction in design area by up to 85%. The package also minimizes loop inductance and thereby achieves a peak efficiency of 93.5%.
This extended collaboration which began in 2010 is intended to provide customers supply chain security while balancing the drive towards best-in-class efficiency and thermal performance in DC-DC buck conversion. It takes advantage of the expertise both companies offer in asymmetric dual MOSFETs which can handle over 30A and increase power density.
“Fairchild and Infineon have standardized the pin-out, providing customers a secure supply chain for their high efficiency design needs in the computing, telecom and server markets,” said Richard Kuncic, Senior Director Low Voltage Power Conversion at Infineon Technologies. “This package alignment is staged to deliver performance leading products in a multi-source, industry standard package.”
“We are pleased to have added these enhancements to our PowerTrench technology”, said Joe Montalbo, Fairchild’s Vice President and General Manager, Consumer, Communications and Industrial, Low Voltage. “This partnership with Infineon, along with the standardized pin-outs, helps to improve the value proposition of this product line and makes it more compelling to our customers.”
About Fairchild Semiconductor
Fairchild Semiconductor (NYSE: FCS) – global presence, local support, smart ideas. Fairchild delivers energy-efficient, easy-to-use and value-added semiconductor solutions for power and mobile designs. We help our customers differentiate their products and solve difficult technical challenges with our expertise in power and signal path products. Please contact us on the web at http://www.fairchildsemi.com
About Infineon
Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2011 fiscal year (ending September 30), the company reported sales of Euro 4.0 billion with close to 26,000 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY). Further information is available at www.infineon.com.
Information Number
INFPMM201202.023
Press Photos
-
Infineon and Fairchild Expand Compatibility Partnership for Power MOSFETs (encompass PowerStage 5x6)Infineon_PowerStageJPG | 2.23 mb | 3543 x 2531 px