Infineon Expands XMC4000 Microcontroller Family; New Series Offers High-Resolution PWM Unit for Efficient Digital Power Conversion
Neubiberg, Nuremberg, Germany – November 27, 2012 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is presenting three new performance classes in its XMC4000 microcontroller family, which was specially developed for industrial applications and uses ARM® Cortex™ M4 processors, this week at the SPS IPC DRIVES 2012 trade show. The new XMC4400, XMC4200 and XMC4100 are the world’s first Cortex-based microcontrollers to offer a high-resolution PWM unit. With a PWM resolution of just 150ps, they are especially suitable for digital power conversion in inverters as well as switching and uninterruptible power supplies (UPS). Other applications are to be found in IO units in automation, user interfaces (HMI) and logging and control systems.
“With the XMC4400, XMC4200 and XMC4100, Infineon is expanding the scalability of the XMC4000 portfolio with further price and performance classes,” says Dr. Stephan Zizala, Senior Director, Industrial und Multimarket Microcontrollers at Infineon Technologies AG. “The new series combines all the strengths of the XMC4000 family with a high-resolution PWM unit, which is unique in the Cortex world. The result is a control quality comparable to the precision of analog solutions.”
The new XMC4400, XMC4200 and XMC4100 series microcontrollers are part of the Infineon roadmap to serve a broad range of industrial applications with the XMC4000 family. Like the XMC4500 MCUs, the XMC4400, XMC4200 and XMC4100 series offer powerful application-optimized peripherals, fast and robust embedded Flash technology, an extended temperature range of -40°C to 125°C, high quality standards and tools for automatic code generation in the DAVE™ 3 development environment.
Further functional features of XMC4400, XMC4200 and XMC4100
The XMC4000 family now comprises four series: XMC4500, XMC4400, XMC4200 and XMC4100. They differ mainly in core frequency, memory capacity, peripheral functions and number of IOs. The XMC4400, XMC4200 and XMC4100 series have a powerful CPU subsystem with 120MHz or 80MHz, DSP functionality, a Floating Point Unit, fast Flash memory (512 KByte, 256 KByte or 128 KByte) with a read time of just 22ns and error correction code as well as SRAMs up to 80 KByte. The extensive range of peripherals includes high-speed 12-bit AD and DA converters as well as integrated delta-sigma demodulator modules (XMC4400). Powerful communication is provided by Ethernet MAC (XMC4400), USB 2.0 and CAN interfaces as well as serial communication channels which can be software-configured individually as UART, SPI, Quad-SPI, I 2S or I 2C. They also provide a touch interface and an LED matrix display.
DAVE™ 3 and third party tools for comprehensive and efficient development support for XMC4400, XMC4200 and XMC4100
The XMC4400, XMC4200 and XMC4100 also are supported with the integrated development platform DAVE 3, which makes convenient, fast and application-orientated software development possible. The Eclipse-based environment with free GNU compiler and debugger can be extended using third party tools. DAVE 3 also supports automatic code generation based on predefined software components, the so-called “DAVE Apps”. The DAVE Apps are configured in a user-friendly way via the graphical user interface. DAVE 3 therefore ensures that developers of industrial applications can make full use of the functionality of XMC4000 microcontrollers with only little programming effort. The code that is generated can be compiled and debugged directly in DAVE 3 or imported into third party tools for further processing (currently Altium, ARM, Atollic, IAR Systems and Rowley). The first DAVE Apps with which, for example, various digital signals can be generated are already available for the XMC4400, XMC4200 and XMC4100 series as downloads. Further DAVE Apps will follow.
Infineon cooperates with more than 20 partners, who provide other specific development tools, software solutions, training and consulting services for the XMC4000 family.
Availability of XMC4400, XMC4200, XMC4100 and development kits
Samples of all three series – XMC4400, XMC4200 and XMC4100 – are available. High-volume production is scheduled to start at the end of the second quarter in 2013. The XMC4400 series (in LQFP-100 or LQFP-64 package) has a clock frequency of 120MHz and Flash memory of up to 512KB. The XMC4200 and XMC4100 series (both LQFP-64 or VQFN-48) operate at 80MHz. The XMC4200 has a Flash memory of up to 256KB and the XMC4100 of up to 128KB. XMC4000 development kits are available for all series.
Further information
More information about the XMC4000 family can be found at www.infineon.com/xmc4000. DAVE 3 can be downloaded free of charge from the Infineon website at www.infineon.com/dave.
Infineon is presenting the new XMC4000 microcontroller series at its booth #328 in hall 1 at the trade show SPS IPC DRIVES (Nuremberg, Germany, November 27-29, 2012). Visit www.infineon.com/sps for information on further exhibition highlights.
About Infineon
Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2012 fiscal year (ending September 30), the Company reported sales of Euro 3.9 billion with close to 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).
Information Number
INFATV201211.018
Press Photos
-
The XMC4000 family was specially developed for industrial applications. As the first Cortex™-based microcontrollers, the XMC4400, XMC4200 and XMC4100 offer a high-resolution PWM unit. With a PWM resolution of just 150ps, they are especially suitable for digital power conversion in inverters as well as switching and uninterruptible power supplies (UPS).XMC4400_4200_4100_LQFP-100_LQFP-64_VQFN-48_6-packagesJPG | 2.07 mb | 6496 x 5315 px
-
The XMC4000 family was specially developed for industrial applications. As the first Cortex™-based microcontrollers, the XMC4400, XMC4200 and XMC4100 offer a high-resolution PWM unit. With a PWM resolution of just 150ps, they are especially suitable for digital power conversion in inverters as well as switching and uninterruptible power supplies (UPS).XMC4400_4200_4100_LQFP-100_LQFP-64_VQFN-48_6-packages_plainJPG | 2.2 mb | 6496 x 5315 px
-
Dr. Stephan Zizala, Senior Director, Industrial and Multimarket Microcontrollers, Infineon Technologies AG Dr. Stephan Zizala, Senior Director, Industrial und Multimarket Mikrocontroller, Infineon Technologies AGZizala_Stephan_0212JPG | 1.63 mb | 1535 x 2126 px