IR's IR1168 SmartRectifier™IC Wins EDN Innovations Award 2010 for Best Component
EL SEGUNDO, Calif. — International Rectifier, IR® (NYSE: IRF), a world leader in power management technology, today announced the IR1168 SmartRectifier™ IC for AC-DC power converters for high-end LCD TVs was voted best product in the Components category of the EDN Innovation Awards, 2010.
Now in its twentieth year, the annual EDN Innovation Awards honor outstanding engineering professionals and products.
The IR1168 SmartRectifier™ 200V dual smart secondary-side rectifier driver IC is designed to drive two N-Channel power MOSFETs used as synchronous rectifiers (SR) in resonant half-bridge topologies. Co-designed with IR's DirectFET® MOSFETs, which feature IR's latest Trench silicon and packaging technology, the IR1168-based solution delivers an efficiency improvement of 1.5 percent for a standard 240W LCD TV switch mode power supply (SMPS) and a reduction of rectifier device temperature of 25°C while shrinking board size by two thirds.
"As a leader in power management, IR is at the forefront of developing innovative energy efficient solutions to help meet our customer's design challenges. We are very pleased that in selecting the IR1168 SmartRectifier IC as Best Component, IR has received such strong support from the engineering community," said Adam White, IR's senior vice president, Worldwide Sales.
The IR1168, featuring IR's proprietary high-voltage IC technology, supports burst mode operation to deliver efficiency benefits even at light loads. Ruggedness and noise immunity are accomplished using an advanced blanking scheme and double-pulse suppression that allows reliable operation in fixed and variable frequency applications. Other key features include maximum 500kHz switching frequency, anti-bounce logic and UVLO protection, 4A peak turn-off gate drive current, micropower start-up and ultra low quiescent current, 10.7V gate drive clamp, 70ns turn-off propagation delay and a wide Vcc operating range from 8.6V to 18V.
About EDN
EDN provides engineers and engineering managers with in-depth design features and deep technical information on microprocessors and other digital ICs, analog ICs, ASICs, computers and software, computer peripherals, test and measurement, components, power sources, interconnections and packaging, and much more. EDN also explores important application areas such as computers, communications, embedded, industrial, and consumer electronics. For more information go to http://www.edn.com.
About International Rectifier
International Rectifier (NYSE:IRF) is a world leader in power management technology. IR's analog- and mixed-signal ICs, advanced circuit devices, integrated power systems, and components enable high-performance computing and reduce energy waste from motors, the world's single largest consumer of electricity. Leading manufacturers of computers, energy-efficient appliances, lighting, automobiles, satellites, aircraft, and defense systems rely on IR's power-management benchmarks to power their next generation products.